articles RSS FEED

All Articles

Display backlight system
Bright, brighter, brightest? Why a display backlight system is more than meets the eye
By Avnet Staff   -   June 27, 2024
The human eye doesn’t perceive light in a linear way. So, if you’re looking to achieve a super-bright result, your display will need a huge amount of energy – in fact, more than double the cost of a standard display.
Coverglass on a display
Colour, style and shape: the art of coverglass
By Avnet Staff   -   June 27, 2024
How many times have you touched a glass screen today? Ten? Twenty? Thirty? More? Unless you’re actively monitoring your screen time, it’s barely even a consideration. But the kind of glass you interact with matters.
Person using a tablet
ePaper integration with PCAP
By Avnet Staff   -   June 27, 2024
Electronic paper (also known as e-ink, electrophoretic display, or electronic ink) is a kind of electronic display that mimics the appearance of ink on paper.
laptop with graphic overlay
How is AI changing the electronics industry?
By Philip Ling   -   May 22, 2024
Artificial intelligence has the potential to influence every part of any company. As a trusted partner and leader in technology, Avnet has a responsibility to its customers and suppliers to consider the impact of AI from all angles.
tensors
Why AI and embedded design share the same DNA
By Philip Ling   -   May 22, 2024
Intelligence comes in many forms. More of us are interacting with devices that appear to understand us. What and how they understand depends on the technology inside. How are embedded engineers implementing intelligence?
a-microchip-with-the-image-of-a-neural-network-on-the-top
Why AI must redefine processor architectures
By Philip Ling   -   May 22, 2024
Artificial neural networks are complex, multi-layered and multi-dimensional arrays of interconnected numerical values. Executing the math behind those connections is at the heart of AI. This math is unlike any other in the digital domain.
Patients using continuous passive motion machines in a medical setting
Learn how AI and the latest CPM technologies optimize patient rehabilitation
By Avnet Staff   -   February 21, 2024
Continuous passive motion (CPM) is now a critical part of patient rehabilitation. New technologies, including artificial intelligence, are helping medical OEMs take the next step to optimize patient therapy.
A stethoscope and medical images with data
Using sound to capture medical data boosts device innovation
By Avnet Staff   -   February 21, 2024
Wearable medical devices provide continuous body monitoring. Acoustic sensing is non-intrusive and the data supports early diagnosis and remote analysis. Are the stethoscope’s days numbered? That’s not likely, but new device opportunities abound.
A CT scanning machine in a hospital setting
Designers lead advances in CT scanning field
By Avnet Staff   -   February 21, 2024
High resolution and low dose are two of the latest developments in computed tomography equipment used by medical professionals. Looking inside tells us how these innovations are being achieved.
Wide bandgap semiconductor material in its raw form
When GaN is too fast for your application, consider SiC instead
By Avnet Staff   -   February 21, 2024
The best power converters are not always the ones that switch the fastest. Gallium Nitride (GaN) switches faster than other power transistors, but sometimes it is too fast. Silicon Carbide (SiC) MOSFETs may sometimes be a better option.
Illustration of a human circulatory system
Safer, targeted approaches to treat atrial fibrillation
By Avnet Staff   -   February 21, 2024
Pulsed field ablation is a bold approach to treating atrial fibrillation. The control required is extreme, leading to innovative solutions and newly patented technologies gaining attention from doctors, patients and OEMs.
seedlings growing out of a circuit board
Hitting the triple bottom line drives sustainable design
By Philip Ling   -   December 6, 2023
Sustainability at a corporate level continues to gain attention. Commercial success comes with social responsibility, something referred to in business as the triple bottom line and represented by the three Ps: profit, people and planet.
SPE & TSN
Ethernet evolution: The rise of SPE and TSN in automotive and industrial applications
By Harvey Wilson   -   September 14, 2023
IT professionals quickly recognized the benefits of networking computers and peripherals as the burgeoning computer industry established itself in the 1980s. However, making it a reality was another matter...
An-image-showing-various-modules-from-3G-4G-and-5G-implying-5G-is-faster
What’s new in mmWave and 5G SoCs and modules?
By Avnet Staff   -   August 24, 2023
This article looks at recent developments in mmWave and 5G modules and systems-on-chips (SoCs), and the benefits they represent to product development teams working at both the board level and system level of design.
5G mast in a cityscape at night
What is the impact of using AI in 5G networks
By Avnet Staff   -   August 22, 2023
AI is impacting the performance, security and maintenance of 5G networks. Network operators are racing to reap the benefits. AI promises to deliver returns on network investment and improve the end-customer experience along the way.
Satellite in Earth's orbit
Addressing the processing needs of Space 2.0 applications
By Paul Leys   -   August 9, 2023
Through low-cost launches designed for nanosatellites, the possibility to put technology into space has opened up a slew of applications. Though there are many possibilities, space environments even in orbits close to Earth are particularly harsh.
AI/ML DVI camera
Advancing quality control: The Evolution, Impact and Future of Defect Visual Inspection (DVI) in Manufacturing
By Michaël Uyttersprot   -   July 26, 2023
In the complex realm of manufacturing, Defect Visual Inspection (DVI) has emerged as a critical process, evolving significantly over time.
Batteries-in-declining-state-of-charge
Extending operational lifetime for battery-powered devices is crucial
July 24, 2023
Ultra-low power devices encourage the use of primary cell batteries. Developers can employ design techniques to maximize the power available. It starts with understanding your application’s power profile.
air conditioning system
AI takes on growing role in HVAC system efficiencies
July 24, 2023
In most countries, buildings account for about 40% of the total energy consumed. HVAC and lighting consume around half that amount. Fortunately, AI is already delivering improved energy efficiency in these systems.
A cnc machine is milling a piece of metal
Explore options for choosing an optical rotary encoder for motion control and position sensing
July 24, 2023
Rotary position sensing is used in motor control and user interface panels. It comprises various encoding methods. Optical encoders can offer advantages. We look at the options and how to choose the right one for your application.
three electric motors on glass table
How are magnetic rotary encoders used in industrial automation?
July 24, 2023
The Hall effect is used in rotary encoders to monitor position, speed and direction in electric motors and rotary dials. The encoder designs vary, so it is helpful to understand the main features and how they affect performance.
A-hand-reaching-out-to-touch-a-display-panel-showing-automation-technology-system
Factory automation realizes boost from new technologies
By Philip Ling   -   July 23, 2023
The technologies behind automation must combine reliability and stability with an eagerness to develop in a commercially responsible way. Discover the technologies making the grade right now.
Vehicle to Grid EV charging
EV Charging Series, Part 3: How V2G Benefits Drivers and Electricity Suppliers
By Harvey Wilson   -   June 19, 2023
Vehicle-to-grid (V2G) is the capability for EVs to send power from their batteries back to the main electricity grid. This can be hugely helpful in meeting demands on the grid, stabilising it, and dealing with the inconsistency of renewables.
The Avnet RFSoC Gen 3 with the Phased Array Antenna Module (PAAM) from Fujikura
How modelling and simulation support mmWave design integration and delivery
By Philip Ling   -   June 6, 2023
5G mmWave system design is too complex to approach at a component level. Engineers need to take full advantage of software in all its forms to bring new solutions to market and provide full lifetime support.
STM32 MCU Series
Transformative IoT solutions with the STM32 32-bit Wireless MCU Series
June 1, 2023
Choosing the right microcontroller for your project is crucial. In this post, we’ll explore the capabilities of ST’s 32-bit wireless MCU, STM32WBA52 and the IoT applications that benefit most from them.
EV charging station in home garage
EV Charging Series, Part 2: Integrating EV Charging with Matter and the Smart Home
By Harvey Wilson   -   June 1, 2023
As electric vehicles (EVs) become more common on our roads, with sales continuing on an upward trend, there’s an increasing focus on how we charge them. For most of us, we’ll want to handle much of our charging at home, both for convenience and to take ad...
The Future of EV charging
EV Charging Series, Part 1: The Future of EV Charging - Revolutionary Developments are Closer Than You Think
By Harvey Wilson   -   May 17, 2023
Electric vehicles (EVs) are big business – you only need to look at Tesla’s share price to see just how big. Imagine how much more valuable the market would be if EVs could charge in a few seconds, not minutes or hours.
Power trends - Si, SiC or GaN? Power dashboard with people surrounding it and analysing
Power trends and the choice between Si, SiC and GaN
By Thomas Hauer   -   May 3, 2023
Wide bandgap (WBG) semiconductors can deliver performance and power efficiency that are superior to those of silicon devices, and have useful properties such as high operating temperature. This means that WBG devices, using materials such as gallium nitri...
two materials combined in organic form
Combining GaN and SiC for cost-effective power conversion
By Avnet Staff   -   April 20, 2023
The public image of silicon carbide (SiC) and gallium nitride (GaN) is as wonder materials. We know they are displacing older silicon technology, boosting the efficiency of power conversion stages. However, neither is a universal solution.
A close-up of an onboard charger in an electric vehicle
Understand practical GaN and SiC differences for EV onboard chargers
By Avnet Staff   -   April 18, 2023
Depending on the design, wide bandgap devices may provide efficiency gains in power conversion for onboard chargers. But which do you choose over silicon if any? We look at the options and offer some advice.
First        1  2  3  ...        Last          Results Per Page: 30  60  90  All