Qseven®

Qseven® designs are typically ones where low power consumption and entry-level compute performance are needed. If this is what your application needs our product offerings will give you a very attractive performance-to-price ratio. A number of our suppliers are capable of customising Q7 designs based on your needs so please contact us if you can’t immediately see an exact match to your requirements as this portfolio is still evolving.

What is Qseven?

Qseven® is an open standard of the SGeT Standardization Group. Taking advantage of the ongoing development in processor technology towards smaller and more power efficient CPUs, Qseven® has in recent years become the most widely adopted new standard for small form factor modules.

The Qseven® specification has been extended to include module architectures based on the Arm® processor which is renowned for its excellent performance to power ratio. Providing different processor architectures and a wide range of modules for commercial and extended temperature together with matching baseboards, the MSC Qseven® family leads the way to feature rich and small, low power modular systems.

GET IN TOUCH

Qseven Modules

Browse our Qseven compute modules, carrier boards and starter kits below, and click the modules or the button to view more details on the features and specifications. Use the contact form to tell us more about your project and talk to an expert about how we can accelerate your product design.

Product

MSC Q7-EL

The new MSC Q7-EL module features Intel’s next-generation low-power, multi-core system-on-chip (SOC) Atom generation (codenamed “Elkhart Lake”). Built on 10nm process technology the SoC integrates next generation Intel Atom core architecture.

Q7 EL SL

Product

MSC Q7-IMX6PLUS

The design of the MSC Q7-IMX6PLUS module was optimized to provide an especially economic platform for NXP’s i.MX6 and i.MX6Plus CPUs offering quad-core, dual-core and single-core ARM® Cortex™-A9 compute performance at very low power consumption.

Avnet Embedded MSC Q7-IMX6PLUS - front side view of the board

Product

MSC Q7-AL

The new MSC Q7-AL module features Intel’s next-generation low-power System-on-Chip (SOC) for the Internet of Things. The Intel Atom Processor E3900 series integrates processor core, graphics, memory, and I/O interfaces into one solution.

Avnet Embedded MSC Q7-AL - front side view of the board

Product

MSC Q7-BT

The MSC Q7-BT module is based on the Qseven Rev. 2.0 and using Intel’s multi-core System-On-Chip (SOC) Atom generation that integrates next generation Intel processor core, graphics, memory, and I/O interfaces into one solution.

Avnet Embedded MSC Q7-BT - front side view of the board

Product

MSC Q7-BW

The MSC Q7-BW module is based on Intel‘s multi-core system-on-chip (SOC) Atom generation (“Braswell”) that integrates next generation Intel processor core, graphics, memory, and I/O interfaces into one solution.

Avnet Embedded MSC Q7-BW - front side view of the board

Talk to the experts!

Need technical support?

Let us know about your product or your challenge and our team will be in touch to discuss how we can support you. 

CONTACT US

 

Qseven Carrier Boards

Contact Us

Submit your inquiry via the form below.

 

Product

MSC Q7-MB-EP5

The EP5 is not suited for low-volume applications. The MSC Q7-MB-EP6 (x86) and the MSC Q7-MB-EP4-001 (ARM) are suggested for evaluation and use in low-volume Qseven applications.

Q7 MB EP5

Product

MSC Q7-MB-EP6

The new Qseven™ Rev. 2.0 embedded platform MSC Q7-MB-EP6 offers a variety of interfaces commonly used in embedded applications such as Gigabit LAN, USB 3.0, USB 2.0

Avnet Embedded MSC Q7-MB-EP6 - front side view of the board

Product

MSC Q7-MB-RP3

The MSC Q7-MB-RP3 is the third generation reference platform provided to test and qualify Qseven™ Rev. 2.0 modules for compatibility with the specification.

Avnet Embedded MSC Q7-MB-RP3 - front side view of the board

Product

MSC Q7-MB-EP4

The Qseven™ embedded platform MSC Q7-MB-EP4 offers a variety of interfaces commonly used in embedded applications such as Gigabit LAN, USB 2.0, RS232 and LVDS / DVI to connect displays.

Avnet Embedded MSC Q7-MB-EP4 - front side view of the board

Qseven Starter Kits

Product

MSC Q7-SK-AL-EP6

The Qseven Starter Kit for Qseven modules with the Intel “Apollo Lake” E3900 is based on a 3.5″ Qseven rev. 2.0 carrier board MSC Q7-MB-EP6 and contains all necessary products to quickly enable the user to run and evaluate the Q7-AL module.

CE6 Starter kit

Product

MSC Q7-SK-BW-EP6

The Qseven Starter Kit for Qseven modules with the Intel “Braswell” N3000 is based on a 3.5″ Qseven rev. 2.0 carrier board MSC Q7-MB-EP6 and contains all necessary products to quickly enable the user to run and evaluate the Q7-BW module range.

CE6 Starter kit

Product

MSC Q7-SK-BT-EP6

The Qseven Rev. 2.0 Starter Kit for Qseven modules with the Intel Atom E3800 SOCs is based on a 3.5″ Qseven carrier board MSC Q7-MB-EP6 and contains all necessary products to quickly enable the user to run and evaluate the E3800 module range.

CE6 Starter kit