Training & Events
Renesas Intersil Space Update
Date: February 14, 2024
Location: online, on-demand
Aerospace & defense   Filter By   Aerospace & defense RSS FEED
Aerospace and defense applications in systems like avionics, communications, guidance and radar systems demand the best in performance and reliability—and the knowledge and expertise to pull it off. Explore our resources to stay up to date with aerospace and defense trends and technology.
Woman riding in self-driving car.
Bringing mm-wave beamforming to new applications
By Steven Fireman   -   April 9, 2024
With 5G rolling out and the help of phased array antennas, the 30 to 300 GHz, and specifically the millimeter-wave bands, of the RF spectrum are making their way into applications like autonomous driving.
Satellite in Earth's orbit
Addressing the processing needs of Space 2.0 applications
By Paul Leys   -   August 9, 2023
Through low-cost launches designed for nanosatellites, the possibility to put technology into space has opened up a slew of applications. Though there are many possibilities, space environments even in orbits close to Earth are particularly harsh.
aircraft flying over city
Where we’re going, we don’t need roads
By Philip Ling   -   February 17, 2023
We’re a grounded species reaching for the stars. Personal aircraft will let us colonize the air immediately above us and expand our cities in ways that don’t need networks of multilane highways. For eVTOLs, air taxis are just the beginning.
satellites in low Earth orbit
Putting 5G in space for the massive IoT
By Philip Ling   -   January 4, 2023
5G cellular networks and the massive IoT are a natural fit. Putting 5G cell towers in space is taking massive to a new level. To learn more, Avnet spoke with Sateliot Chief Business Officer Gianluca Redolfi, one of the pioneers in this area.
Globe and FPGA chip illustrated
FPGAs fit for space
By Paul Leys   -   November 4, 2022
The arrival of Space 2.0 has democratised the use of satellites and opened up an array of applications that can be serviced by electronics in low-Earth orbit (LEO) as well as those on higher trajectories such as geosynchronous equatorial orbit (GEO).
Brand new rad-hard MPUs next to each other
Radiation-hardened processors for space
By Paul Leys   -   September 28, 2022
Lower launch costs have helped open up a raft of applications for satellites that, by featuring advanced sensors and computing, are able to deliver novel communications and remote-monitoring services.
Image of the satellite signals
Overcoming the radiation challenges of space electronics
By Paul Leys   -   May 2, 2022
Through low-cost launches designed for nanosatellites, the possibility to put technology into space has opened up a slew of applications. Though there are many possibilities, space environments even in orbits close to Earth are particularly harsh.
Image of the globe covered by satellite signals
Nanosatellites enable space-based applications for the many
By Paul Leys   -   April 13, 2022
Nation states and major multinationals used to be the only organisations that could launch and operate satellites.
James Webb Space Telescope launch
How streaming HD video from space enables future missions
By Philip Ling   -   March 21, 2022
As the recent James Webb Space Telescope launch demonstrated, there is no doubt that streaming HD video from space is going to be hugely popular with the public and even more important for the engineers responsible for future missions.
Image of a robot walking in the hallway
How space robotics extends our capabilities and insights
By Paul Leys   -   March 8, 2022
In August 2012, Voyager 1, a spacecraft launched by NASA in 1977, became the first human-made object to reach interstellar space.
Image of a virtual screen with numbers and codes
AI/ML related applications emerging within the space industry
By Paul Leys   -   March 8, 2022
Rapidly growing interest in the use of artificial intelligence (AI) in space exploration and commercialisation is being fuelled by the promise that it can improve the robustness and cut the cost of missions.
A satellite orbiting over the Earth with Sun shining in the distance
Selecting SSDs for aviation, space and defence applications
By Paul Leys   -   January 27, 2022
As more electronics-based hardware is used for aviation and space applications, whether for civilian or defence purposes, the demands placed on data storage become significant.
Two astronauts observing Milky Way
Why ‘new space’ satellites demand a new approach to components
By Paul Leys   -   June 18, 2021
Traditional satellites can cost hundreds of millions of dollars, with this price tag in part driven by the need to use expensive space-grade components, capable of operating for many years in extremely harsh conditions.
Illustration of a campus with 5G network
5G Campus Networks: Build your own
May 29, 2021
Operating a private campus network offers several advantages and will help improve production and enable factory automation.
Smart cars in a crossroad
Top 10 pitfalls in developing machine vision systems with artificial intelligence
April 28, 2021
Machine vision (MV) and artificial intelligence (AI) provide valuable inspection and analysis capabilities to a wide range of leading-edge applications. As with all advanced technologies, there are pitfalls to avoid.
Smart cars in a crossroad
FPGA vs. GPU vs. CPU – hardware options for AI applications
April 28, 2021
Field programmable gate arrays (FPGAs) deliver many advantages to artificial intelligence (AI) applications. How do graphics processing units (GPUs) and traditional central processing units (CPUs) compare?
Smart cars in a crossroad
Why artificial intelligence at the edge matters
October 27, 2020
AI at the edge will have profound effects on many industries, including transportation, defense, manufacturing and healthcare to name a few. How will AI at the edge change these industries, and why does it matter?
Satelite in space
Low-Earth-Orbit Satellites and IoT: The Next Space Revolution
June 27, 2019
Over the past decades, small satellites & IoT have dramatically changed the future of humans in space. The focus shifted from one-of-a-kind systems performing specific missions to satellite constellations working in concert to achieve a larger purpos
Illustration of an aircraft taking off
Smart Airports: IoT is Taking off
February 6, 2018
Airports are a massive part of the economy and key players in regional growth and development.
First1 Last  Results Per Page: 30 6090All