Pressure Sensors: The Design Engineers' Guide

Pressure sensors for corrosive liquids and gases

Some pressure sensors are specifically designed to work with corrosive, aggressive or highly contaminated liquids and gases, collectively known as ‘corrosive media’.

These corrosive substances will destroy or damage other substances that they come into contact with, including metals and organic compounds. This makes them difficult and dangerous to work with and raises unique challenges for the design of pressure sensors with corrosive media compatibility.

Applications

Pressure sensors for corrosive media are used in applications such as industrial measurement and control, industrial boilers, monitoring the levels of chemical storage tanks, waste management, medical devices, instrumentation and analytical devices.

They also find applications in energy technologies such as those using natural gas, biogas, landfill gas and CHP (combined heat and power).

Measurement options

Pressure sensors for corrosive media usually measure pressure in one of two ways: absolute or gauge. 

Absolute pressure is measured relative to a particular value, such as zero or atmospheric pressure at sea level. With this method, the reading is always the same, regardless of where the unit is located.

Gauge pressure is measured relative to the surrounding atmosphere, meaning that readings can vary based on location and altitude.

Technology

Pressure sensors for corrosive media are transducers, generating an electrical signal in proportion to the pressure they measure. This allows pressure to be monitored by various devices with a suitable interface.

Most pressure sensors for use with corrosive media use the principle of piezoresistance. The sensor is based around a diaphragm made from a ceramic material that’s elastic but resistant to corrosion and abrasion.

The diaphragm acts as a semiconductor distortion gauge: when the corrosive liquid or gas presses on it, it is bent out of shape, which distorts the crystalline structure of the material. This, in turn, changes the electrical resistance of the diaphragm, allowing the sensor to reflect changes in pressure in the form of a change in current.

Options and specifications


A typical pressure sensor designed for corrosive media

Pressure sensors for use with corrosive media often feature housings made from stainless steel or plastics such as PVDF, PVC or PPS. The sensor elements themselves are typically ceramic, although some sensors use a stainless steel diaphragm backed by silicon oil that transfers pressure to the sensing element.

The pressure sensors will usually specify a suitable pressure range (for example, 200 mbar–35 bar). Certain sensors may be able to measure both absolute and gauge pressure (see above), with a pressure range specified for each. Some sensors can be configured to measure negative pressure as well as positive.

Some sensors for corrosive media are temperature-compensated, so their readings are not affected by changes in media temperature.

Sensors will also specify the voltage output that they use to indicate pressure changes, and their output at zero pressure (for example, 100mV).

In some cases, the O-ring used to seal the ceramic diaphragm to the body of the sensor can be made from different materials, such as fluorocarbon plastomer (which resists mineral acids, petroleum oil, salt solutions and chlorinated hydrocarbons), nitrile rubber (which resists paraffin-based materials, fatty acids, glycerines or alcohols) or EPDM - ethylene propylene diene monomer (which resists many acids and alkalis).

Some sensors may be certified under a standard such as ATEX 95 (for Europe) or IECEx 02 (worldwide). Under EU law, ATEX 95 is required for all electrical and non-electrical equipment that’s used in hazardous environments, while IECEx 02 is intended only for electrical equipment in hazardous environments. Hazardous environments include those involving flammable materials or dust.

Limitations

Many sensors are suitable for use with either corrosive liquids or corrosive gases. Their datasheet or other supporting material will specify which media they’re compatible with.

Other sensors are suitable for use with specific types of liquid or gas. However, manufacturers will sometimes be able to modify their sensors to suit specific requirements.

Engineers may need to consider what will happen in the event of the sensor failing. Corrosive or hazardous media could enter the sensor, leading to contamination. Conversely, internal parts or materials (such as oil used as a filling fluid) may leak into the process media.

If you want to learn more about the different types of media that pressure sensors can measure, the applications of each type, and the different sensor options for your design, click the links below to jump to the section you're interested in.


Looking for more on pressure sensor technology? Check out the further chapters of this guide below, or if you're pressed for time you can download it in a PDF format here.

Need some advice on pressure sensors?

Our pressure sensor experts are on hand to help you make the right choice for your application.

Webinar

Discover the keys to designing pressure sensor applications with this 30-minute technical presentation and Q&A with Nicholas Argyle, Applications Engineer EMEA, TE Connectivity.

Watch On Demand

White paper

Need a more digestible introduction to pressure sensors? Download the white paper, 'Pressure sensors: Design considerations and technology options'.

Download

Sensor solutions brochure

Discover the latest sensor solutions available from Avnet Abacus.

Download

Sensors linecard

Explore our pan-European sensor suppliers and their products and solutions.

Learn More

New products

Discover the latest product announcements from our sensor suppliers.

Learn More

Place custom HTML here...

Bourns

BPS130 series MEMS pressure sensor

The BPS130 series MEMS pressure sensor features harsh media compatibility and high temperature operation with high accuracy.

Bourns BPS130 series MEMS pressure sensor

Pressure Sensors Chapter 1 GBL

Display portlet menu

Chapter 1

How pressure sensors work

An introduction to pressure sensors covering the different types, how they work, their function, construction, and what to consider in your design choices.

Pressure sensors chapter 1 graphic

Pressure sensors chapter 5 GBL

Display portlet menu

Chapter 5

Types of pressure measurement

What’s the difference between absolute, gauge and differential pressure sensors? And how do you know which one to use?

Pressure sensors guide chapter 5 graphic

Pressure Sensors Chapter 2 GBL

Display portlet menu

Chapter 2

Pressure sensor applications

Discover the recent innovations in pressure sensor technology that are enabling smarter, safer, and more environmentally friendly electronics for businesses and consumers alike.

Pressure sensor guide chapter 2 graphic

Pressure sensors chapter 6 GBL

Display portlet menu

Chapter 6

The core pressure sensor technologies

What’s the difference between the different pressure sensor technologies? And how do you know which one to use?

Pressure sensor guide chapter 6 graphic

Pressure Sensors Chapter 3 GBL

Display portlet menu

Chapter 3

The different types of pressure sensors

Discover how pressure sensors vary according to the type of pressure measurement, sensing principles, output signal, media, MEMS technology, mounting and more.

Pressure sensor guide chapter 3 graphic

Pressure sensors chapter 8 GBL

Display portlet menu

Chapter 8

Pressure sensing in harsh environments

An in-depth guide to pressure sensors for harsh environments - designing for extreme temperatures, high pressure, and corrosive and dynamic environments.

Pressure sensor guide chapter 8 graphic

Pressure sensors chapter 4 GBL

Display portlet menu

Chapter 4

Pressure sensor output signals

Sensors, transducers, or transmitters? The right selection is important for your application. So what's the difference and how do you choose between them?

Pressure sensor guide chapter 4 graphic

Pressure sensors chapter 9 GBL

Display portlet menu

Chapter 9

Understanding specifications

Explore the datasheet and the different factors affecting the accuracy of pressure sensor readings. Discover how to make the right choice for your application.

Pressure sensor guide chapter 9 graphic
Image Product Description Link New