Featured Articles
AI/ML - Location, Location, Location
In the last few years, huge leaps in artificial intelligence (AI) and machine learning (ML) technology have enabled the incorporation of ‘intelligence’ in a rapidly growing number of products in applications as diverse as GPT tools, IC layout, and autonomous navigation. The adoption of AI and ML has made such products more powerful, faster, accurate and easier to use.
These examples demonstrate more than just the range of applications that can be aided or enabled by AI/ML. Each also gives a use case of where AI/ML can be deployed – in the cloud, on premise, or at the edge, respectively.
Read Article
AI and the Question of Processors
As transformative as artificial intelligence (AI) has already been in agriculture, medicine, finance, automotive, and elsewhere, there remain seemingly endless future benefits of AI. With no end in sight for the boom in the AI market, vendors of graphics processors (GPUs), general purpose processors (CPUs), neural processors (NPUs) and other specialized AI processors will be fighting each other for market share for years to come.
No single processor type is likely to emerge as a definitive winner, appropriate for all AI workloads, at least not in the foreseeable future. Each type of processor has advantages and drawbacks. As always in engineering, the tradeoffs will balance out differently for each use case. Avnet Silica can provide expert guidance as customers evaluate which processor type will be best for their specific AI workloads.
Read Article
Parsing AI - Glossary
A good first step toward exploring the adoption of AI technology is gaining familiarity with concepts and the specific engineering terminology associated with them. One of the difficulties with learning about AI is that some of the concepts are interdependent, and terms that aren’t strictly interchangeable can be used for each other. This can streamline verbal communications, but it can be confusing to the uninitiated. Compounding the confusion, any two organisations might have slightly different definitions for any given term.
Our purpose here is to be neither comprehensive nor fully definitive. It is to introduce the uninitiated to some of the most common concepts and terms in AI.
Read Article
AI/ML Models and Algorithms
Artificial intelligence (AI) and machine learning (ML) can be used to pull insights out of huge volumes of information quickly and efficiently. AI/ML can also give machines the ability to process information similar to the way humans do.
AI/ML can perform recognition and classification, predictive analytics, natural language understanding, and other tasks that are difficult or impossible to accomplish with traditional computing.
These capabilities lead to an impressive variety of use cases: voice recognition, autonomous driving, epidemiology, pharmaceutical design, software coding, financial trading, and more.
Read Article
Evolution of Generative AI
Generative AI is not new. It has, however, recently taken an enormous leap in what it can do, inspiring no little amazement, as well as a bit of alarm.
A popular candidate as the first generative AI is the first chatbot, ELIZA, introduced in the 1960s, which was trained to respond like a psychologist. The subsequent history of AI research was marked by AI “winters” alternating with periods of resurgence typically coincident with some applicable technological advance, such as the introduction of microprocessors or the formulation of AI techniques such as back-propagation.
Read Article
Related Articles
Placing Greater Intelligence at the Edge
By having the intelligence closer to where the action is, it will be possible for systems to react more quickly to changing situations, for instance, where there are serious cost implications or are safety-critical, as well as allowing for better user experience without any annoying lags. Having access to edge-based ML inferencing will be beneficial in a broad array of application scenarios. Among these will be factory automation, machine monitoring, predictive maintenance, object recognition/categorisation, access control, and smart homes/buildings.
Replacing centralised intelligence, to a certain degree, with a distributed strategy that puts more autonomy at the edge will call for locally situated processing capabilities. This is why microcontroller units (MCUs) are now starting to emerge that can provide the strong ML inferencing performance needed, while at the same time supporting low-power operation.
Read Article
How is AI Changing the Electronics Industry?
Artificial intelligence (AI) and machine learning (ML) have created an inflection point in product design. For two decades we have seen an exponential increase in data creation. The Internet of Things (IoT) is a big part of that, but companies like Avnet have been creating their own data for much longer.
Now, AI and ML are providing a viable way to make more use of it.
Avnet Senior Vice President Rebeca Obregon and Chief Information Officer Max Chan provide some insights into how distributors need to think about AI. They also talk about how distribution will react to the increasing demand for AI and ML hardware and software solutions.
Read Article
Why AI Must Redefine Processor Architectures
The demand for AI running on programmable platforms is a unifying application. Microprocessors and microcontrollers all share similarities, but the applications they target tend to vary. AI is different.
General purpose is essential to the industry. It offers economies of scale in manufacturing. Common architectures enable a common toolchain, which makes software development manageable. Similar is good, it creates competition and innovation. These are positives for customers in a global industry.
Read Article
Why AI and Embedded Design Share the Same DNA
In simple terms, running an ML model on an embedded system comes with all the same challenges doing clever things on constrained platforms has always had. The details, in this case the model, vary, but the basics are the same. Engineers need to select the right processing architecture, fit the application into the type and amount of memory available, and keep everything within a tight power budget.
The key difference here is the kind of processing needed. ML is math-intensive; in particular, multidimensional math. ML models are trained neural networks, which are basically multidimensional arrays, or tensors. Manipulating the data stored in tensors is fundamental to ML. Efficient tensor manipulation within the constraints of an embedded system is the challenge.
Read Article
The Impact of Using AI in 5G Networks
To deliver an increase in capacity and throughput with a reduction in latency, 5G networks operate at frequencies up to 71 GHz. Trees and other foliage are great for the environment but not so good for RF energy propagation, particularly mmWave frequencies. To compound things, the density of vegetation and the level of attenuation it presents, changes with the seasons.
Artificial intelligence (AI) technologies can significantly improve performance and user experiences.
Read Article
Advancing quality control: The Evolution, Impact and Future of Defect Visual Inspection (DVI) in Manufacturing
In the complex realm of manufacturing, Defect Visual Inspection (DVI) has emerged as a critical process, evolving significantly over time. The landscape of visual inspection has transformed from manual checks performed by artisans to AI-enhanced automated systems. As manufacturing processes continue to become more sophisticated, the importance and effectiveness of advanced Defect Visual Inspection (DVI) solutions escalate, presenting opportunities for improved quality control.
Read Article
Read all Artificial Intelligence Articles
On-Demand AI/ML Webinars
See all of our on-demand webinars for Automotive on the Avnet Silica DEEP portal.
GO TO PORTAL
Featured Webinars
Accelerate and simplify your Edge AI Vision Projects with Arduino Pro
Avnet Silica and Arduino invite you to a dynamic 45-minute journey into the heart of Edge AI Vision applications within the industrial and Enterprise realms, where challenges meet innovation head-on. Discover how Arduino provides a better and easier approach to overcoming the challenges of developing embedded Edge AI OEM solutions and products. Through the lens of a compelling customer worker safety wearable use case, we'll delve into the transformative power of the new Arduino Pro portfolio, featuring the Arduino Pro Portenta H7 SOM and industrial edge ready Arduino Pro Nicla Vision sensor and how it solved the customer’s business outcomes on accelerating time to market.
GO TO WEBINAR
Revolutionising Visual Quality Control & Defect Inspection
Discover the transformative power of Defect Visual Inspection (DVI) technology in a quality control environment. We'll delve into the core functional features of a powerful visual inspection system employing computer vision and artificial intelligence. It is all at the edge, to keep the quality control right there where the sensor is on industrial embedded devices and to preserve data privacy and industrial secrets by keeping your data localised.
Witness DVI in action with a live demonstration, showcasing its precision and efficiency in defect detection across various industries. We'll also provide insights into how to acquire and implement DVI, whether through a kit, SOM (system on module), or software.
GO TO WEBINAR
MuseBox - The ultimate AI/ML prototyping Accelerator on AMD KV260 for Real-Time Embedded Vision Applications
Learn about MuseBox's capabilities and supported platforms, with a special emphasis on KRIA. Through live demonstrations, we will demonstrate the power of MuseBox in action, from prototyping to product development.
MakarenaLabs will provide an overview of their IP and consulting capabilities for your AI/ML projects, and we’ll show you how to get started with MuseBox, including access to the platform and the support provided by MakarenaLabs and Avnet Silica.
GO TO WEBINAR
Featured Podcasts
Episode 51: Smart Tech Synergy: Unveiling the Future of IoT and AI
We now live in a world where every device communicates, and every data point tells a story. And 2023 definitely will be remembered as the year of Artificial intelligence. Joining us today is David Ly, CEO of Iveda. They provide global solutions for cloud-based video AI search and surveillance technologies. We'll explore how integrating IoT and AI can revolutionize everything from smart cities to telehealth and advanced security systems.
Episode 50: Demystifying AI in IoT: Real-Time Analytics and Beyond
Together with Mohammed Dogar (VP, Global Business Development and Ecosystem), we'll explore the AI Center of Excellence at Renesas, unravel some common misconceptions about AI in the IoT space, and discuss the opportunities in real-time analytics.
We'll also delve into how technology is evolving in areas like voice, vision, and audio analytics, and how engineers can navigate this AI-centric landscape despite not being data scientists.
Episode 45: Emotion in the Machine: Exploring Affective Computing
Today’s special guest is Nina Holzer. She is a researcher from the renowned Fraunhofer Institute for Integrated Circuits IIS and the team lead for 'Multimodal Human Sensing'.
Together, we'll explore the fascinating intersection of human emotions, artificial intelligence, and the future of human-computer interaction. So, tune in as we delve deep into the heartbeats of our machines.
Episode 44: Seeing Beyond the Surface: AI in Defect Visual Inspection
Today, we're diving deep into a technological revolution reshaping the quality control and manufacturing world: AI-based Defect Visual Inspection, or DVI.
With us today is Giovanni Gualdi, the CEO of Deep Vision Consulting, a visionary pushing the boundaries of how we perceive and rectify defects. And Michaël Uyttersprot from Avnet Silica is someone at the forefront of integrating smart solutions into industrial spaces. We will explore the mechanics, use cases, and business models of AI-powered quality control and manufacturing inspections.