Hero Banner

Sub Navigation

Intro text (LC)

Embedded platforms for demanding vision applications

Vision systems need to manage multiple high-resolution images coming from multiple cameras simultaneously. Adding AI to the workload means running compatible software on a processor platform capable of combining high memory bandwidth and multiple camera interfaces.  

The solution is a 64-bit platform that extends memory addressing capacity while preserving software compatibility and adding the resources needed to tackle demanding vision applications. GPUs, camera interfaces and memory bandwidth are specific capabilities that need to be fully integrated into your chosen platform. AMD’s embedded processor families offer the right mix of performance and efficiency.

Main body and table (LC)

High-resolution image processing requires substantial working memory

Vision AI is moving from simple pass/fail inspection to systems that see, understand and act in real time. The shift is chaining what engineers need from an embedded platform. Processor performance and TOPS ratings get most of the attention, but memory is often what limits a vision system. That balance may only show up in production. Here are three things every AI vision system needs to deliver, and why memory becomes the deciding factor.

  • A vision system must keep up with every frame from every camera; capturing, processing and acting on high-resolution video from several cameras at once, without dropping frames. Every stream needs its own buffer for raw frames, pre-processing and inference results. Adding a camera, increasing resolution or frame rate and the memory needs go up with it or frames get dropped or delayed. On a production line, that means defects pass inspection. In a robot it means reacting too late.
  • Running models that are accurate enough to trust. Detection, segmentation and vision-language models are what separate a guess from something a customer can rely on. That’s harder to achieve at the edge because the models are large, and the weights, intermediate data and any other models they rely on all have to fit into the same memory at the same time. Compensating for memory bandwidth issues creates latency, which may result in false rejects or missed faults. Ultimately, that erodes trust in the system.
  • Turning vision into action must be fast and repeatable. For a vision system, recognition is just the start. The result needs to become an action in real-time. That’s harder if the CPU, GPU and NPU have separate memory, because data has to move between them, adding latency and timing uncertainty. A unified memory pool that the CPU, GPU and NPU can all read and write without copying reduces handoffs and increases performance.

How AMD matches resources to application

 

EXAMPLE APPLICATIONS SMART CAMERAS MULTI-CAMERA INSPECTION ROBOTICS & PHYSICAL AI VISION ANALYTICS
Platform Ryzen AI Embedded P100 Ryzen Embedded 9000 Ryzen AI Embedded X100 EPYC Embedded 4005/9005
AI Engine NPU, up to 80 system TOPS Up to 16 Zen 5 cores with AVX-512 for inference CPU, GPU and NPU on one chip, running models with 100B+ parameters High core counts for aggregating many streams
Memory DDR5-5600 or LPDDR5x up to 8533 MT/s, with ECC Dual-channel DDR5 with ERC Up to 128 GB of unified LPDDR5 192 GB up to 9 TB per socket
Benefits Runs vision AI at low power without a separate accelerator Fast, predictable compute for machine-vision pipelines One shared memory pool, so no copying data between Many cameras, long retention, model training at the edge

 

Avnet Silica and AMD logo (sHTML)

 

AMD Webinar Spotlight (GBL)

Training & Events

Discover why AMD x86 Embedded Processors are the Right fit for You

Not all x86 embedded processor suppliers are the same. With AMD products, you should expect leadership performance, longevity, and reliability to power your bespoke embedded applications and offer scalability and differentiation for your customers.

A man is watching webinar

Conclusion (LC)

Dive deeper into the benefits of running vision AI on AMD’s embedded processors

The AMD Ryzen AI Embedded P100 series has a configurable total dissipated power (TDP) of 15-54 W. The range suits a fanless vision system that might be in a sealed enclosure, delivering ‘always-on’ low-power inference. The combined system throughput (CPU, GPU and NPU) is up to 80 TOPS. In a mobile robot, this might mean the CPU handles navigation and motion control, the GPU processes camera feeds, and the NPU runs object detection.

The AMD Ryzen Embedded 9000 brings up to 16 Zen 5 cores, large cache and 28 PCIe Gen5 lanes to accommodate discrete accelerators and frame grabbers. These credentials make it a good choice for machine vision in defect detection, quality control, and T&M. With AMD’s 3D V-Cache reaching up to 128 MB, some AI models and working data could remain entirely in cache rather than in DRAM.

The AMD Ryzen Embedded X100 breaks down the memory barrier. With its unified, zero-copy memory architecture, the CPU, GPU, and NPU all work from the same space, backed by 144 MB of cache. With up to 128 GB of LPDDR5x-8533 with ECC on a 256-bit bus, the X100 can run models with 200B+ parameters. A workload can be split across all three engines: GPU for large vision and vision-language models; NPU for always-on detection, and CPU for planning and control.

x86 (HV2)

AMD x86 Embedded

The new standard in embedded innovation.