Custom Meta Tags

EBV - Solutions - Markets - Transportation and Hirel Animated HB Static HTML

EBV - Automotive NEW Sub Navigation

EBV - Transportation - Glossary AEC Introduction (LC)

Glossary - AEC

As experts in automotive market, EBV can help you to recognise the most common terms and abbreviations in the areas of AEC, Functional safety and Telematics:

EBV - Transportation - Glossary - AEC Static HTML

5 Why

 

Based on the Ishikawa diagram analysis the 5 Whys is a questions-asking method used to explore the cause/effect relationships underlying a particular problem. Ultimately, the goal of applying the 5 Whys method is todetermine a root cause of a defect or problem.  Ishikawa Diagrams might be known as: Pareto, fishbone diagrams, cause-and-effect diagrams orFishikawa

 

6 Sigma

 

refers to a quality improvement and business strategy concept started by Motorola in the United States in 1987.  In statistical terms, 6-Sigma is the abbreviated form of 6 standard deviations from the mean, which mathematically translates to about 2 defects per billion.  Thus, strictly speaking, your process is said to have achieved 6-sigma if it is producing no more than 2 defects per billion parts produced. Nowadays replaced by (or part of) Zero defect tolerance strategies.

 

ABUS

 

“ AutomobileBitserielleSchnittstelle“ VW (Toshiba/ TEG) -Busstandard (replaced by CAN)

 

AEC – Q101

 

only ‚discrete‘ semiconductor parts f.ex.: Transistors, Diodes...

 

AEC – Q2xx

 

only for passive and E-Mech. parts f.ex.: Capacitors / Resistors and some sensors

 

AEC – Qxxx

 

Specification how to qualify electronic parts

 

AEC-Q100

 

An automotive quality standard that outlines the stress test for IC qualification in automobiles. Altera is an active member of the AEC council, which governs this standard.

 

AUTOSAR

 

Automotive System Architecture consortium was established to define an open standard for automotive E/E architecture. It serves as a basic infrastructure for the management of functions within both future applications and standard software modules.

 

CAN

 

Car Area Network by Bosch (Intel / NXP) max 1Mbaud ISO 11898-1:2003 Road vehicles — Part 1: Data link layer and physical signallingISO 11898-2:2003 Road vehicles — Part 2: High-speed medium access unitISO 11898-3:2006 Road vehicles — Part 3: Low-speed, fault-tolerant, medium dependent interfaceISO 11898-4:2004 Road vehicles — Part 4: Time-triggered communicationISO 11898-5:2007 Road vehicles — Part 5: High-speed medium access unit with low-power modeISO/NP 11898-6 Road vehicles — Part 6: High-speed medium access unit with selective wake-up functionality “Partional Networking”

 

Commercial vehicle operations (CVO)

 

CVO is the application of intelligent transportation system technology to commercial vehicles.

 

ELV

 

End of Life Vehicle  The initial Directive 2000/53/EC of the European Parliament and the Council of 18 September 2000 regulates the recycling of motor vehicles within the European Union (EU).(following regulations see GADSL)

 

IDB-1394

 

An in-vehicle network protocol designed for high-speed multimedia applications that require large amounts of information to be moved quickly on a vehicle. Previously known as IDB-M, IDB-1394 is built on the IEEE-1394 standard.

 

IDB-C

 

An in-vehicle network defined in the SAE J2366 - ITS data bus specifications series. IDB-C is based on CAN 2.0B (controller area network) silicon and physical layer, specifically on SAE J2284 - high-speed CAN.

 

IEC61508

 

IEC61508“This International Standard covers those aspects to be considered when electrical/electronic/programmable electronic (E/E/PE) systems are used to carry out safety functions. A major objective of this standard is to facilitate the development of application sector international standards [ … ] A dual objective of this standard is to enable the development of E/E/PE safety-related systems where application sector international standards do not exist.”  -> applicable for all vehicles esp. those >3,5 t

 

IEEE

 

Institute of Electrical and Electronics Engineers, Inc.; a professional society and standards-making body.

 

ISO

 

International Standards Organization.

 

ISO / TS16949*

 

Reunification of all requirements in a quality management system of European and American automobile industry. Valid only for production processes. (replaces the QS9000).*(ISO – International Standardization Organization TS- Technical Specification)

 

 

ISO 9141

 

or known as K&L-Line (ISO 9141-2 or ISO14230-4)          Lowspeed 1 or 2 wire communication interface used for OBD and OBDII

 

ISO Bus

 

ISO 11783 (or ISO Bus or ISOBUS) is a communication protocol for the agriculture industry based on the SAE J1939 protocol (which includes CANbus) . It is managed by the ISOBUS group in VDMA

 

ISO/IEC 15504

 

(Spice- SoftwareProcess Improvement and Capability Determination)Q-System for software development

 

ISO26262

 

“ISO 26262 is intended to be applied to safety-related systems that include one or more E/E systems and that are installed in series production passenger cars with a max gross weight up to 3,5 t.[…]”

 

J1850

 

Delco / GM / Ford –Bussystem (US Standard - new applications addressed with CAN)

 

JASPAR

 

Japan Automotive Software Platform Architecture consortium was created by Japanese OEMs to define an open architectural platform, whereby making it easier for all the suppliers and OEMs to develop the next-generation system architecture.

 

Kaizen

 

a Japanese term that basically translates to 'continuous improvement' or 'change to become good', is a management concept originated by the Japanese in order to continuously effect incremental changes for the better, involving everybody within the organization from workers to managers. Kaizen is aimed at producing more and more value with less and less wastes (higher efficiency), attaining better working environment, and developing stable processes by standardization.

 

Media oriented system transport (MOST)

 

A versatile, high-performance and low-cost multimedia network technology based on synchronous data communication. It is ideal for multimedia applications such as audio, video, navigation, and communication in the automotive sector.

 

OEM

 

Origin equipment manufacturer = Car maker = Car Manufacturer

 

Open Alliance

 

Automotive Alliance - enable wide scale adoption of Ethernet-based automotive connectivity, establish industry standards for Ethernet connectivity over single pair, unshielded cable and enable the migration from multiple closed applications to an open, scalable Ethernet-based network.

 

OSEK/VDX

 

An operating system, communication and network management specification developed by automotive industry companies. OSEK/VDX was created as a joint project in the German and French automotive industry aimed at an industry standard for an open-ended architecture for distributed control units in vehicles.

 

PALMNET

 

Japanese trial of a standard

 

Poka-Yoke

 

Mistake proofing is a quality management concept developed by a Matsushita manufacturing engineer to prevent human errors from occurring in the production line.Poka yoke (pronounced “poh-kahyoh-kay”) comes from two Japanese words – “yokeru” which means “to avoid”, and “poka” which means “inadvertent errors. The main objective of poke yoke is to achieve zero defects

 

PPAP

 

Level 1 Part Submission Warrant (PSW) only. Level 2 PSW with product samples and other items requested. Level 3 PSW with product samples and complete supporting data. -> Most used format (w/o NDA) Level 4 PSW and other items requested.Level 5 PSW with product samples and complete supporting data available for review at the manufacturer.

 

Production part approval process (PPAP)

 

PPAP, 3rd edition, Automotive Industry Action Group (AIAG) is one of the key requirements for the automotive industry. A PPAP document outlines all the manufacturing quality processes that an integrated circuit (IC) manufacturer undertakes for a specific device.

 

PSI5

 

Peripheral Sensor Interface 5 - used forsatelite sensorsf.ex acceleration Sensors in Airbag systems

 

PSW

 

Part Submission Warrant Beside the testing of the sampled parts the PSW is the basic document for the initial sampling procedure. The PSW is equal to a commitment from customer to release the product ant the intention to use it. Comment: if a customer accepts the sampling with sending back the PSW we (the supplier) needs to confirm every change in the process.(ACN / PCN / PDN must be sent out in time)

 

SAE

 

Society of Automotive Engineers.

 

SENT

 

Single Edge Nibble Transmission - Communication protocol for point to point direct comunications with sensors e.q. Hall effects

 

Society of Automotive Engineers (SAE)

 

A one-stop resource for technical information and expertise used in designing, building, maintaining and operating self-propelled vehicles for use on land or sea, in air or space.

 

The 8 disciplines

 

4D could be a proper format for Interrim Reports or Final Reports whenever no PCA's could be applied

 

Tier

 

Supplier (Ranked by 1(direct System supplier) / 2 (indirect or subsystem supplier) / 3 (development company or module manufacturer))

 

TPM

 

Total Productive Maintenance  is a maintenance process developed for improving productivity by making processes more reliable and less wasteful

 

TQM

 

Total Quality Management TQM tries to improve quality by ensuring conformance to internal requirements, while Six Sigma focuses on improving quality by reducing the number of defects and impurities

 

TS16949

 

ISO/TS 16949:2002 is an ISO technical specification, which aligns existing American (QS-9000), German (VDA6.1), French (EAQF), and Italian (AVSQ) automotive quality systems standards within the global automotive industry, with the aim of eliminating the need for multiple certifications to satisfy multiple customer requirements.

 

Umbrella Specification

 

Material content data can be captured by forming cross-company product groups with typical values. These material data sheets, so-called umbrella specifications, greatly simplify the declaration without any noticeable loss of accuracy. only Infineon and NXP working on this level using Umbrella Specs as MCDS

 

V-Methode Analysis / Synthesis

 

Method for fast turnaround development of automotive systems

 

VAN

 

Vehicle Area Network PSA / Renault – Bus standard (replaced by CAN)

 

VDA

 

"Verband der Deutschen Automobilindustrie" Equivalent to AEC the German Council for standardization of automotive procedures / processes and Market requirements