Custom Meta Tags

EBV - Solutions - Markets - Transportation and Hirel Animated HB Static HTML

EBV - Automotive NEW Sub Navigation

EBV - Transportation - Body and Comfort Main Title

Body & Comfort – Creating a Pleasant Environment

EBV - Transportation - Body and Comfort Intro (MM)

With people spending a considerable amount of time in vehicles each week, having an in-cabin environment that is enjoyable to be situated in is paramount. Automobile manufacturers fully recognise this as a differentiator, with a great deal of engineering effort being invested into it.

EBV - Transportation - Body and Comfort Accordion Static HTML

Controlling the Infotainment System With Gestures

The breadth of infotainment equipment being included in vehicle designs is now staggering - all calling for advanced multimedia technology.

In addition to their operation, providing an effective means of control is important. Over the last 15 years, there has been a shift away from using buttons, switches and dials, with these being replaced by touch displays. As these can still, however, present a distraction for drivers, there is increasing interest in HMIs that require less attention and do not call for drivers to take their eyes off the road. ToF will allow simple gesture recognition to be conducted, so the sound system's volume can be adjusted, a different radio station picked, or a phone call initiated - all without the driver’s attention needing to be averted.

 

Building a Bridge Between Audio and Video

Part of the TSN family of protocols (actually preceding them, in fact) is audio video bridging (AVB).

This is being widely incorporated into vehicle infotainment systems where Ethernet communication is in use, so as to provide the necessary synchronisation to audio and video streams. Since Ethernet does not normally support deterministic operation, ABV is needed to ensure that the different multimedia endpoints are kept in time with one another. Take the speakers in a vehicle’s sound system as an example; without the determinism that ABV provides to the Ethernet infrastructure, the output from different speakers would be out of synch - leading to poorer audio quality being experienced.

 

The Smartphone as a Human Machine Interface

Bluetooth pairing means that that a car can access information from a user’s smartphone, so that personal preferences can be applied, such as seat positioning, ambient lighting, or musical taste.

This will be of particular value as we move into an era of autonomous vehicles being a pooled resource, with people ordering one to pick them up as required.

 

Storage Capacity for Tomorrow's Smart Vehicles

Greater infotainment capabilities, along with increased use of sensors for autonomous driving, AI-based processing and new in-vehicle networking architectures will lead to cars soon needing to store TBytes worth of data.

This will mandate inclusion of high integrity DDR3, DDR4 and DDR5 memory resources. DDR5 is becoming the standard in vehicles, offering higher bandwidth with lower power consumption to support AI-driven applications and edge computing. Already on the horizon is DDR6: with base speeds of 17,600 MT/s, extended memory channels, and even greater energy efficiency, it will further revolutionize data processing in the automotive industry. Another important trend in automotive storage is the integration of advanced solutions that enable the faster processing of vehicle data, particularly for autonomous driving systems. Such systems require rapid access to substantial data sets to support decision-making processes, and eMMC and UFS storage solutions provide the necessary density, resilience and high read/write speeds. Today, eMMC is often integrated with energy-saving DRAM components within a single, compact multi-chip package (MCP), which reduces the overall size and simplifies the development process while ultimately lowering costs.

 

A Variety of Applications for Magnetic Sensors

Magnetic sensors are pivotal in enhancing vehicle comfort levels.

They provide occupants with the ability to adjust seating, as well as supporting the operation of climate control systems, contributing to the stabilisation systems used to ensure a smooth ride and being an integral part of window and sunroof opening/closing mechanisms.

Take a look at the full range of products and services offered by EBV to make your designs more comfortable and ensure that the driving experience is satisfying. This includes microprocessors, memories, communication ICs, ToF sensors, microphones, and magnetic sensors.

 

Shared Contact EBV (GBL)

Do you have a Question?

Contact EBV

If you need any assistance, please click below to find your closest EBV sales office.

Locations_EBV-SharePoint-CTA-768x432

EBV - Transportation - AES Transportation (GBL)

All Electric Society

Powering the Future of Transportation

Explore semiconductor solutions for EVs, charging infrastructure, battery management and intelligent mobility systems.

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.

EBV - Automotive - Related NPI Static HTML