Custom Meta Tags

EBV - Solutions - Markets - Transportation and Hirel Animated HB Static HTML

EBV - Automotive NEW Sub Navigation

EBV - Transportation - Zonal Architecture - Title Static HTML

Zonal Architecture – The Electronic/Electrical System for the Vehicles of Tomorrow

EBV - Transportation - Zonal Architecture Intro (MM)

With electromobility, automated driving functions, and consumers’ desire for personalised driving experiences including modern infotainment, more and more electronics and functions are finding their way into vehicles. The integration of advanced technologies and the growing number of electronic systems are increasing the complexity of the electronic/electrical (E/E) architecture. At the same time, customers expect vehicle functions to be updated conveniently and securely over the air throughout the vehicle’s lifetime.

EBV - Transportation - Zonal Architecture Accordion Static HTML

From Domain-Specific to Zonal Architecture

In traditional E/E architectures, each function (brakes, lighting, infotainment, etc.) is managed by its own ECU, complete with software and wiring.

Over time, this has resulted in an increasingly complex network of more than 100 ECUs in a single vehicle. With the so-called zonal architecture, this complexity can be significantly reduced. The key lies in the shift from a logical transformation into a scalable and centralized Software Development to build the bridge to perform OTA updates for a Software Defined Vehicle and a physical transformation with an outcome of zonal aggregation and ECU clustering. For instance, these zone controllers are installed in the edge areas of the vehicle and manage the devices within their respective zones, such as front- and rear lighting, actuators, suspension and doorsystems . Instead of each component running its own software, the zone controller acts as a hub, responsible for power distribution and data communication. The zone controllers are connected to a central high-performance computer that manages the different vehicle functions – while the zone controllers execute them. This shift replaces hundreds of point-to-point cables with a simpler, more manageable zonal layout. As a result, weight optimization, design clarity and system efficiency are significantly improved to build up real time processes, on time over the air updates to secure the system.

 

The Benefits of a Zonal E/E Architecture

The zonal architecture offers advantages for vehicle development, production, and operation alike:

up to 20% fewer embedded control units, plus up to 10% savings in material and wiring-harness weight

  • Reduced complexity and lower weight of the wiring harness
  • Lower material and assembly costs
  • Improved scalability – new functions can be added or modified via software
  • Simplified development and over-the-air (OTA) updates thanks to centralised software control
  • Easier coordination of functions – the central computer issues a single command, executed by the relevant zone controllers

 

Innovation Driving Zonal Architectures

The transition to zonal architectures is driving new technical solutions across a wide range of areas.

Ethernet as the Central Communication Standard

For seamless, cross-functional data exchange between zones, robust and high-speed communication networks are essential. These include multi-gigabit Ethernet and SerDes (serializer/deserializer) applications, capable of transferring the huge volumes of real-time data generated by modern sensors, cameras, and radar/lidar systems. However, maximum data rates are not always required: CAN/CAN FD and CAN XL transmits up to 20 Mbit/s, sufficient for connecting low-bandwidth devices such as headlights, indicators, or door locks. The standard utilizes the mature bus communication ecosystem – including time synchronisation and error correction – but without the overhead of higher-speed Ethernet, such as 100BASE-T1 or gigabit Ethernet.

Transition to 48 V Architectures

Moving from traditional 12 V systems to 48 V architectures reduces current levels, minimises resistive losses, and improves overall efficiency in power distribution. This enables better thermal management and supports scalable high-performance computing platforms, in line with the requirements of SDVs and electrification.

Smart Switches in Power Distribution

Zone controllers do not just route data; they also distribute power to the components in their zones. They therefore play a critical role in system safety and diagnostics. Smart switches provide far more than basic circuit protection. They allow for voltage and current monitoring on every channel, support safety standards such as ASIL B and ASIL D, and offer fail-safe and fail-operational modes. Even in case of faults, the function can be maintained. For example, in the event of a malfunction, a smart switch can reduce power, isolate the fault, or switch to a safe fallback mode instead of completely shutting down critical systems such as headlights. This level of transparency and control is essential for higher levels of automated driving.

 

New Cybersecurity Concepts for Zonal Architectures

Zonal E/E architectures also mean that the physical separation of different systems within the vehicle disappears.

To effectively prevent cyberattacks, new software-level security measures must be implemented. High-performance firmware for hardware security modules anchors security functions directly onto the chips of vehicle computers and zone controllers, according to ISO 26262 safety- and ISO/FAE 21343 security standards. Automotive-specific post-quantum cryptography already provides protection today against future threats posed by quantum computing.

EBV’s portfolio includes solutions for both zone controllers and central vehicle computers from leading manufacturers. Systems for automotive connectivity, ADAS, and in-vehicle infotainment complete the offering.

 

Shared Contact EBV (GBL)

Do you have a Question?

Contact EBV

If you need any assistance, please click below to find your closest EBV sales office.

Locations_EBV-SharePoint-CTA-768x432

EBV - Transportation - AES Transportation (GBL)

All Electric Society

Powering the Future of Transportation

Explore semiconductor solutions for EVs, charging infrastructure, battery management and intelligent mobility systems.

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.

EBV - Automotive - Related NPI Static HTML