Custom Meta Tags

EBV - Solutions - Markets - Transportation and Hirel Animated HB Static HTML

EBV - Automotive NEW Sub Navigation

EBV - Transportation Power Main Title

Power – Drive Systems in a Phase of Transition

EBV - Transportation - Power Intro (MM)

We are in the midst of a transformation in mobility – away from combustion engines and toward electric powertrains. However, this is a process that takes time. According to the International Energy Agency, sales of electric cars grew by 20% in 2025 to exceed 20 million units worldwide, meaning that a quarter of all new cars sold were electric. However, this also means that vehicles with combustion engines still have the largest market share, both now and in the foreseeable future. Therefore, the powertrains of automobiles today still need to be divided into two different types. There are the traditional ICE vehicles, which currently still represent the larger proportion of vehicles on the road. Then there are the EVs, which are increasing in number every year, and where the majority of engineering focus is now placed as the shift from ICEs continues over the course of the next decade.

EBV - Transportation - Power Description Static HTML

The Three Key Elements of the Electric Powertrain

Innovations in this field will transform our driving experience, energy usage and energy integration.

Breakthroughs in vehicles and batteries, the expansion of charging infrastructure, and the integration of renewable energies will all contribute to the rapid evolution of the electric vehicle industry.

The Three Key Elements to an EV’s Powertrain:

  • The on-board charger (OBC) – This takes the current from the AC mains (coming from a residential block, office or street-based charging point) and converts it into DC. This DC current is then used to charge the battery. When fast charging (from a charging roadside station) is being carried out, the OBC does not need to be involved. Here the current can be supplied straight to the battery.
  • The battery management system (BMS) – This is responsible for looking after the Li-ion battery. It must ensure that the battery operates in a way that ensures the longest possible working lifespan and the conditions that it is running at are maintained within optimal margins, the cell loads being balanced accordingly. Via sensors situated on individual battery cells, it can monitor the temperature levels and other parameters. This will safeguard against the prospect of thermal runaway or other problems occurring.
  • The inverter – This has the job of using the charged energy in the battery to propel the EV’s traction motor, as well as controlling its rotational speed. Though the energy stored in the battery is in a DC form, it needs to be converted back into AC before it reaches the motor.

 

WBG Technology is Going to be Pivotal in Future OBC Designs

In order to utilise the available charging current as effectively as possible, the OBCs placed in EVs need to support high efficiency operation.

This will also mean that there is less wasted energy turned into heat, so the cost involved and space taken up by thermal management will both be lowered. At the same time, there is increasing pressure to increase the power densities of OBCs. That will allow their contribution to the overall weight of the vehicle to be reduced, enabling greater distances to be travelled on the stored charge. The higher temperature-withstand levels, elevated voltage capabilities, and faster switching speeds that WBG technology is able to support are going to be pivotal in future OBC designs – enabling more efficient, robust and compact solutions. The need to downsize EVs’ inverters and boost their operational efficiency (through mitigating switching losses) are very similarly apparent. Once again, it will be the use of WBG that will be the foundation for this.

 

Smarter BMS Enable Better Battery protection

The BMS technology being incorporated into the new breed of EVs will call for more advanced sensors.

These will have higher resolutions, so that temperature and current fluctuations can be more accurately determined, as well as increased responsiveness, in order that arising situations can be addressed at the earliest stage, before damage is done to the vehicle or the occupants put in any danger. The speed of the supporting communication infrastructure will need to be increased too.

 

Faster Charging

Much of the progress made in electric vehicles can be attributed to innovative battery technology.

In 2025, according to the Eurostat study "Digitalisation in Europe", more than a third of people in the EU (35%) used generative AI tools.

For example, advances in battery chemistry and charging infrastructure have significantly reduced charging times. Many of today's electric vehicles can be charged to 80% of their capacity within half an hour and even faster with a solid state battery using a direct current fast charger. However, the charging infrastructure still needs to be expanded further – and as quickly as possible. This is a huge market that offers equally huge opportunities for companies that manufacture and distribute charging solutions.

At EBV Elektronik, together with our sister companies Avnet Abacus and Avnet Embedded, we support manufacturers with everything they need for their charging solutions: from suitable hardware and software modules to the necessary charging cables and connectors to specific cloud solutions. This end-to-end solution significantly reduces time to market – the best starting position for securing market share in this rapidly growing industry. Find out more about our one-stop shop for the development of charging infrastructure here.

 

Shared Contact EBV (GBL)

Do you have a Question?

Contact EBV

If you need any assistance, please click below to find your closest EBV sales office.

Locations_EBV-SharePoint-CTA-768x432

EBV - Transportation - AES Transportation (GBL)

All Electric Society

Powering the Future of Transportation

Explore semiconductor solutions for EVs, charging infrastructure, battery management and intelligent mobility systems.

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.

EBV - Automotive - Related NPI Static HTML