The robotics industry faces a structural growth surge: Mordor Intelligence estimates the global market volume for 2026 at US$88.27 billion and forecasts a rise to US$218.56 billion by 2031. That corresponds to an average annual growth rate of 19.86 per cent. At the same time, the technological focus is shifting from rigidly programmed individual applications towards flexible, connected systems capable of learning.
The International Federation of Robotics (IFR) sees artificial intelligence and autonomous robotics in particular as central trends for 2026. Analytical AI can evaluate large volumes of data, recognise patterns and, for example, predict maintenance needs or optimise routes and resources in intralogistics. Generative AI also opens up new forms of human-robot interaction, for instance via natural language and gestures, and supports the learning of new tasks as well as the creation of training data in simulated environments. The next development step is considered to be agentic AI: it combines structured decision logic with the adaptability of generative models, so that robots can act more independently even in complex real-world environments. This requires close integration of information technology (IT) and operational technology (OT). Real-time exchange between data processing, sensors and physical control makes robots more versatile and creates the basis for data-driven Industry 4.0 applications. Humanoid robots are also moving from the prototype stage towards practical trials, initially above all in automotive production, warehousing and manufacturing. However, they have to prove their industrial value through high reliability, short cycle times, low energy consumption and predictable maintenance costs. In parallel, functional safety and cybersecurity are gaining importance. Cloud-connected, AI-supported robots need traceable decision processes, clear liability rules, robust access concepts and the protection of sensitive video, audio and sensor data.
Let's talk
Better connected through LinkedIn
Get directly in touch with our Industrial Director Andrej Orel


The five most important robotics trends (source: IFR)
The technological basis for almost all current robotics trends
Semiconductors form the technological basis for almost all current robotics trends, from autonomous AI and IT/OT convergence to safe humanoid systems. AI accelerators and edge processors enable autonomous decisions with low latency. Advanced sensors improve environmental and touch perception. SiC and GaN devices increase the efficiency of drives and power supplies. Chiplets, 3D packaging and secure microcontrollers create compact, powerful and connected robot systems.
SoC architectures make robots more autonomous and more responsive
AI-optimised edge processors and modern SoC architectures make machines faster, more autonomous and more responsive. Particularly important here are energy-efficient computing solutions that evaluate image and sensor data directly in the device and thus make real-time applications reliably possible in the first place.
In robotics, AI-optimised edge processors and SoC architectures handle the local evaluation of sensor, image and motion data directly in the system. This makes robots faster, more autonomous and more responsive, because latency falls and cloud connections become less critical.
The most important trends include specialised AI accelerators in the chip, stronger integration of CPU, GPU, NPU and image processing in a single SoC, and energy-efficient designs for mobile and collaborative robots. Added to this are more compact form factors, higher memory bandwidth and optimisations for real-time inference, for example for navigation, object recognition and quality inspection. In parallel, the term “physical AI” is gaining weight, because AI works directly in machines, vehicles and robots as part of the control logic.
In semiconductor technology, three developments are particularly relevant: advanced packaging processes that enable more computing power in a small area, a stronger focus on energy efficiency, and closer coupling of computing and sensor systems. For robotics applications, what is decisive is therefore less the maximum peak performance than the ability to run AI robustly, economically and in real time at the edge of the network.
Find out about our comprehensive portfolio for high-performance computing (HPC), from MCUs and MPUs to embedded processors with integrated AI accelerators.
GaN/SiC: new possibilities for mobile and humanoid robots
In robotics, compact and efficient drives determine the agility, range and performance of the systems. Wide-bandgap power semiconductors such as GaN and SiC are regarded as key technologies for the next generation of robust, highly dynamic robot drives.
Wide-bandgap power semiconductors, in particular gallium nitride (GaN) and silicon carbide (SiC), enable compact, highly dynamic and energy-efficient drives. Thanks to their higher switching frequencies and lower losses compared with classic silicon, motors and gearboxes can be built smaller, which is particularly decisive for mobile, collaborative or humanoid robots.
The most important trends include the integration of GaN-based drivers directly into joint modules, the increase in power density through higher voltages (up to 800 V and more), and the combination with advanced cooling concepts and Ethernet-based real-time communication architectures. In parallel, SiC solutions are gaining importance where high continuous loads and thermal robustness are required, for example in heavy industrial robots or automated guided vehicles.
Particularly relevant at present is the further development of GaN HEMTs and SiC MOSFETs with lower switching losses, improved EMC properties and higher reliability under dynamic load changes. In addition, new packaging technologies and system-in-package integration are driving miniaturisation, while at the same time the cost per watt is falling, a decisive factor for series readiness in robotics.
Find out more about EBV’s offering in the field of SiC and GaN power electronics.
Semiconductor miniaturisation enables the next generation of safe robots with real-time 3D perception
Highly integrated sensor technology and 3D imaging are what makecollaborative and humanoid robots truly fit for use. Multimodal sensor fusion, safety-certified 3D ultrasonic and lidar systems, and miniaturised semiconductor solutions open up new fields of application for robotics.
Highly integrated, safe sensor technology , including 3D imaging, forms the technological backbone of modern robotics. It enables machines to capture their environment precisely, detect obstacles and interact safely with people. Without such sensor systems, neither the sensitive control of robot arms nor the autonomous navigation of humanoid platforms in dynamic environments would be conceivable.
Current trends include the fusion of multimodal sensor data from lidar, time-of-flight cameras, radar and tactile sensors in order to create real-time 3D models of the environment. Safety-certified 3D ultrasonic sensors are also increasingly used, reliably detecting people even in poor lighting conditions and meeting standards such as IEC 61496 or ISO 13849. In parallel, optical force-torque sensors and infrared-based depth-sensing systems are gaining importance in order to ensure intuitive human-robot interaction and collision-free movements.
In semiconductor technology, development is driven above all by miniaturised, energy-efficient image sensors with integrated on-chip signal processing. New CMOS technologies enable higher resolutions with lower latency, which is decisive for safety-critical applications. Specialised ASICs and edge-AI chips that pre-process sensor data directly and thus reduce the computing load on central controls are also gaining relevance. These advances make robots not only safer, but also more compact and more economical to use.
EBV’s portfolio offers you the right sensors for your requirements from the world’s leading manufacturers.
Ethernet/TSN and power line: how the neural backbone of modern robot systems is created
Ethernet/TSN and power line communication are becoming a key factor for the next generation of robots: they enable deterministic real-time communication, which is what makes precise movements, safe human-robot collaboration and seamless cloud connection possible in the first place. The following overview shows the most important technology trends and highlights which semiconductor innovations are currently driving this development.
Connected real-time data architectures based on Ethernet/TSN (Time-Sensitive Networking) and power line communication (PLC) form the neural backbone of modern robot systems: they enable deterministic, synchronised data streams between sensors, actuators and controls, and thus precise movement sequences, collaborative scenarios and seamless integration into higher-level IT and cloud systems. The most important technology trends are the convergence of wired TSN with mobile 5G networks for hybrid, real-time capable architectures, the use of standardised Ethernet hardware instead of proprietary solutions, and the integration of OPC UA over TSN for vendor-neutral interoperability. In parallel, PLC is gaining importance where additional cabling is uneconomical, for example in retrofittable or rotating robot components.
In semiconductor technology, three developments are currently driving adoption: first, integrated TSN-capable Ethernet controllers in SoCs and microcontrollers that implement real-time functions directly in the chip. Second, energy-efficient, highly integrated PLC modems with a small footprint for compact robot joints. Third, hardware-accelerated time-stamping and synchronisation logic (IEEE 802.1AS), which ensures sub-microsecond accuracy even under high network load, a basic prerequisite for multi-robot coordination and digital twins.
Find out more about EBV’s TSN solutions.
Root of trust will protect robots against attacks and manipulation directly in the hardware
Quantum-resistant hardware security is developing into a central prerequisite in robotics, so that autonomous systems remain reliably protected against manipulation, espionage and attacks in future too. The root of trust in particular is coming into focus, because it secures identity, integrity and trusted updates directly in the hardware.
Quantum-resistant hardware security and an anchored root of trust are becoming the security foundation in robotics: they protect the identity, firmware and update paths of connected robots against manipulation, supply chain risks and future attacks using quantum computers. In practice, the focus is shifting from pure software security towards hardware-supported trust, because autonomous systems are increasingly coupled with the cloud, the edge and industrial networks.
The most important trends include post-quantum cryptography for signatures and key exchange, secure boot chains, hardware-based attestation, and the integration of TPMs, secure elements and HSM-like functions directly into controls and sensors. In parallel, zero-trust architectures, identity management for machines and the protection of over-the-air updates are gaining importance, because robots are operated over long lifecycles and extended regularly.
For semiconductor technology, three developments are particularly relevant: specialised security controllers, more cryptographic functions on chip, and application-oriented quantum security at silicon level. Manufacturers are working to integrate root-of-trust mechanisms directly into microcontrollers, SoCs and secure elements in order to reduce latency and shrink attack surfaces.
Explore EBV’s solutions around hardware-based security.
Solutions
EBV Embedded Solutions
We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

Resources
EBV Podcast
Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.