Custom Meta Tags

EBV - Markets - Industrial Animated HB Static HTML

Custom Meta Tags

EBV - Industry and Energy - Factory automation Main Title (MT)

Factory automation

EBV - Industry and Energy - Intro Mixed Media (MM)

Factory automation is increasingly developing into connected, data-driven production systems in which real-time monitoring, direct data access and high process quality work closely together. IIoT, HMI, edge computing, cybersecurity, predictive maintenance and digital twins are growing together into an integrated architecture that creates transparency, reduces downtime and at the same time supports safety and regulatory requirements.

A defining feature of current solutions is the shift of data processing and control closer to the machine. Edge-based architectures reduce latency and improve responsiveness, while digital twins use live data to enable robust simulations and predictive maintenance. Combined with IIoT and AI applications, unplanned outages can be reduced and maintenance processes planned better. Factory automation is thus developing from pure monitoring into a system that detects conditions early and continuously optimises workflows.

Industrial Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our Industrial Director Andrej Orel

EBV - Industry and Energy - Factory Automation Technologies Static HTML

At the same time, HMI solutions are gaining importance, presenting complex production data clearly through intuitive interfaces and powerful graphics engines. Modern visualisation supports not only maintenance and operation, but also rapid responses to quality deviations, safety events or load peaks. Via connected drives and systems, operating data such as speed, torque, current and temperature is captured continuously and made usable for process optimisation and condition-based maintenance.
 

Semiconductor technologies are the core of smart factories 

Semiconductors form the technological basis of this development. They enable capable sensor technology, precise signal processing, fast communication, efficient motor control and secure data processing at the edge of the network. Whether microcontrollers, power semiconductors, memory devices or connectivity ICs: only these create the conditions for machines to capture, analyse and securely pass on data in real time. In factory automation, semiconductors are therefore not just components, but central enablers for connectivity, miniaturisation, energy efficiency and industrial resilience.

Working with EBV allows industrial application areas to be opened up and assessed technically in a targeted way. Our specialists help you keep track of developments and identify the solutions with the greatest potential, from production safety and automation through miniaturisation and connectivity to scalable system architectures.

Factory-automation-graphic

The pillars of a smart factory (source: LightGuide)

 

EBV - Industry and Energy - Factory Automation - Accordion Static HTML

More diagnostics, redundancy and security: semiconductors strengthen functional safety

Functional safety is a central prerequisite for the reliable operation of modern factory automation. The key standard here is IEC 61508; the implementation of safety-critical functions is supported by current semiconductor solutions.

As an international basic standard, IEC 61508 provides the framework for the functional safety of electrical, electronic and programmable systems in factory automation. It covers the entire safety lifecycle, from risk analysis through development to operation and maintenance, and thus supports the design of sensors, controls and actuators for defined Safety Integrity Levels (SIL). Several trends are emerging in semiconductor solutions: microcontrollers and systems-on-chip integrate more capable diagnostic functions, redundancy and safe monitoring units. At the same time, specialised safety microcontrollers with lockstep cores, error correction and integrated self-tests are gaining importance. The increasing connectivity of machines is also driving secure industrial Ethernet interfaces and security functions, as cybersecurity and functional safety move closer together. In parallel, certified software libraries, operating systems and development tools make standard-compliant implementation easier. Artificial intelligence and edge computing are being used increasingly, but they pose new challenges for safety evidence. The announced third edition of IEC 61508 therefore addresses IoT, AI and complex semiconductor architectures more strongly, among other things.

Find out more about EBV’s broad portfolio of microcontrollers, digital ICs and sensors, all of which comply with IEC 61508.

 

Semiconductor solutions strengthen the security of connected production plants

Cybersecurity is increasingly becoming a strategic success factor in factory automation: the more closely plants, machines and sensors are connected, the more important their protection against manipulation, failures and data misuse becomes. Against this background, the focus is shifting to semiconductor solutions that move security functions directly into the hardware, creating robust foundations for connected production.

Cybersecurity in factory automation has long since ceased to be a purely IT topic; it is a basic prerequisite for stable processes, secure remote maintenance and the protection of connected production plants against manipulation, failures and sabotage. Security functions are increasingly being considered directly in architecture, development and integration; this includes security by design, segmented OT/IT networks, continuous monitoring and AI-supported anomaly detection. Hardware-based protection concepts that secure authenticity and integrity at component level are also particularly relevant. This means that secure element chips are gaining importance: they serve as a trusted root for identities, store key material in a tamper-protected way and support secure authentication of machines, sensors and gateways. The trend here is towards smaller, energy-efficient and more easily integrable devices that fit seamlessly into industrial IoT and edge environments. Cybersecurity in factory automation is thus shifting increasingly from retrofitted protection to an embedded system property.

Explore EBV’s solutions around hardware-based security.

 

AI semiconductors make factory automation faster, more precise and lower-maintenance

AI-supported process control and predictive maintenance are becoming central levers in factory automation for greater efficiency, availability and process stability. Semiconductor solutions are increasingly bringing AI functions directly to the plant, so that data can be evaluated in real time and failures detected earlier.

The use of AI in process control and predictive maintenance is increasingly becoming the link between real-time data, stable processes and falling downtime costs. The current trend is towards semiconductor solutions that bring AI functions closer to the machine: edge TPUs accelerate specialised inference directly at the edge of the network, NPUs handle more complex models in industrial PCs, gateways and embedded systems, and modern MCUs integrate AI elements for energy-efficient condition monitoring in sensors and actuators.

Particularly important here is the shift of analysis and decision-making into production itself, in order to reduce latency and avoid having to send data streams to the cloud permanently. At the same time, requirements are growing for robust connectivity, interoperability and cyber-resilient architectures, so that AI-supported control becomes not only faster but also more reliable. In practice, this means more predictive maintenance, more precise process management and higher plant availability with lower energy and service costs at the same time.

Find out about our comprehensive portfolio for high-performance computing (HPC), from MCUs and MPUs to embedded processors with integrated AI accelerators.

 

Wide-bandgap semiconductors enable a leap in efficiency in industrial automation

Energy efficiency in factory automation has long been more than a cost issue; it is becoming a central competitive factor. In drives and power electronics in particular, the focus is shifting to technologies that enable higher efficiency, more compact designs and lower losses.

Rising energy costs, stricter climate targets and pressure for higher productivity are bringing the topic of energy efficiency ever more into focus in industrial manufacturing. WBG semiconductors such as SiC and GaN are therefore gaining importance, as they make drives, power supplies and converters more efficient, more compact and thermally more robust than classic silicon solutions. In practice they mainly enable energy-efficient motor drives, higher switching frequencies, smaller cooling and passive components, and better power density. Important technology trends currently include the increased use of SiC in powerful, high-voltage drives, the growing use of GaN in compact, high-frequency part-load and auxiliary systems, and integration into modular, scalable drive concepts. In addition, there is a clear trend towards greater system efficiency along the entire automation chain, from the power supply to the servo drive.

Find out more about EBV’s offering in the field of SiC and GaN power electronics.

 

IO-Link and integrated intelligence are changing sensor technology in the factory

Sensors provide the data basis for precise control, quality assurance and efficient processes. In particular, intelligent sensors with integrated microcontroller electronics and digital communication via IO-Link are shaping the connected production of today and tomorrow.

Sensors are the sensory organs of factory automation: they capture physical quantities such as position, pressure or temperature and make this data available to control systems in real time. Without them, precise process management, quality control and predictive maintenance would not be possible. At present, development is shaped above all by intelligent sensors with integrated signal pre-processing and communication. Modern smart sensors combine sensor element, analogue-to-digital converter and microcontroller in one housing and handle tasks such as filtering, plausibility checking or self-diagnosis directly at the measuring point. This reduces data volumes, increases robustness against interference and enables decentralised decision logic close to the process. In parallel, IO-Link is establishing itself as an open, manufacturer-independent point-to-point standard that transmits both process data and parameter and diagnostic information bidirectionally over a simple three-wire connection. IO-Link allows end-to-end parameterisation, fast device replacement scenarios and the integration of sensors into higher-level IIoT and condition-monitoring concepts. Together, intelligent sensor technology and digital fieldbuses such as IO-Link lead to a more connected, data-driven factory in which sensors not only measure, but actively contribute to the efficiency, flexibility and transparency of production.

EBV’s portfolio offers you the right sensors for your requirements from the world’s leading manufacturers.

 

Modular semiconductor concepts accelerate change in factory automation

Chiplets and heterogeneous integration enable controls that aremore modular, more powerful and more adaptable. At a time of increasing product variety and shorter product cycles, such architectural approaches are coming more strongly into focus.

Chiplets and heterogeneous integration are seen in factory automation as the key to more flexible, more compact and more powerful control systems. Chiplets are small, specialised semiconductor building blocks that are assembled modularly into an overall system, instead of integrating everything into one large monolith. Heterogeneous integration means combining different, separately manufactured devices such as logic, memory, sensors or power electronics into a shared assembly. This is attractive for automation because controls can be configured more specifically and adapted more quickly depending on the machine task. Central trends include advanced packaging, 2.5D and 3D integration, energy-efficient edge processing, and closer coupling of AI, IIoT and digital twins in industrial control architectures. The development is thus aimed at modular systems that combine higher computing power, better scalability and shorter development cycles.

Find out more about the chiplets in EBV’s portfolio.

 

AI and 3D image processing drive machine vision forward in production

Machine vision is now a central building block for quality assurance, process control and flexibility in production. The use of AI, edge processing and high-resolution image processing in particular is currently driving development and changing the possibilities for its use.

Machine vision is increasingly becoming a central building block of modern production processes: systems with cameras, lighting and evaluation software inspect components in real time, support robot guidance and assure quality directly on the line. The trend is towards more intelligent applications in which AI-supported evaluation, edge processing and high-resolution image sensors work together. This makes it possible to handle complex surfaces, changing products and difficult lighting conditions more reliably. At the same time, 3D vision, multispectral methods and the connection to IIoT and automation platforms are gaining importance, because image data is then not only captured but can also be used across production.

At the heart of machine vision solutions are CMOS-based image sensors, which today characterise the majority of industrial cameras, as well as powerful processors and specialised AI accelerators for evaluation at the edge. Added to this are memory devices and fast interface ICs that transport and buffer large volumes of image data reliably.

Find out more about EBV’s portfolio of smart cameras and image sensors.

 

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.