Custom Meta Tags

EBV - Markets - Industrial Animated HB Static HTML

2609 Hero Banner_2

EBV - Industry and Energy - Energy Storage (MT)

Energy Storage – from grid support to a digital energy system

EBV - Industry and Energy - Energy Storage - Intro (MM)

Energy storage is becoming ever more important for smart grids and renewable energies, because as wind and solar power expand, feed-in becomes more variable and grids therefore need more balancing, flexibility and resilience. From the large storage park at industrial sites, hospitals or campuses to the compact home battery, storage is moving into the role of an infrastructural link that brings generation and consumption closer together.

Technologically, the market is shaped above all by decentralised storage architectures and increasing coupling with photovoltaics and e-mobility. Added to this are bidirectional charging, peak shaving and new forms of local energy networking, in which households and companies are more strongly involved in the active control of the electricity system. The trend is towards more autonomy at the grid edge, supported by digital platforms that control energy flows more precisely and reduce losses.

Industrial Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our Industrial Director Andrej Orel

EBV - Industry and Energy - Energy Storage - Accordion Static HTML

Battery-Capacity

Added battery capacity in Europe (market scenarios for annual BESS additions in Europe 2026–2030). (Source: ees/SolarPower Europe)

 

More efficiency and safety in the BESS

For semiconductor solutions, new SiC and IGBT generations are currently particularly relevant, promising higher efficiency, lower switching losses and more robustness in BESS inverters and converters. Added to this are integrated BMS devices with precise cell monitoring, isolated measurement and communication paths, and protective functions for high-voltage racks. Important developments also include devices for bidirectional power flows, for example for peak shaving and vehicle-to-grid, as well as safety and diagnostic functions that bring functional safety, certification and cybersecurity together better. In parallel, digital battery passports, cloud-capable condition algorithms and reference designs for faster development cycles are gaining importance, because they bring BESS projects from the laboratory into industrial application more quickly.
 

Pre-certified BMS SoCs simplify the design of BESS applications

Highly integrated, pre-certified BMS SoCs are regarded as an important building block for safe and efficient battery storage systems. They bundle central protection, measurement and diagnostic functions in one chip and thus support the scaling of BESS applications while reducing complexity.

Highly integrated, pre-certified BMS SoCs for functional safety monitor and protect battery packs. They simplify secure communication between cells, power electronics and control. In practice, they support the trend towards more compact, more cost-efficient and at the same time safety-critical storage solutions that absorb load peaks, integrate renewable energies and work stably in the field for years.

The most important technology trends include higher integration of measurement, protection and diagnostic functions, more precise state estimation for SoC and SoH, faster responses to fault patterns, and more robust communication paths such as CAN FD and IsoSPI. In parallel, functional safety is gaining weight, because operators and manufacturers of BESS increasingly rely on standard-oriented, certification-friendly platforms in order to reduce development times and validation effort. Predictive monitoring and software-supported fault detection are also becoming more important, in order to detect failures early and increase availability.

On the semiconductor side, two developments currently shape the market for highly integrated, pre-certified BMS SoCs: first, devices with integrated functional safety, self-diagnosis and redundancy functions are coming more strongly into focus, because they simplify certification and increase resilience in BESS applications. Second, manufacturers increasingly rely on SoCs that bundle more precise cell voltage and temperature measurement, faster fault detection and secure communication interfaces in a single chip. Added to this is the trend towards modularly scalable platforms that can be adapted more easily to different cell chemistries, voltage levels and system sizes. In practice, this means fewer external components, lower complexity in pack design and shorter development times with a higher level of safety at the same time.

Find out about BMS SoCs from the leading manufacturers in EBV’s portfolio.

 

BESS need more than power: identity and protection are becoming standard

Storage plants are increasingly connected, remotely maintainable and therefore vulnerable. This makes hardware-based cybersecurity for BESS ever more important. At the same time, the  digital battery identity (the EU “battery passport”) creates the basis for verifiably securing the origin, condition and integrity of battery systems across their entire lifecycle.

BESS not only buffer energy; as connected infrastructure elements they also have to be secured against manipulation, failures and supply chain risks. Digital identities create transparency about the origin, configuration, condition and lifecycle of a battery, while hardware-supported security functions protect identities, keys and firmware at device level. The most important trends include secure boot and update processes, tamper-resistant hardware root-of-trust approaches, end-to-end traceability along the supply chain, and closer alignment with industrial and energy security standards such as IEC 62443 and ISO/IEC 27001.

Among battery trends, circular business models, second-life applications and digital product passports are also coming into focus, because operators and manufacturers increasingly have to prove exactly which cells, modules and components are built into a storage system and how they have been operated. In parallel, pressure is growing to consider OT and IT security together, in order to harden BESS against ransomware, unauthorised remote access and configuration errors.

In semiconductor technology, secure elements, microcontrollers with integrated security functions, hardware-based key storage and trusted authentication are therefore becoming ever more relevant. Equally important are robust edge and communication devices that secure identities locally while being energy-efficient, updatable and designed for industrial long-term availability.

Find out more about our semiconductor solutions for implementing the hardware basis for the EU battery passport, from secure identity through tamper protection to data retrieval.

 

Specialised computing cores improve battery analysis in energy storage systems

Precise SoC and SoH algorithms are becoming ever more important for battery storage, because they largely determine the safe, efficient and economical operation of BESS. New impetus comes above all from edge AI, hybrid model approaches and specialised computing cores that bring more intelligence directly into the systems.

State-of-charge algorithms (SoC) estimate the current charge level of a battery storage system, state-of-health algorithms (SoH) assess the ageing condition and thus the remaining performance. Both are central to BESS, because they control how safely, efficiently and economically a storage system is operated.

Current trends are above all the use of data-driven models based on deep learning, hybrid approaches combining physics and AI, and adaptive control for real-time operation. Hybrid approaches combine physical prior knowledge with learning models so that forecasts become more precise and at the same time more robust. Added to this are digital twins, explainable AI (which makes it traceable why a model arrives at a particular prediction) and forecasting models that capture not only the charge level but also degradation and fault patterns better.

In semiconductor technology, the focus is therefore shifting to edge AI and specialised computing cores. In demand are energy-efficient AI accelerators, FPGA-based platforms, RISC-V and TPU-like architectures, and TinyML-capable designs that can run SoC/SoH models with little memory and low latency. For BESS, this means more intelligence in battery management with lower energy demand and better real-time capability at the same time.

Get to know EBV’s portfolio of processor solutions for edge AI and specialised computing cores from the leading manufacturers.

 

Rack and cluster architectures need robust, isolated data paths

As battery energy storage expands, the communication paths in rack and cluster architectures are also coming more strongly into focus. Because in high-voltage storage systems there are particular requirements for data transmission between the components.

In high-voltage storage systems (systems with voltages from over 60 volts up to several hundred volts), isolated communication is a central element, because it secures data paths between high-voltage areas, battery monitoring and power electronics. In rack architectures, the focus is above all on the reliable connection of individual battery modules, sensors and control units, while cluster architectures additionally have to secure stable communication between several racks and the higher-level system layer.

Current trends include more robust Ethernet and fieldbus solutions that enable fast and interference-proof data transmission both within the rack and between clusters. Added to this are more strongly integrated protection concepts against overvoltage and transient interference that run along the entire communication chain. At the same time, modular, scalable designs are gaining importance, because BESS projects can then be adapted more easily to different power ratings and plant layouts.

In semiconductor technology, isolated transceivers, digital isolators and interface devices with high immunity to interference are therefore coming into focus. Low power consumption, compact designs and high data rates combined with robust dielectric strength are important. For rack and cluster systems, it thus becomes decisive that communication remains not only secure, but also flexible, easy to maintain and resilient in the long term.

Explore EBV’s offering in the field of analog components, where you will find all the building blocks for communication protected against high-voltage influences.

 

Reference designs and modular semiconductor platforms significantly accelerate the development of BESS

The market for battery storage is growing rapidly and at the same time places high technical and economic demands on manufacturers. Anyone who shortens development times can turn innovations into marketable solutions faster and position themselves better in the competition.

The market for BESS is characterised by high investment pressure, regulatory requirements and rapid expansion of storage, grid and industrial capacity. Reference designs and modular semiconductor platforms help providers reduce development cycles considerably, because they provide proven building blocks, documented interfaces and tested system architectures. Instead of designing every function from scratch, developers can build on validated preliminary work, reduce risks earlier and move from prototype to series production faster. Companies benefit from shorter time-to-market, lower development costs, more predictable quality results and faster scaling.

At the same time, BESS and their components are increasingly integrated into compact platforms: power electronics, control and software work together more closely. Digital monitoring and diagnostics continuously supply data on condition, efficiency and possible faults. Modular architectures make scaling and variant creation easier. More efficient semiconductors reduce losses, while connected development processes speed up testing, coordination and approvals.

EBV offers a wide range of reference designs for various applications in the field of BESS. Ask our experts.

 

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.