Industrial communication is more than the wire between sensor and controller. It is the backbone of modern manufacturing: highly connected, real-time capable, interoperable. And the basis for the next steps in the evolution, from predictive maintenance through digital twins to autonomous manufacturing systems.
Industrial communication is rapidly becoming the critical point of modern manufacturing systems. While Industry 4.0 and the Industrial Internet of Things (IIoT) have long been established, the efficient networking of machines, sensors and edge devices remains a central challenge.
Let's talk
Better connected through LinkedIn
Get directly in touch with our Industrial Director Andrej Orel

Market shares of industrial Ethernet protocols such as PROFINET, Ethernet, EtherCAT and others according to an Omdia study (source: Omdia, Industrial Communication Report 2025)
At field level, IO-Link has established itself as a universal interface for sensors and actuators. Above it, Ethernet-based fieldbuses dominate such as PROFINET or EtherCAT. Time-Sensitive Networking (TSN) extends standard Ethernet with time slots and prioritisation mechanisms for reliable, jitter-free transmission of time-critical data. One game changer is Single Pair Ethernet (SPE). SPE transmits Ethernet data over just one wire pair and can supply power in parallel. This makes Ethernet consistently possible right down to sensor and actuator level. Wireless technologies and fibre optics complement the portfolio. Wi-Fi is used for moving machine parts, while fibre optics offer the highest bandwidths and electromagnetic immunity for demanding environments. Industrial communication forms the nervous system of the digital factory. Trends such as IO-Link, PROFINET, EtherCAT and OPC UA point the way to end-to-end, standardised networking. TSN and SPE close the last gaps for a uniform infrastructure from the sensor to the cloud. Ethernet is the standard in mechanical engineering: only one per cent of companies do without it.
Connectivity is increasingly integrated directly into MCUs and MPUs
Semiconductors form the physical basis of every industrial communication solution. At present, the integration of connectivity functions directly into microcontrollers and processors is rising: modern SoCs combine computing power with Ethernet, Wi-Fi and Bluetooth interfaces on a single chip. In addition, specialised PHYs and switches for industrial Ethernet, in particular for PROFINET, EtherCAT and Single Pair Ethernet, are gaining importance, because they are what makes deterministic real-time communication possible in the first place.
As a leading distributor of semiconductors and embedded solutions, EBV Elektronik supports its customers along this path. With a portfolio ranging from microcontrollers through connectivity solutions to edge computing platforms, EBV paves the way into the IoT, via edge and gateway to the cloud.
TCP/IP is becoming the key protocol of industrial networks
TCP/IP communication forms the backbone of industrial networks today, connecting machines, controls and IT systems through a shared data basis. As production and automation become more connected, it continues to gain importance, because it enables the exchange of information just as much as the integration of new functions and applications.
The TCP/IP protocol is the common language in industrial networks for data exchange between machines, controls and IT systems; it connects classic automation with the connected world of IIoT and Industry 4.0. The trend is towards convergent architectures in which real-time communication, diagnostics and cloud connection come together over a uniform infrastructure.
The most important technology trends include industrial Ethernet as the dominant basis, the increasing use of OPC UA as an interoperable data interface, and TSN, which is intended to secure time-critical communication more precisely. Added to this is the growing importance of wireless connections, for example for flexible plant concepts, mobile systems and production environments that are hard to access. In parallel, IPv6 remains relevant, because the number of connected devices in the industrial environment continues to rise.
In semiconductor technology, the focus is above all on integrated network controllers, multi-protocol capable communication devices and energy-efficient edge components that can process TCP/IP data traffic robustly and with lower latency. Equally important are security functions directly in the chip, for example for encrypted communication and secured device identities, because connected production and IT integration increase the attack surface.
Find out about the TCP/IP products in EBV’s portfolio.
TSN makes industrial networks real-time capable and predictable
Time-Sensitive Networking (TSN) is regarded as an important building block for the next generation of industrial networks, because it extends Ethernet with precise time control and deterministic data transmission. TSN thus creates the basis for bringing classic automation, connected machines and IT systems together in a shared infrastructure.
Time-Sensitive Networking (TSN) is developing in industrial networks from a specialist topic into a key building block for convergent Ethernet architectures: the technology brings real-time capability, predictable latency and precise time synchronisation to industrial communication, creating the basis for applications in which control, sensor and IT data come together on one network.
The most important trends include closer integration of TSN with OPC UA and PROFINET, the development of uniform configuration and QoS models, and progressive standardisation for industrial automation, for example via IEC/IEEE 60802. In parallel, the combination of TSN and network virtualisation is gaining importance, because manufacturers want to use it to create flexible, scalable and at the same time deterministic infrastructures for smart production.
In semiconductor technology, the current focus is above all on industrial SoCs and FPGAs that support TSN functions not only in software but also bring hardware for time synchronisation, scheduling, redundancy and determinism. For machine builders and automation specialists, this is decisive, because genuine TSN performance in the field can generally only be achieved with appropriate integrated network technology; standard Ethernet components alone are usually not sufficient.
Find out more about EBV’s TSN solutions.
Single Pair Ethernet reduces wiring effort in industrial networks
Single Pair Ethernet (SPE) is regarded as a key technology for making industrial networks more space-saving, more cost-efficient and at the same time high-performing. In densely wired automation environments and IIoT applications in particular, SPE creates the basis for end-to-end communication right down to field level.
Single Pair Ethernet (SPE) is developing into an important bridging technology in industrial communication between sensors, actuators and the cloud: transmission over just one twisted wire pair saves space, reduces cabling costs and therefore suits densely packed automation systems and compact robots particularly well. Central trends include greater continuity from field level into IT systems, the growing importance of PoDL for data and power over the same line, and increasing standardisation and interoperability around industrial Ethernet architectures. Added to this are more compact cables with smaller bending radii, greater ranges in relevant sub-applications, and new point-to-point and multidrop approaches that make SPE more attractive for Industry 4.0 and IIoT scenarios.
For semiconductor technology, what matters above all is that SPE needs robust, energy-efficient PHYs, suitable transceivers and integrated PoDL solutions that support industrial EMC requirements and long service lives in the field. At the same time, the focus is shifting to higher integration density, lower power consumption and a broader portfolio for different ranges and data rates, because SPE is developing from a pure cabling question into a system platform for industrial networks.
Find out about the SPE connectivity solutions in EBV’s portfolio.
New wireless standards make factories more connected and more robust
In industrial automation, wireless communication is developing from a supplementary topic into a key one, because it supports flexible plant concepts, mobile applications and scalable IIoT structures. With new wireless standards and private mobile networks, the focus is not only on more bandwidth, but also on robustness, low latency and the most efficient possible use of energy.
Wireless connectivity is increasingly becoming an enabler for flexible, mobile and scalable applications in industrial networks, wherever cabling is too inflexible, too expensive or technically impractical. Current trends are above all Wi-‑Fi 6/6E and Wi-‑Fi 7 with higher bandwidth and lower latency, private 5G networks for campus and plant communication, Bluetooth Mesh for robust IIoT topologies, LoRa for low-energy wide-area applications, and NB-IoT and Cat-M1 for narrowband, low-power edge connectivity.
In practice, the focus is thus shifting from pure range towards more deterministic communication, higher device density and better resilience. In manufacturing in particular, hybrid architectures are gaining importance, in which different wireless standards are combined depending on the application.
For semiconductor technology, the current focus is above all on energy-efficient wireless SoCs, high-performance RF front ends, integrated multi-band antenna solutions and security functions at chip level. In addition, system-on-chip approaches, edge-AI capable radio modules and optimised components for low latency and high robustness are driving development forward, because industrial wireless systems have to meet ever more complex requirements for performance, security and energy consumption.
Get to know EBV’s broad portfolio around wireless connectivity for industrial applications.
From TPM to IEC 62443: how cybersecurity is reliably anchored in industrial communication
The increasing connectivity of production plants and IIoT devices makes industrial networks attractive targets for cyberattacks, and purely software-based solutions are increasingly reaching their limits here. Hardware-based cybersecurity relies on chip-level security mechanisms to prevent manipulation and unauthorised access at the root.
Hardware-based cybersecurity for OT and IIoT nodes forms the technical foundation of secure industrial networks: it protects controls, sensors and gateways directly at chip level against manipulation, unauthorised access and lateral attacks within production environments. Instead of purely software-based measures, it moves cryptographic keys, identities and integrity checks into trusted hardware, an approach that is gaining importance particularly in view of increasing AI-supported attacks on PLCs and HMI systems.
The most important trends include the integration of hardware security modules (HSM) and trusted platform modules (TPM) into industrial communication controllers, the use of secure boot and firmware signing to prevent malware at field level, and the enforcement of zero-trust architectures through hardware-bound device identities. This is complemented by standardised security certifications to IEC 62443-4-2 and the increasing micro-segmentation of OT networks by means of hardware-supported access controls.
In semiconductor technology, secure element IPs for microcontrollers, hardware-accelerated crypto engines with side-channel resistance and the integration of physically unclonable functions (PUF) for keyless authentication are currently gaining particular relevance. These technologies make it possible to anchor security functions directly in IIoT chips in an energy-efficient and space-saving way, a decisive step towards security by design in industrial automation.
Explore EBV’s solutions around hardware-based security.
New packaging techniques improve thermal management, density and reliability in industrial networks
Advanced packaging techniques and 3D integration enable high functionality in a small space and thus set new standards for efficiency and reliability. For compact communication modules in demanding environments in particular, they are becoming an enabler for robust, temperature-stable and high-performance systems.
Advanced packaging techniques and 3D integration bring computing, communication and interface functions together in a small space and thus enable robust, compact and energy-efficient communication modules. Current trends are chiplet architectures, heterogeneous integration of logic, memory and analog functions, 2.5D and 3D stacking, and advanced substrates and new interconnect techniques for better signal paths and higher reliability.
For industrial communication, what counts above all is that such packaging approaches combine higher integration density with good heat dissipation and mechanical stability. This is important for communication modules in harsh environments, for example in machine controls, edge gateways or network nodes, where small size, temperature resistance and long service life have to come together.
In semiconductor technology, chiplet-based designs, thermally optimised 3D integration and packaging-related co-design approaches are currently considered particularly relevant. They support compact, high-performance communication modules that work reliably despite dense packing and fit into industrial networks with high demands on signal quality and robustness.
Find out about the chiplet solutions in EBV’s portfolio.
Solutions
EBV Embedded Solutions
We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

Resources
EBV Podcast
Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.