Custom Meta Tags

Hero Banner

AVA - Industrial Automation - Sub Navigation

AVA - The Internet of Everything in the industrial environment - Intro - Static HTML_1

The Internet of Things in the industrial environment

Digitalisation and connectivity are forging new avenues for automation within the manufacturing industry under the banner of Industry 4.0. Through the IoT, devices, machinery, and systems are now interconnected, capturing a vast amount of machine-generated data. Digital twins, replicas of physical assets within the factory, enable their simulation, control, and enhancement. These digital twins represent products, machines, and their components as digital models, incorporating all geometry, kinematics, and logic data. McKinsey estimates that manufacturers utilising digital twins can boost their revenue by up to 10 percent, enhance product quality by up to 25 percent, and reduce time to market by up to 50 percent. By merging digital twins with Metaverse applications such as Virtual Reality (VR), industrial enterprises can create simulated worlds that precisely model the operational environment for forward-looking decision-making.
 

 

Learn More

Applications in Industrial Automation

The introduction of the Internet of Things in manufacturing and industrial processes elevates the possibilities of connectivity and the resulting benefits to a new level: Better-coordinated production steps lead to significant time savings and, thus, higher productivity. Digital twins can be based on a broader data foundation and replicate their real counterparts more accurately and realistically. Decisions can be made much faster and on a broader basis with the help of intelligent machines and their access to extensive data volumes. Reactions to disturbances within the production process and external problems, such as disruptions in the supply chain, can be made almost in real time.

The applications of the Internet of Everything in the industry are diverse:

  • Predictive Maintenance: Through the continuous monitoring and analysis of machine parameters such as temperature, vibration levels, noise development, speed, and operating time, it is possible to determine when damage and, subsequently, an unplanned shutdown will occur and when maintenance is required. According to a Deloitte study, manufacturers can increase the uptime of their equipment by 20 percent, reduce maintenance costs by 10 percent, and cut maintenance scheduling time by 50 percent through predictive maintenance.
  • Quality Control: Sensors on the production line, quality control systems, employee feedback, and customer reviews can be merged and analysed in the IoT. Based on this, production processes can be adjusted, or the product design can be changed.
  • Health and Safety of Workers: Wearables and sensors monitor the vital parameters of employees. Analysing this data can help detect when an employee becomes inattentive or the workload is too high. Accordingly, production plans can be dynamically adjusted, production processes adapted, or employees alerted.
  • Human-Machine Collaboration: Cobots can anticipate the following command from a human by analysing various interaction possibilities such as gestures, speech, eye movements, and brain activity. Recognising intention allows for a more natural interaction and significantly more efficient collaboration.

Sensing as the basis of the Industrial IoT

Intelligent, connected sensors form the technical foundation of the Internet of Things. In the industrial environment, they must meet exceptionally high robustness, size, power consumption, and reliability requirements. There is also a trend towards digital output sensors that deliver easily communicable data directly from the source. Depending on the application, data collection focuses on real-time capability, application-specific key performance indicators, expectations of the sensor's battery life, and integrated edge computing capabilities.
 

Robust connectivity as a prerequisite in the IoT

IoT applications depend on feedback provided by various sensors within the factory. Each of these sensors requires both energy to operate and a connection to the network for information exchange. The number of required connections within the factory will increase with the IoT. The performance requirements for connectors are high, whether for powering energy-intensive processes or providing secure high-speed communication for intelligent automation devices or AI applications at the "edge". At the same time, connectivity technology must be robust and sealed against media such as water or chemicals to withstand the harsh environmental conditions in today's factories.
 

The Internet of Things requires a secure power supply

Power supplies are a critical component, especially in the industrial Internet of Everything (IIoT). Automation systems require a consistent and reliable power source to ensure smooth operation and avoid downtime or malfunctions. Controls, measuring devices, manufacturing plants, robots, and communication networks all need energy. Power supplies must ensure stability and reliability to benefit from the advantages of the IoT in the industrial environment, even in harsh conditions, while offering high efficiency and good EMC protection.
 

IoT solutions as a growth stimulus for companies

The Internet of Things is a crucial component of the advancing digital transformation and will continue to automate processes within and surrounding the industry. It facilitates the achievement of objectives such as efficiency optimisation, cost reductions in production, faster processes, and the implementation of new business models more readily. When used correctly, the IoE can provide growth stimuli, bolstering the competitiveness and future viability of the company.

 

Industrial Automation IoT and Sensor Innovations for Predictive Maintenance Wallpaper - Static HTML_3-GM

Industrial Automation: IoT and Sensor Innovations for Predictive Maintenance

This whitepaper explores the transformative impact of IoT and advanced sensor technologies on industrial automation. It delves into key applications like condition-based monitoring and predictive maintenance, examining various sensor types and overarching trends such as wireless connectivity, energy efficiency, and AI at the edge. A detailed use case highlights the benefits of customized IoT sensors in reducing maintenance efforts for industrial pumps. Discover how these innovations drive efficiency and reliability in modern industrial settings.
 

Thank you for your interest!

Please fill in the form below to download our whitepaper.

 
 

2024-07-IoT-Industrial-Automation-White-Paper-Socials

 

 

 

Webinars - Static HTML_3-JZ

Join Us for Exclusive Webinars

Avnet Abacus, in collaboration with industry leaders Molex and Kyocera AVX, is excited to announce two new webinars focused on the transformative potential of IoT in industrial automation. These sessions will explore cutting-edge technologies, innovative solutions, and practical insights to help you leverage IoT for enhanced efficiency, productivity, and connectivity in your industrial applications.

Don't miss this opportunity to learn from the experts and stay ahead in the rapidly evolving field of industrial automation.
 



IoT Podcast - Static HTML_3-AN

Podcast

Join "The Technology Addicts" podcast by Avnet Abacus and explore the exciting world of IoT - Industrial Automation solutions with our inspiring interview guests.
 

 
 

 

 

 

Solution Overview - Static HTML

What makes a factory smart?

Measure more

IoT data from smart sensors provides the foundation for a smart factory. Adding sensors to your factory floor reveals valuable insights into operations.


Real-time data

Data captured in real-time can be displayed on a configurable dashboard, showing the status of factory assets. Device health is continuously monitored, to generate predictive maintenance reports.


See everything

Monitor the location of your assets and track them on a customized map-based user interface. Instantly identify an asset and access its status, including historical operational data.


Automate action

Empower the workforce to be an active part of operations using a smart ticketing system. Review and elevate tickets as it moves through the system, with associated documentation always accessible.

AVA - Suppliers - Static HTML

Featured Suppliers

Amphenol+Corporation+Logo
bel-logo
bourns-logo
Harwin+New+Logo
KYOCERA-AVX+Logo
/Molex-logo
Murata-logo
samtec-logo
TDK
TE-Connectivity-Logo
 

 

 

 

 

CTA-Lower - Hero Banner V2

Static HTML_2