Design HB2 Silica

Reference Design Details

Design Hub

Search Reference Designs

SubNav - Design Hub

Script Application

This is a toast message

Motion Sensor Module based on Renesas Solution

This solution is an analog motion sensor that can detect motion from two meters away by using a passive infrared sensor (PIR) sensor. The sensor is connected to a bandpass filter using op amps (SLG88103) to condition and filter the signal. The amplified condition signal is connected to the analog pin of the MCU to determine the strength and distance of motion. The signal also connects to nano-powered comparators, forming a window comparison that can be used to wake up an MCU or system upon motion detection.
CATEGORY
Embedded,Sensors,Analog
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
Motion Sensor Module based on Renesas Solution

 

DH Related Events Menu