Custom Meta Tags

EBV - Markets - Hero_Banner_Animation_Living_infrastructure Static HTML

Custom Meta Tags

EBV - Living and Infrastructure - Smart Home (MT)

Smart Home & Building – ecosystems that adapt to their users

EBV - Living and Infrastructure - Smart Home - Intro (MM)

The shift towards intelligent buildings is one of the most defining forces of innovation in the electronics industry. Whether a home, an office complex, a hospital or an educational institution, modern smart homes and smart buildings are turning into connected ecosystems that adapt dynamically to their users' needs. EBV Elektronik sees this application area as a holistic approach to creating energy-efficient, safe and comfortable living and working spaces: from intelligent home automation through building management systems (BMS/BACS) to IoT-based solutions for HVAC, access control and sensor-driven optimisation.

Graphic Smart home

Living and Infrastructure Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our Living & Infrastructure Manager Borut Kastelic

EBV - Living and Infrastructure - Smart Home - Accordion Static HTML

Semiconductor solutions drive progress

At the heart of it lies the ability to capture data precisely from distributed sensors, transmit it over suitable wireless or wired technologies and evaluate it right at the network edge.

On this basis, adaptive systems emerge that automatically regulate lighting, climate or air quality and adapt to occupancy, time of day or individual preferences. High-quality, energy-efficient lighting becomes a key technology here: it influences not only energy consumption but also the wellbeing of users, for instance through circadian lighting concepts that support productivity and health. At the same time, technologies such as UV-C disinfection improve hygiene and safety in sensitive environments. Presence detection and people counting, meanwhile, allow resources to be managed as needed, lower operating costs and reduce the CO₂ footprint.

Technologically, this development rests on capable semiconductor solutions: microcontrollers and processors, connectivity standards such as Wi-Fi, BLE, Zigbee or Matter, and a broad range of sensors for temperature, movement, air quality or flow form the foundation. They are complemented by modern access technologies such as NFC, UWB or 3D-based authentication. Regulatory requirements also push innovation further, for example stricter energy-efficiency rules or the growing electrification of heating systems through heat pumps. One clear trend is the shift of intelligence towards the edge: AI-supported algorithms analyse sensor data in real time and continuously optimise building operation, from predictive maintenance to the autonomous control of complex systems.

With a comprehensive semiconductor portfolio and deep application know-how, EBV Elektronik plays a decisive part in advancing future-ready smart-home and smart-building solutions.

 

Capable MCUs and MPUs for more intelligence "on site"

The boundaries between microcontrollers (MCUs) and microprocessors (MPUs) are increasingly blurring, driven by the integration of dedicated neural processing units (NPUs) directly into the silicon chip.

While MPUs have traditionally dominated compute-intensive operating systems such as Linux in smart-hub centres, high-performance MCUs are now conquering the edge-AI space for specific sensor nodes. Manufacturers are expanding their portfolios to enable localised intelligence "on device", which minimises latency and strengthens privacy in smart homes through data-protection-compliant processing without a mandatory cloud connection. In the smart building in particular, this architecture allows predictive maintenance and adaptive energy control, because the algorithms run directly on the microcontroller rather than streaming data to the cloud. Standards such as Matter also simplify the interoperable networking of heterogeneous devices, while the hardware works more energy-efficiently thanks to hardware accelerators for machine learning (ML). Looking ahead, we can expect the entire building infrastructure to move towards autonomous, AI-supported systems that do not merely react but anticipate users' needs. This development marks a paradigm shift away from purely connectivity-based solutions towards locally acting systems in building automation that make decisions on their own.

Browse EBV’s Embedded Processing portfolio – semiconductor solutions for almost any application, from simple 8-bit microcontrollers to AI accelerators.

 

Connectivity solutions deliver end-to-end interoperability in the smart building

Connectivity solutions in the smart-home and smart-building sector remain highly hybrid.

Semiconductor solutions that combine multi-protocol connectivity (Wi-Fi 6/7, BLE 5.4, Zigbee 4.0, Matter over Thread) on a single chip therefore play an ever more important role, increasingly integrating edge-AI functions for local data processing. While established KNX systems continue to form the basis for lighting, blinds, door access and ventilation, Single Pair Ethernet (SPE) is gaining importance thanks to lower cabling costs and simpler installation. Wi-Fi 6/7 with multi-Gbps data rates and BLE 5.4 for battery-powered devices enable cost-effective retrofit solutions, while Power over Ethernet (PoE) and Power over Data Line (PoDL) score particularly well in safety-critical applications such as surveillance and access control. At the same time, Matter 1.5 is being used as a cross-vendor standard in more and more applications, though established technologies such as Zigbee, with its migration into the sub-GHz range, and Z-Wave Long Range remain relevant for critical applications. For asset tracking in large buildings such as hospitals or shopping malls, solutions such as BLE and UWB come into play, while Li-Fi serves niches as a tap-proof alternative in highly sensitive enterprise environments. The upshot: protocol fragmentation is here to stay, but multi-protocol SoCs with edge AI and zero-trust security make the complexity invisible to end users.

EBV’s extensive portfolio of connectivity solutions covers smart-home and smart-building applications.

 

Sensors are becoming ever more energy-efficient and intelligent

In the smart home and smart building, highly efficient semiconductor solutions for sensor technology are increasingly taking hold.

In 2025, according to the Eurostat study "Digitalisation in Europe", more than a third of people in the EU (35%) used generative AI tools.

Alongside classic temperature, light and pressure sensors for capturing ambient conditions, more and more solutions for monitoring air quality are being used. Modern devices use various detection methods to measure CO₂ levels and detect volatile organic compounds (VOCs), a basis for intelligent indoor-climate control. Advanced optoelectronics such as infrared time-of-flight sensors (IR-ToF) also allow the precise counting of people in a room, so that ventilation and air conditioning can be controlled as needed. Radar solutions are also gaining importance in this context. Both technologies are considerably more effective than the pyroelectric sensors used in the past. Sophisticated smoke sensors based on spectral sensing can recognise the type of smoke, whether it comes from an actual fire or from cooking, and so prevent false alarms in hotel or restaurant kitchens. One fundamental trend here is the development of ultra-low-power sensors that shut down completely when idle with the help of dedicated power-saving ICs and become active only when needed. This contributes significantly to extending battery life in wireless sensors and to building low-maintenance systems.

Discover EBV’s extensive portfolio of diverse sensor solutions for the smart home and building automation.

 

Power and motor control – more efficiency in ever more compact spaces

In modern homes and buildings, power- and motor-control ICs are becoming increasingly important, driven by stricter EU efficiency requirements, the demand for quieter, smarter household appliances and the general electrification of ever more applications.

One fundamental trend here is the use of wide-bandgap semiconductors (WBG) such as silicon carbide (SiC) and gallium nitride (GaN), which enable higher switching frequencies, lower losses and more compact designs. In parallel, miniaturisation is advancing through intelligent power modules (IPMs), which combine power semiconductors (such as IGBTs or MOSFETs), driver circuits and protection functions in a single package. This integration allows not only more efficient motor control in washing machines, refrigerators or ventilation systems but also intelligent functions such as load-dependent control, predictive maintenance and seamless networking within the building ecosystem. With the introduction of standards such as "Ki Cordless Kitchen" and inductive power transfer of up to 2.2 kW, the wireless supply of small kitchen appliances is becoming reality, a step that would be hard to imagine without modern WBG components, driver ICs and HMI components. For manufacturers, this means that whoever invests today in integrated, efficient and connected power solutions is ready for the next generations of smart buildings and homes.

EBV’s portfolio covers all the key components around drive control and power management – our experts help you choose.

 

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.