Custom Meta Tags

EBV - Markets - Hero_Banner_Animation_Living_infrastructure Static HTML

Custom Meta Tags

EBV - Living and Infrastructure - Smart Agriculture - Title (LC)

Smart Agriculture and Environmental Systems

For more productive and more sustainable farming

EBV - Living and Infrastructure - Smart Agriculture - Intro (MM)

Agriculture faces profound change. Driven by the need to feed a growing world population, to use resources such as water and energy more efficiently and to meet the consequences of climate change, the sector is increasingly turning to digital innovation. With technologies such as IoT connectivity, intelligent sensors, data analytics and automation, agricultural production is becoming more productive, more sustainable and more climate-resilient, while natural resources are protected.

Digitalisation is decisive for this transformation: AI and machine learning analyse large volumes of data to support precise decisions, for instance in forecasting weather conditions or detecting plant diseases. Autonomous tractors and robotic systems take on tasks such as planting, weeding and harvesting without human intervention and noticeably lower operating costs. IoT-enabled devices link various agricultural machines and sensors to collect real-time data and allow remote monitoring.

Living and Infrastructure Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our Living & Infrastructure Manager Borut Kastelic

EBV - Living and Infrastructure - Smart Agriculture - Diagram Static HTML

Intelligent irrigation systems optimise water use, sensors monitor the nutrient content of the soil, and cloud-based platforms support farmers in making data-driven decisions. These developments aim to minimise the ecological footprint of agriculture while maximising yields and productivity at the same time. According to the market analysts at The Insight Partners, the market for smart agriculture is expected to grow by 43 billion US dollars by 2031, corresponding to an average annual growth rate of 12%.

 

Graphic_Smart_Farming

 

Four trends shape semiconductor solutions for smart agriculture

Without advanced microchips, sensors and connectivity solutions, these intelligent agricultural systems would be inconceivable. Semiconductors make it possible to capture, process and transmit data, bridging the physical world and digital control.

Four fundamental trends are emerging here: first, the integration of AI directly into microcontrollers (edge AI), which allows autonomous decisions without a cloud connection. Second, the development of ultra-efficient chips that lower energy consumption and extend the operating life of battery-powered devices. Third, the miniaturisation of sensors, which opens up new fields of use in agriculture. And fourth, closer networking of system components to create holistic solutions for farmers.

EBV is a strategic partner for developing innovative agricultural technology: our experts support device and system manufacturers not only by supplying the right components such as sensors, MCUs and connectivity modules, but throughout the entire development process of intelligent agricultural systems, from automated irrigation to livestock monitoring and drone control.

 

EBV - Living and Infrastructure - Smart Agriculture - Accordion Static HTML

Energy-self-sufficient and connected: new sensors drive precision farming

Semiconductor-based sensors enable precise, energy-efficient, and connected measurement of soil moisture, nutrient levels, air quality, or microclimate.

~US$59 bn intelligent agricultural-sensor market by 2032 (Zion Market Research)

The market analysts at Zion Market Research assume that the market for intelligent agricultural sensors will grow by 16 per cent a year, to around 59 billion US dollars in 2032. Four technology trends currently dominate: first, the miniaturisation and integration of MEMS sensors (micro-electro-mechanical systems), which offer compact, robust and cost-effective solutions for field and greenhouse applications. Second, the development of energy-self-sufficient sensor nodes through energy harvesting and ultra-low-power semiconductors, which allow maintenance-free continuous operation outdoors. Third, the on-chip integration of AI functions (edge AI), which enables local data pre-processing and real-time decisions directly at the sensor, for instance to detect drought stress or pest infestation. Fourth, the ongoing networking via low-power wide-area networks (LPWAN) such as LoRaWAN or NB-IoT, which support area-wide, cloud-connected sensing.

With its sensor portfolio from the leading manufacturers, EBV supplies the key building blocks for resource-efficient, data-driven agriculture and environmental monitoring.

 

Image sensors deliver data beyond the visible range

Image sensors capture optical and multispectral data from plants, soils or water bodies and provide the basis for precise resource management, early-warning systems and data-driven decisions in agriculture.

Their spread is increasing rapidly, driven by falling component costs, more capable embedded platforms and the growing pressure to raise yields while minimising environmental impact. The main systems in use are camera systems on tractors, drones and stationary measuring stations, often coupled with AI analysis in real time. Three technology trends currently dominate: first, the integration of AI directly on the sensor (edge AI); second, multispectral and SWIR extensions (short-wave infrared) for deeper insight into plant physiology; and third, ultra-low power consumption and miniaturisation for self-sufficient IoT networks.

EBV carries image sensors from the leading suppliers on its line card – discover the comprehensive portfolio.

 

Ever more computing power in ever less space

Microcontrollers (MCUs) and microprocessors (MPUs) form the technological backbone of modern smart-agriculture and environmental-systems solutions: they control sensors for capturing soil moisture, air quality or climate data and enable decentralised, energy-efficient decisions directly in the field or in greenhouses.

Their spread is increasing worldwide, driven by advances in miniaturisation, falling component costs and the integration of AI functions at the edge. Three central technology trends currently shape the development: first, the integration of edge AI into energy-efficient MCUs, which makes local data analysis and pre-processing possible without a cloud connection, crucial for real-time monitoring in rural regions with unstable connectivity. Second, the ability to run machine-learning models directly on the device. This is enabled by ultra-low-power architectures (TinyML) running on MCUs. They are used, for example, to detect plant diseases through camera-based image analysis. Third, the convergence of multi-sensor fusion and adaptive communication: modern MPUs combine data from moisture sensors, spectral cameras and weather stations and adjust transmission protocols (LoRaWAN, NB-IoT, BLE) dynamically to energy availability and network quality, an approach that is already leading to significantly improved resource management in pilot projects.

Browse EBV’s comprehensive portfolio of MCUs and MPUs.

 

Robust wireless systems enable efficient networking of widely dispersed devices

Wireless connectivity is decisive in agricultural applications in particular, in order to network the widely spread-out devices with one another.

The spread of such solutions is growing rapidly, driven by falling IoT semiconductor costs, better energy efficiency and the expansion of LPWAN and 5G networks into rural regions too. Current technology trends are shaping the next generation:

  • Ultra-low-power MCUs with integrated radio (BLE 5/6, Zigbee, Thread) that run for years without a battery change.
  • LPWAN standards such as LoRaWAN, NB-IoT and MIOTY for long-range, robust connections at minimal energy consumption.
  • Multi-protocol SoCs that support several wireless standards in parallel and so increase scalability and future-proofing.

These trends make wireless systems smaller, cheaper and more reliable, and thus ready for mass use in precision farming, greenhouse automation or environmental monitoring.

See the solutions around wireless connectivity that EBV keeps ready in a comprehensive portfolio.

 

Multi-GNSS and RTK are the new key technologies for precise smart agriculture

GNSS positioning systems enable precise machine navigation, yield mapping, resource-saving application of seed and fertiliser, and the real-time monitoring of environmental and soil parameters.

While classic GPS systems still dominate today, modern semiconductor solutions increasingly rely on multi-GNSS chips that process signals from GPS, Galileo, GLONASS and BeiDou in parallel, a development that noticeably improves availability and accuracy even under difficult conditions such as forest or dense vegetation. Three central technology trends currently shape the field: first, the integration of RTK (real-time kinematic) into compact GNSS modules, which enables centimetre-accurate positioning for autonomous tractors, drones and robotic systems. Second, the combination of GNSS with 5G/NTN communication technologies, which allows robust, low-latency data transmission and cloud connection of distributed sensor nodes even in rural dead spots. Third, the miniaturisation and energy efficiency of semiconductor chips, which makes GNSS receivers integrable into wearables and distributed environmental measuring stations. In animal tracking, highly efficient GNSS semiconductor modules with an integrated low-power mode and support for various GNSS systems enable long-lasting, precise location of grazing livestock, wild animals and farm animals, even in remote or heavily wooded areas. By coupling this with IoT platforms and AI-supported movement analysis, health status, behavioural patterns and stress indicators can be identified early, which significantly improves animal welfare, herd management and the prevention of human-wildlife conflicts.

Explore EBV’s portfolio of positioning solutions from the leading manufacturers.

 

Energy harvesting makes environmental monitoring self-sufficient

Energy harvesting enables a self-sufficient, low-maintenance power supply for sensors and IoT devices that cannot be connected to the mains, or only with great effort.

Particularly in hard-to-reach or expansive agricultural and environmental-monitoring applications, it allows operation without battery changes and so supports sustainable, scalable solutions. The main sources in use are photovoltaic systems, thermoelectric generators and vibration- and ambient-based energy sources such as RF- or magnetic-field-based systems. Three central technology trends currently shape the development: first, the miniaturisation and greater efficiency of semiconductor-based energy-harvesting chips, which work reliably even with weak ambient energy. Second, the combination of several energy sources in hybrid systems, such as photovoltaics plus thermoelectrics, to increase the overall energy yield and close supply gaps. Third, the integration of AI and IoT for dynamic, real-time optimisation of energy management, for instance through predictive load control or adaptive energy distribution.

EBV offers a comprehensive range of different energy harvesting solutions.

 

Power management and connected BMS transform energy efficiency in smart agriculture

Power management and battery-management systems (BMS) reliably supply sensors, drones, autonomous machines and decentralised measuring stations with power and extend battery life in the field, the greenhouse and nature monitoring.

With the boom in precise, data-driven agriculture and area-wide environmental measuring networks, the spread of these systems is rising rapidly; market analyses forecast double-digit growth rates for BMS worldwide by 2030. The main systems in use are IoT-enabled BMS for lithium-ion and LFP batteries in solar irrigation, agricultural drones, electric tractors and in autonomous weather and soil stations. New technologies are driving the development: AI-supported state estimation (SOC/SOH), improved thermal management, ultra-low-power semiconductors for energy harvesting and standardised communication protocols for cloud connection. Four trends dominate:

  • integration of AI/ML for predictive maintenance and greater efficiency,
  • solid-state and LFP batteries with more robust BMS algorithms,
  • energy-harvesting solutions with highly efficient power management for self-sufficient sensor nodes,
  • connected BMS architectures with 5G/LoRaWAN for real-time energy management in the agricultural smart grid.

From power discretes through multi-channel PMICs and Power over Ethernet ICs to power modules – explore EBV’s power-management portfolio.

 

From SiC to isolation – analog components make a decisive contribution to resilient environmental systems

Analog and power semiconductors form the neural and energetic backbone of modern smart-agriculture and environmental systems: they supply sensors, actuators and communication modules with power precisely, convert measurement signals and so enable real-time decisions in the field.

In system development, architectural trade-offs have to be considered: smaller form factors and lower power consumption often conflict with high signal quality and durability, a balancing act that is particularly critical in the harsh agricultural environment. Power supplies must be designed to be especially robust, reliable and safe for use in extreme environmental conditions. Key requirements are a wide-range input voltage and high load stability, resistance to temperature and climate, a high degree of protection and mechanical durability, and reliable EMC and overvoltage protection.

Four technology trends dominate: first, wide-bandgap semiconductors such as SiC and GaN for highly efficient, compact power supplies in solar pumps or drones. Second, the integration of analog and digital functions into mixed-signal ASICs and power-management ICs for more robust, more intelligent systems. Third, reliable isolation technologies that guarantee high safety standards in harsh environments. Fourth, ultra-low-power components for battery-powered field sensors with long run times. Amplifiers, data converters and switching regulators remain key building blocks here, and their progress is a major force behind the digitalisation of agriculture and environmental systems.

EBV’s solution portfolio comprises state-of-the-art analog components. Discover our most important product groups and find the right solutions for your project.

 

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.