The All Electric Society is taking shape: electrical energy is increasingly becoming the connecting medium for mobility, heat, industrial processes and digital infrastructure. The drivers are the expansion of renewable energies, the electrification of vehicle fleets and building technology, and the growing electricity demand of data centres, communication networks and automated production plants. Studies by the International Energy Agency expect electricity to take a considerably larger share of final energy consumption in the course of decarbonisation. In parallel, the architecture of the energy supply is changing fundamentally. A largely centrally organised system is being replaced by distributed generators, battery storage, charging points, heat pumps and controllable loads. However, this also increases the challenge of reliably balancing generation and load at all times, particularly when solar and wind energy feed in depending on the weather and local grid bottlenecks.
For the electronics industry, this development opens up a broad field of innovation. Power semiconductors based on silicon carbide and gallium nitride increase the efficiency of converters, fast-charging infrastructure, photovoltaic and battery systems. Intelligent sensors, connected controls and edge computing simultaneously create the data basis for more precise energy management. Non-invasive load management is gaining particular importance here: it analyses electrical signatures in the grid in order to identify individual loads or load groups, without having to equip every endpoint separately with measuring technology. Combined with artificial intelligence, load profiles can be forecast, flexible consumption prioritised and energy flows optimised predictively.
Let's talk
Better connected through LinkedIn
Get directly in touch with our Industrial Director Karl Lehnhoff

Semiconductors as enablers of the electrified future
Semiconductors are what make electrical energy efficiently measurable, controllable and convertible in the first place. The most important trends currently include the rising importance of wide-bandgap materials such as silicon carbide and gallium nitride, which set new standards in power electronics, charging infrastructure, inverters and drive systems through higher switching frequencies, lower losses and more compact designs. Likewise, advanced packaging concepts, chiplet architectures and stronger system integration are coming into focus in order to combine computing power, energy efficiency and thermal management better. Added to this are edge AI and sensor-level data processing, which in combination with connected controls enable more precise load and energy management.
You can find much more information about the All Electric Society, its impact in the individual sectors and suitable, innovative semiconductor solutions here.
WBG semiconductors accelerate the energy transition
The All Electric Society needs more than just electricity: it needs intelligent, highly efficient conversion technology. Wide-bandgap power electronics deliver exactly that: more compact, more economical and more robust than ever before.
In an increasingly electrified world, from e-mobility through renewable energies to data centres and industrial drives, wide-bandgap power electronics enable higher efficiency, smaller systems and therefore lower material and energy consumption across the entire lifecycle.
The most important trends include the broad commercialisation of silicon carbide (SiC) and gallium nitride (GaN) in inverters, chargers and DC/DC converters, the integration of WBG components into modular power electronics platforms, and the coupling with digital control and AI optimisation methods. In parallel, requirements for reliability, standardisation and lifecycle-oriented environmental assessments are rising, for example in the context of PV systems, wind power or railway power systems.
In semiconductor technology, the current focus is above all on scaling SiC substrates to larger wafer diameters, improving GaN-on-Si processes for cost-effective mass production, and developing ultra-wide-bandgap materials such as gallium oxide. In addition, vertical GaN power devices, improved gate driver architectures and thermally optimised package concepts are gaining importance in order to exploit the advantages of WBG semiconductors fully in high-power applications too.
Find out more about EBV’s offering in the field of SiC and GaN power electronics.
Local AI and low-power inference chips are revolutionising the energy infrastructure
The All Electric Society poses new challenges for energy infrastructures: real-time data from millions of decentralised nodes has to be processed, analysed and translated into control commands within milliseconds. Edge computing and edge AI provide the answer, through local intelligence at the network edge that minimises latency, reduces cloud loads and strengthens the resilience of critical systems.
In the All Electric Society, edge computing enablesdata processing directly at decentralised nodes such as charging stations, smart meters or microgrid controls. By processing real-time data locally, edge computing reduces latency to milliseconds, relieves central cloud infrastructures and increases the resilience of critical energy applications. Current technology trends include the integration of AI models at the network edge for predictive maintenance, the networking of edge devices via 5G networks, and hybrid edge-cloud architectures that combine data protection and scalability.
In the field of edge AI in particular, the decentralised execution of AI models is gaining importance, because it enables real-time decisions without cloud dependency. For applications such as load forecasting in smart grids, adaptive charging strategies for electric vehicles or fault detection in energy infrastructures, edge AI is indispensable in order to ensure autonomy and speed of response.
Energy-efficient inference chips form the technological backbone of this development. These specialised semiconductors optimise energy consumption when running pre-trained AI models and thus enable edge-AI systems to operate even in resource-constrained environments. In the All Electric Society, where every watt-hour counts, they reduce the ecological footprint of decentralised computing power and are what make edge AI economically scalable in the first place.
Find out about our comprehensive portfolio for edge computing, from energy-efficient MCUs to embedded processors with integrated AI accelerators.
New sensor trends make electrical systems more intelligent and more efficient
Sensors are a key technology of the All Electric Society, because they are what make electrical systems visible, controllable and efficient. Sensor technology is changing from pure measurement towards intelligent, energy-efficient system building blocks.
Sensors are the central sensory organs of an increasingly electrified world: they supply the data with which power grids, buildings, industrial plants and mobility are controlled, monitored and secured efficiently. Without precise sensor technology, efficiency potential remains unused, faults are hard to detect and complex systems can only be managed to a limited extent. Sensor development is therefore currently moving to the centre of numerous applications around energy, automation and digital infrastructure.
The most important technology trends include higher measurement accuracy, miniaturisation and sensor fusion, that is, the intelligent combination of several measured variables. Added to this are connected sensor systems that not only capture data but pre-process it directly and thus make it usable faster. New material systems are also gaining importance: the focus here is above all on flexible, thin and partly organic or inorganic semiconductor materials. They enable more sensitive, more robust or more flexible sensors and can be adapted better to demanding environments.
Also in demand are low-power designs, for example architectures with short activation, local signal processing and as little data traffic as possible, in order to reduce energy consumption and costs. Particularly relevant is also the integration of several functions in a small space: sensors increasingly handle not only measurement, but also pre-processing, diagnostics and interface tasks.
EBV’s portfolio offers you the right sensors for your requirements from the world’s leading manufacturers.
Semiconductors with hardware protection are becoming ever more important for secure energy and industrial networks
Cybersecurity is becoming a critical cornerstone in the All Electric Society, because connected energy, industrial and building systems only work stably if digital attacks, manipulation and failures are effectively warded off. With growing pressure from regulation and ever more complex system architectures, the secure design of devices, networks and supply chains is coming more strongly into focus.
Cybersecurity is not a peripheral topic in the All Electric Society, but the prerequisite for connected energy, industrial and building systems to function reliably and for failures, manipulation or data leaks not to disrupt operation. Current trends are above all zero-trust architectures, AI-supported attack detection, secure remote access, continuous asset and vulnerability management, and the protection of IT and OT networks along the entire supply chain. For energy applications, segmented networks, robust identity and permission concepts, and resilient restart plans are also gaining weight.
The EU Cyber Resilience Act significantly increases the pressure on manufacturers: products with digital elements will in future have to be developed securely, documented and supplied with updates across their entire lifecycle. For operators and suppliers, this means more evidence, reporting and governance obligations as well as a stronger focus on security by design and security by default. Particularly for connected devices in energy grids, charging infrastructure and building automation, cybersecurity is thus becoming a competitive and approval issue.
In semiconductor technology, hardware root of trust, secure elements, TrustZone approaches, cryptographic accelerators and protected firmware update paths are therefore moving to the centre. Better protection mechanisms against manipulation and side-channel attacks, as well as more transparency across the entire supply chain, are also relevant. In the end, what is decisive is a chip that is not only powerful, but demonstrably trustworthy.
Explore EBV’s solutions around hardware-based security.
MRAM and eNVM strengthen the All Electric Society with robust, energy-saving memory solutions
Non-volatile memories such as MRAM and eNVM are coming more strongly into focus in the All Electric Society, because they secure data even without a permanent power supply and at the same time enable energy-efficient, robust electronics. Particularly in connected industrial, energy and edge applications, they are regarded as a key building block for greater resilience, security and system availability.
Non-volatile memories such as MRAM and eNVM are gaining importance in the All Electric Society, because they make controls, sensors and edge systems immediately operational again even after a power failure, while also reducing standby consumption. Current trends range from embedded NVM in microcontrollers through MRAM as a robust alternative to flash to eNVM for safety-critical industrial, energy and automotive applications.
The EU Cyber Resilience Act increases the pressure for hardware-based security functions, secure update capability and resilient data retention across the entire product lifecycle. This speaks in favour of MRAM and eNVM, because they preserve configuration data, logs and key material without an additional power supply and thus make security by design in connected devices easier.
From the point of view of semiconductor technology, integration into advanced process nodes, lower write voltages, higher endurance and better scalability of embedded solutions are currently particularly relevant. In parallel, the focus is shifting to energy-efficient architectures for edge AI and industrial IoT, where MRAM and other eNVM approaches are convincing less as a mass replacement for flash than as specialised devices for robust, low-power electronics.
Find out about the extensive range of non-volatile memories in EBV’s portfolio.
More efficiency, more security, more integration: PMICs are changing the power supply of modern systems
The electrification of industry, mobility and infrastructure increases the pressure on power supply electronics to become ever more efficient, compact and intelligent. This is exactly where advances in power management ICs and integrated voltage regulators come in, which as invisible key building blocks of the All Electric Society are what make new applications reliably possible in the first place.
Advances in power management ICs and integrated voltage regulators are what make electrification efficient, compact and system-capable. Current trends range from higher integration density through finely scalable multi-rail supply to better efficiencies, smaller designs and more closely coupled protection and diagnostic functions. Also particularly relevant are the closer integration with GaN and SiC power paths and the growing role of PMICs in AI edge devices, industrial electronics, energy storage and connected infrastructures. At the same time, the EU Cyber Resilience Act puts manufacturers under pressure to consider security by design, update capability and vulnerability management at chip and firmware level. This shifts PMICs and voltage regulators from pure supply components to security- and compliance-critical system building blocks. In semiconductor technology, system-in-package approaches, heterointegration, digital control and the coupling of energy efficiency with functional safety currently dominate.
Find out about EBV’s portfolio of the most current PMICs from the leading manufacturers.
Solutions
EBV Embedded Solutions
We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

Resources
EBV Podcast
Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.