Custom Meta Tags

Hero Banner

Pressure Sensors: The Design Engineers' Guide

Long Copy

Pressure sensors for different media types

Applications

Water-Pressure-Tank-Diagram-EN-Image

Water pressure sensors are often used to measure the level of water in a tank, or the rate of change in that level (as shown in the diagram on the right). The sensor is fitted to the top of an open-ended tube submerged within the container. As the water level rises, the air above the water in the tube is compressed, increasing the pressure on the sensor. An analogue-to-digital convertor (ADC) is used to convert the signal from the sensor into a digital value.

They can also be used to gauge the pressure in pipes where water is flowing – for example, in water distribution systems, to automatically determine whether pumps need to be activated to increase the flow rate.

And they can be used to gauge the depth of a submerged object – for example, in deep-sea diving.

Measurement options

Water pressure sensors can measure pressure in several different ways:

  • Absolute water pressure is measured against zero. This is similar to the way gas pressure sensors measure gas pressure as compared with a vacuum.
  • Gauge pressure measures water pressure against the atmospheric pressure around the sensor. If the water pressure sensor is completely submerged in water, a vent line is used to allow air from above the surface to enter the sensor, to provide the reading for atmospheric pressure. The vent line can often be run through the power cable supplying the sensor.
  • Differential pressure reflects the difference between two bodies of water – for example, in two separate tanks or containers, or two water pipes. This can be used to measure pressure drops across filters, or measure flow rates by measuring the difference in pressure across a restriction.

Technology

Water pressure sensors are transducers, generating an electrical signal in proportion to the pressure they measure.

Switching-Water-Pressure-Sensor-EN-Image
A typical water pressure switch

Water pressure sensors typically contain a physical diaphragm, often made of silicon, which bends as pressure is applied. The diaphragm is a strain gauge, which varies its electrical resistance when force is applied. This resistance is used to modify the output voltage of the sensor.

Some water pressure sensors provide zero-based outputs, where zero pressure results in no output signal at all. For example, their output might be in the range 0–5V. Others offer voltage at zero pressure, with a range such as 1–5V.

One drawback of zero-based output is the difficulty of identifying problems with the sensor itself. For example, in a water-pumping system, a pump might be configured to activate when the water pressure rises above a certain point, perhaps indicating that a certain depth of water has accumulated. If the water pressure sensor has a 0V signal, that might indicate zero pressure – or the sensor may have failed completely, which would mean that the pump did not activate as water levels rose, perhaps leading to a flood. In contrast, a zero reading from a ‘voltage at zero pressure’ sensor would clearly indicate a fault.

Options and specifications

Specifications to consider when choosing a water pressure sensor include:

  • Type of measurement (absolute vs. gauge)
  • Pressure measurement range
  • Accuracy (usually expressed as a percentage)
  • Media compatibility
  • Moisture resistance
  • Operating temperature range
  • Venting (see below)
  • Vibration resistance

For wireless water pressure sensors, additional relevant options are:

  • Transmitter wiring (cable or flying lead)
  • Transmitter accuracy
  • Radio frequency
  • Electromagnetic interference

Sensors that measure gauge pressure must be vented, so you may need to consider sealing methods for outdoor applications, high-pressure water jets (in a car wash or industrial process, for example), or where the sensor will be exposed to a lot of water vapour. An alternative is to use a sealed gauge, or a sensor that measures absolute pressure.

Pumping systems may sometimes be subject to ‘water-hammer’, where the opening or closing of valves sends a shock-wave through the water, causing a pressure transient or pressure spike that may exceed the measurement range of the sensor. To protect against this, some sensors can be fitted with restrictor plugs to slow down water flow and mitigate the effects of the spike.

Some water pressure sensors can indicate that they have developed a fault by sending their signal output out of range (either below the lowest point or above the highest point). In pumping applications, this can help to prevent flooding, or protect the pump from running dry or incurring extra damage.

Limitations

Since water pressure sensors may come into contact with different kinds of water, you may want to consider their suitability for different pH levels (acidic or alkaline), salt water, chemicals or other contaminants.

Not all pressure sensors may be suitable for use with potable (drinking) water. The regulations concerning what materials can come into contact with drinking water vary from country to country.

If you want to learn more about the different types of media that pressure sensors can measure, the applications of each type, and the different sensor options for your design, click the links below to jump to the section you're interested in.


Looking for more on pressure sensor technology? Check out the further chapters of this guide below, or if you're pressed for time you can download it in a PDF format here.

Pressure-Sensors-Guide-Download-CTA-EN-Image

Pressure Sensors Contact GBL

Need some advice on pressure sensors?

Our pressure sensor experts are on hand to help you make the right choice for your application.

Right Rail Card Dark

Webinar

Discover the keys to designing pressure sensor applications with this 30-minute technical presentation and Q&A with Nicholas Argyle, Applications Engineer EMEA, TE Connectivity.

Watch On Demand

Right Rail Card Dark_1

White paper

Need a more digestible introduction to pressure sensors? Download the white paper, 'Pressure sensors: Design considerations and technology options'.

Download

Right Rail Card Dark_2

Sensor solutions brochure

Discover the latest sensor solutions available from Avnet Abacus.

Download

Right Rail Card Dark_3-RB

Sensors linecard

Explore our pan-European sensor suppliers and their products and solutions.

Learn More

Right Rail Card Dark_3-KI

New products

Discover the latest product announcements from our sensor suppliers.

Learn More

Pressure Sensors Chapter 1 GBL

Chapter 1

How pressure sensors work

An introduction to pressure sensors covering the different types, how they work, their function, construction, and what to consider in your design choices.

Pressure sensors chapter 1 graphic

Pressure sensors chapter 5 GBL

Chapter 5

Types of pressure measurement

What’s the difference between absolute, gauge and differential pressure sensors? And how do you know which one to use?

Pressure sensors guide chapter 5 graphic

Pressure Sensors Chapter 2 GBL

Chapter 2

Pressure sensor applications

Discover the recent innovations in pressure sensor technology that are enabling smarter, safer, and more environmentally friendly electronics for businesses and consumers alike.

Pressure sensor guide chapter 2 graphic

Pressure sensors chapter 6 GBL

Chapter 6

The core pressure sensor technologies

What’s the difference between the different pressure sensor technologies? And how do you know which one to use?

Pressure sensor guide chapter 6 graphic

Pressure Sensors Chapter 3 GBL

Chapter 3

The different types of pressure sensors

Discover how pressure sensors vary according to the type of pressure measurement, sensing principles, output signal, media, MEMS technology, mounting and more.

Pressure sensor guide chapter 3 graphic

Pressure sensors chapter 8 GBL

Chapter 8

Pressure sensing in harsh environments

An in-depth guide to pressure sensors for harsh environments - designing for extreme temperatures, high pressure, and corrosive and dynamic environments.

Pressure sensor guide chapter 8 graphic

Pressure sensors chapter 4 GBL

Chapter 4

Pressure sensor output signals

Sensors, transducers, or transmitters? The right selection is important for your application. So what's the difference and how do you choose between them?

Pressure sensor guide chapter 4 graphic

Pressure sensors chapter 9 GBL

Chapter 9

Understanding specifications

Explore the datasheet and the different factors affecting the accuracy of pressure sensor readings. Discover how to make the right choice for your application.

Pressure sensor guide chapter 9 graphic

NPI Product Table

Image Product Description Link New

Static HTML