Pressure Sensors: The Design Engineer's Guide

Pressure sensors: 8 life-saving medical applications

Many medical devices now depend on accurate and stable pressure measurements in order to operate reliably. What’s more, patient care is expanding beyond the hospital and the GP‘s surgery and arriving in patients’ homes, in the form of home health monitoring.

As a result, developing with pressure sensors has become an integral part of designing medical applications. Below, we explore 8 different uses of pressure sensors in medical technology.
 

1. Getting the mix right in medical ventilators

A ventilator works by mixing air with pure oxygen to help the respiratory function of a patient. Differential or gauge pressure sensors are normally sited between valves and regulators to ensure the air and oxygen are mixed in the right quantities (see diagram below). In this kind of application, small surface-mount sensors are ideal; they will typically be specified for a pressure range of 2in or 5in H2O and are available with either analog or digital (I2C) outputs.

Despite being small and low power, these low pressure sensors can often include an integrated DSP (digital Signal processor) for compensating for non-linearity, offsets or the effects of temperature.
 

2. Monitoring oxygen therapy effectiveness

Oxygen therapy comes in a number of forms, as concentrated oxygen can be an effective initial treatment for asthma, bronchitis and oedemas, as well as heart failure.

Oxygen therapy systems use differential pressure sensors at several points in the system to monitor the pressure of the oxygen as it is mixed with atmospheric air. These sites are usually at the outlet of the oxygen tank, inline with the pressure regulator, and next to the flow control valve (see diagram below).

A diagram showing how differential pressure sensors are used in an oxygen concentrator
Pressure sensors are used at multiple points in an oxygen concentrator to monitor oxygen pressure

The pressures sensors in this application are likely to be differential pressure sensors with a scale of up to 4 kPa.
 

3. Delivering hyperbaric therapy

Raising the air pressure in a sealed chamber containing a patient is known as hyperbaric therapy and can be effective for a number of conditions. It is used to treat decompression sickness experienced by divers, and can also help patients with skin grafts or burn injuries. It can also be effective in treating carbon monoxide poisoning and even some necrotising infections.

Pressure sensors are used to monitor the pressure inside the chamber and control the amount of pressure applied during treatment. This will typically take the form of an absolute pressure sensor capable of measuring pressures up to around 100 kPa.

Even this most industrial of treatments is making inroads into patient’s homes, as ‘soft’ chambers become increasingly available - although the pressures these soft chambers can achieve are lower than the professional-grade ‘hard’ chambers. Typically, a soft chamber will require gauge pressure sensors capable of measuring around 0.3 to 0.5 bar, while a hard chamber would employ gauge pressure sensors able to measure as much as 6 bar.
 

4. Providing positive pressure masks to treat sleep apnoea

Sleep apnoea is a condition that causes the sufferer to stop breathing while asleep. Left untreated it can lead to a number of serious conditions, from chronic fatigue to potential heart failure.

The treatment involves using a device called a continuous positive air pressure machine, or CPAP, which delivers air at a positive pressure to a mask worn over the nose and mouth of the patient. An airflow pressure sensor is used to monitor the air pressure, detecting when the patient is breathing in and immediately turning on a fan to create positive pressure to open the airways (see diagram below). As the patient breathes out the fan is deactivated, allowing the patient to exhale without forcing them to fight against the positive pressure.

Sleep apnoea machines will likely employ a differential pressure sensor able to measure pressures up to 4 kPa.
 

  A diagram showing how pressure sensors are used to control drug deliveryHow pressure sensors are used to control drug delivery

5. Automating drug infusion

Drugs delivered in liquid form can be an effective form of treatment, as can other types of fluids e.g. for rehydration. These fluids can be administered either intravenously, subcutaneously or directly into a vein, and are typically delivered using infusion pumps. In order to ensure the correct volume of fluid is administered at the correct rate, the pumps use a number of sensors including gauge and differential pressure sensors, to closely monitor and control the flow of liquid.

Differential pressure sensors are used in drug delivery systems (see diagram to the right) to measure and control the flow of liquids into the patient. This ensures the right volume of drugs is delivered at the right time throughout the day and night, without the need for constant medical attention.

Differential pressure sensors are normally calibrated to measure flow rates in the range of 0.5 to 10.0 micro litres/min.
 

 

 

6-8. Measuring in vivo blood pressure, ex vivo blood pressure and intraocular pressure

In vivo blood pressure sensing involves implanting a sensor into the body. It can now be achieved using tiny absolute pressure sensors designed for this purpose.

Ex vivo blood pressure sensing, from outside the body, can be implemented using gauge pressure sensors to measure the blood pressure when the heart beats (systolic) and between the heart’s beats (diastolic).

Sensors for both in vivo and ex vivo blood pressure sensing need to be able to measure pressures up to 300 mm Hg (maximum). In vivo applications tend to use absolute pressure sensors, while ex vivo favour gauge pressure sensors.

MEMS-based gauge pressure sensors are now being used to measure the intraocular pressure of a patient’s eyes, which is particularly important after an operation to replace a cataract.

Manufacturers are now producing an ever-widening range of pressure sensors for medical applications, including disposable pressure sensors based on MEMS technology that can be used inside the body or in-line with fluids entering the body. These are produced in clean rooms and in accordance with industry-accepted guidelines including those generated by the Association for the Advancement of Medical Instrumentation (AAMI).

Pressure sensors have become an essential element of medical care, providing accurate and stable measurement of critical pressure levels in gas and liquids within the body and in treatments being applied to patients.

Future developments will enable more sophisticated, and ever smaller medical equipment to be developed, as well as lowering the price point for home-use devices.

One significant result will be an elevated quality of life for an ageing population.
 

What else are pressure sensors used for?

Find out more in our articles on applications in automotive, building automation, consumer and wearables, medical and industrial applications.

Pressure sensors: 10 innovative automotive applications.

Pressure sensors: 8 building automation applications.

Pressure sensors: 11 life-enhancing consumer applications.

Pressure sensors: 3 applications enabling smart factories in Industry 4.0.

Looking for more on pressure sensor technology? Check out the further chapters of this guide below, or if you're pressed for time you can download it in a PDF format here.

Need some advice on pressure sensors?

Our pressure sensor experts are on hand to help you make the right choice for your application.

Webinar

Discover the keys to designing pressure sensor applications with this 30-minute technical presentation and Q&A with Nicholas Argyle, Applications Engineer EMEA, TE Connectivity.

Watch On Demand

White paper

Need a more digestible introduction to pressure sensors? Download the white paper, 'Pressure sensors: Design considerations and technology options'.

Download

Sensor solutions brochure

Discover the latest sensor solutions available from Avnet Abacus.

Download

Sensors linecard

Explore our pan-European sensor suppliers and their products and solutions.

Learn More

New products

Discover the latest product announcements from our sensor suppliers.

Learn More
 

 

Bourns

BPS125 series digital ultra-low pressure sensor

The BPS125 line has been designed to provide high sensitivity/accuracy, long-term reliability and ultra-low pressure sensing with a digital output (I2C).

TE Connectivity 1620 Series AAMI Pressure Sensor Product Spotlight

Display portlet menu

TE Connectivity

1620 series AAMI compliant medical pressure sensor

TE Connectivity's 1620 series disposable pressure sensor is a fully piezoresistive silicon pressure sensor for use in invasive blood pressure monitoring.

TE Connectivity 1620 Series AAMI Pressure Sensor

SMI SM4000-SM1000 Series Spotlight

Display portlet menu

TE Connectivity's SMI Pressure Sensors

SM4000 / SM1000 series gage and differential pressure sensors

The SM4000 and SM1000 medium pressure MEMS sensors offer gage and differential pressure measurement from 2.5PSI to 30PSI providing a calibrated and temperature compensated digital or digital and analog output signal.

Pressure Sensors Chapter 1 GBL

Display portlet menu

Chapter 1

How pressure sensors work

An introduction to pressure sensors covering the different types, how they work, their function, construction, and what to consider in your design choices.

Pressure sensors chapter 1 graphic

Pressure sensors chapter 6 GBL

Display portlet menu

Chapter 6

The core pressure sensor technologies

What’s the difference between the different pressure sensor technologies? And how do you know which one to use?

Pressure sensor guide chapter 6 graphic

Pressure Sensors Chapter 3 GBL

Display portlet menu

Chapter 3

The different types of pressure sensors

Discover how pressure sensors vary according to the type of pressure measurement, sensing principles, output signal, media, MEMS technology, mounting and more.

Pressure sensor guide chapter 3 graphic

Pressure sensors chapter 7 GBL

Display portlet menu

Chapter 7

Pressure sensors for different media types

An in-depth guide to pressure sensors for different media types. Learn about the technology, applications, different options, their specifications and their limitations.

Pressure sensor guide chapter 7 graphic

Pressure sensors chapter 4 GBL

Display portlet menu

Chapter 4

Pressure sensor output signals

Sensors, transducers, or transmitters? The right selection is important for your application. So what's the difference and how do you choose between them?

Pressure sensor guide chapter 4 graphic

Pressure sensors chapter 8 GBL

Display portlet menu

Chapter 8

Pressure sensing in harsh environments

An in-depth guide to pressure sensors for harsh environments - designing for extreme temperatures, high pressure, and corrosive and dynamic environments.

Pressure sensor guide chapter 8 graphic

Pressure sensors chapter 5 GBL

Display portlet menu

Chapter 5

Types of pressure measurement

What’s the difference between absolute, gauge and differential pressure sensors? And how do you know which one to use?

Pressure sensors guide chapter 5 graphic

Pressure sensors chapter 9 GBL

Display portlet menu

Chapter 9

Understanding specifications

Explore the datasheet and the different factors affecting the accuracy of pressure sensor readings. Discover how to make the right choice for your application.

Pressure sensor guide chapter 9 graphic
Image Product Description Link New