Custom Meta Tags

Hero Banner

Automotive: The Design Engineer's Guide

Long Copy

Electric vehicle (EV) on-board chargers

 
Figure 1: Plug-in hybrids and battery electric vehicles offer the greatest fuel saving, and the ability to recharge from the grid

While safety, reliability, and comfort are all important when choosing a vehicle, with plug-in hybrid electric vehicles (PHEVs) and battery electric vehicles (BEVs) there’s another critical factor to consider; the time taken to charge. While replenishing an internal combustion engine (ICE) vehicle takes just a few minutes, the time needed to replenish the motive battery on PHEVs and BEVs is significantly longer.

Several types of electric power are now available. Hybrid vehicles have both a fossil fuel powered drivetrain and an electric drivetrain which can be organised in different ways. Some types, such as mild hybrid, have a smaller battery and this is charged from a combination of the ICE and a generator. And regenerative braking provides some charge to extend the range while the vehicle is slowing down and the motor acts in reverse as a generator. PHEVs and BEVs include the ability to plug in to the mains grid and recharge the battery from there, while the vehicle is stationary. 

 

Overview of EV charging

The Society of Automobile Engineers (SAE) has defined the primary types of charging available for EVs in its SAE J 1772 standard. The standard contains estimated charging times, however these can only be taken as a rough guide, as there are many influential factors, including the state of charge (SOC) of the battery and the efficiency of the charger.

Table

SAE charging configurations and ratings terminology
AC level 1 (SAE J1772™) PEV includes on-board charger *DC level 1 EVSE includes an off-board charger
120 V, 1.4 kW (12 A)
120 V, 1.9 kW (16 A)
200-450 VDC, up to 36 kW (80A)
Est. charge time: Est. charge time (20 kW off-board charge):
     PHEV: 7 hrs (SOC* - 0% to full)      PHEV: 22 mins (SOC* - 0% to  80%)
     BEV: 17 hrs (SOC - 20% to full)      BEV: 1.2 hrs (SOC - 20% to 100%)
AC level 2 (SAE J1772™) PEV includes on-board charger (see below for different types) *DC level 2 EVSE includes an off-board charger
240 V, up to 19.2 kW (80A) 200-450 VDC, up to 90 kW (200A)
Est. charge time (3.3 kW on-board charger) Est. charge time (45 kW off-board charger)
     PHEV: 3 hrs (SOC* - 0% to full)      PHEV: 10 mins (SOC* - 0% to 80%)
     BEV: 7 hrs (SOC - 20% to full)      BEV: 20 mins (SOC - 20% to 80%)
Est. charg time (7 kW on-board charger)
     PHEV: 1.5 hrs (SOC* - 0% to full) *DC level 3 (TBD) EVSE includes an off-board charger
     BEV: 3.5 hrs (SOC - 20% to full) 200-600V DC (proposed) up to 240 kW (400 A)
Est. charge time (20 kW on-board charger) Est charge time (45 kW off-board charger)
     PHEV: 22 mins (SOC* - 0% to full) BEV (only): <10 mins (SOC* - 0% to 80%)
     BEV: 1.2 hrs (SOC - 20% to full)  
*AC level 3 (TBD) > 20 kW, single phase and 3 phase
*Not finalised
Voltages are nominal configuration voltages, not coupler ratings
Rated power is at norminal configuration operating voltage and coupler rated current
Ideal charge times assume 90% efficient chargers, 150W to 12V loads and no balancing of Traction Battery Pack
Notes:
1) BEV (25 kWh usable pack size) charging always starts at 20% SOC, faster than a 1C rate (total capacity charged in one hour) will also stop at 80% SOC insteadof 100%
2) PHEV can start from 0% SOC since the hybrid mode is available


Figure 2: SAE J1772 defines the various types of charging available for PHEVs and EVs

Long Copy_1

Primarily, charging can be either AC or DC. The battery requires DC to charge, so, in AC charging, a conversion is needed between the charging socket and the battery, while with DC charging the vehicle is plugged directly into DC that can be fed to the battery. The various ‘levels’ relate to the amount of power that can be delivered, and this, in turn, relates to the power source. The higher the level, the more power that’s available and the shorter the charging time.

The other key difference is where the charger is located. In DC charging, the charger is external to the vehicle and all power conditioning (including rectification) is done outside the vehicle. DC charging tends to have the highest power ratings and is used for many commercial / public charging stations, such as those found on the forecourts of gas stations or beside the highway.

AC charging typically includes an on-board charger that moves around with the vehicle. The AC charger receives the mains via a charging cable and connector and converts this to a DC voltage at the appropriate level.

Charging typically breaks down into three types, based upon the activity / lifestyle of the vehicle user. ‘Main harbour’ charging refers to charging at or near a home or workplace while ‘destination’ charging includes charging when the vehicle is parked somewhere while an activity takes place. Examples include restaurants, shopping malls, sports stadia, etc. Both of these categories typically provide AC power and rely on on-board charging while the final charging type (‘range extension’ charging) uses DC power at very high levels. Range extension charging is similar to fuel stations and allows vehicles to be rapidly recharged during a journey.
 

Benefits of on-board charging

The major benefit of on-board charging is that it uses readily-available AC power and, via an extension lead, the vehicle can be plugged into any of the billions of outlets installed in every building.

Level 1 AC charging makes use of a single-phase supply and it’s this that limits the power available to around 1.9kW with a 120V supply, and 3.7kW with a 220-240V supply. This is the most common type of charging available in private residences.

Businesses, however, often have three-phase electricity available and using this for charging will increase the available power to around 20kW which offers far more rapid charging than Level 1.

AC charging is the most flexible, as charging points are available and can provide the entire charging needs for some users, depending upon their lifestyle and how the vehicle is used. If the vehicle is solely used for commuting during the day, then charging the vehicle overnight is very convenient. AC charging is far less suited to range extension charging, where the distance to travel exceeds the range of the vehicle, as the charging times are simply too long.
 

Requirements for an on-board charger

The primary role of an on-board charger (OBC) is to manage the flow of electricity from the grid to the battery. This means that the OBC must comply with the requirements of the grid in locations where it will be used. The primary requirement is not to inject reactive power back onto the grid, which is achieved by having a power factor (PF) of >0.9. The OBC must also suit the types of charger available, meaning that it has to support single-phase and 3-phase operation.

There will also be requirements to provide isolation from the power source and a maximum current that the grid can deliver, which must be factored in to the design. As with all power systems, there is a potential to generate electromagnetic interference, so all relevant EMC standards must be complied with. At this power level, the ability to communicate with the grid is also necessary.


Figure 3: A Block diagram of a typical on-board charger

Because the OBC is permanently mounted, the weight must be minimised, to reduce its impact on the range of the vehicle. Efficiency is also important, and there are other benefits to efficiency too, such as requiring less thermal management which will reduce the size, weight and cost of the OBC.

In future, it may be possible to use the vehicle as a portable energy store, using the energy stored in the battery to power the home during times of peak demand or high electricity costs. The battery would then be replenished at times of cheaper electricity. This would save money for the home owner and help the electricity companies by balancing the load on the grid. In order to facilitate this, the OBC would need to return energy to the grid through an inverter.

The benefits of wireless charging could apply equally to vehicles as they do to smaller portable devices such as smartphones or tablets, especially to add a ‘top up’ charge to extend their range. Wireless technology will be particularly appropriate to vehicles that follow pre-determined routes, or often wait at a specific place, because the charging stations will be fixed. This would include buses that follow specific routes stopping at the same bus stop and taxis that wait at a taxi stand (perhaps at an airport or railway station).
 

Design challenges

Designing for power systems is generally a constant challenge to meet high efficiency requirements in a small space and this is particularly true in the case of OBCs. The efficiency of the OBC is particularly important as it can reduce charging time.

The more efficient the OBC design, the less waste heat is generated during charging which reduces the need for thermal management. If it becomes necessary to add heatsinks to an OBC design then the size and weight will increase, neither of which are desirable within the confined spaces of a modern car – especially as weight decreases the overall efficiency of the vehicle.

Regulatory compliance is a challenge with OBCs, particularly with the need to meet power factor rules for the grid when the vehicle is plugged in for charging. Commonly a boost converter is used for power factor correction (PFC) to rectify the AC input and deliver a high-level DC voltage to a DC-DC converter that’s used to charge the EV battery.

Any design for an automotive application has to take account of the harsh environment of the vehicle. Designers are required to produce designs that are able to cope with prolonged vibration, heat, cold and significant amounts of conducted and radiated electrical noise.
 

Passive components for OBCs

Passive devices such as magnetic components and capacitors play a pivotal role within all aspects of OBCs. The boost converter that forms the front-end of the PFC stage will contain a common-mode EMC filter, filter capacitors, PFC coils and a DC Link capacitor that provides a charge reservoir between the boost stage and the DC-DC converter.

LLC converters are widely used in industrial and consumer applications and, although there is no specific output choke used, magnetic components are used for an isolating transformer and output EMC filter, along with various capacitors.

The potential to adopt wireless charging brings a wider requirement for passive components including the coils for power transfer (transmit and receive), such as the one shown on the right, and proximity detectors to ensure that the vehicle is correctly aligned with the charger.

While many recent advancements in power electronics have been centred on semiconductor devices such as MOSFETs and IGBTs and their associated control, very few of these would be able to achieve their full potential without corresponding increases in performance of the passive devices that they rely on as well as connectors and cabling.

In many applications, multiple resistors are used in parallel, simply to handle the required power dissipation. While this provides a solution at the circuit level it increases the component count, cost and board space required – none of which is ideal in an automotive setting. One recent innovation is the first high-power resistors that are offered with an AEC-Q200 qualification (left). These 1% tolerance devices are supplied in an insulated package designed to be mounted directly to a heatsink where they are rated at up to 800 W. This high-power dissipation allows multiple lower powered devices to be replaced by a single resistor, or (due to their pulse capability) larger wirewound resistors can be replaced, saving board space. 

Inductors are one component that, if not selected carefully, can be damaged by prolonged exposure to heat and vibration. However, rugged types that are qualified to AEC-Q200 are available such as metal composite power chokes that are needed for step-up and step-down operation as well as filtering. The latest versions offer high vibration resistance and are able to operate at temperatures as high as 150°C (including self-heating) while maintaining excellent inductance stability over this extended temperature range. The shielded construction virtually eliminates flux leakage, thereby minimising any EMI issues. 
 

Summary

On-board charging is, and will remain, an important aspect of all EVs for the foreseeable future as, while it is slower than the rapid DC chargers, it allows greater flexibility to charge (or top-up) vehicles from commonly available power points. However, while the vehicle is in motion, the OBC has no function and if it’s excessively large or heavy, then all it does is reduce range.

Consequently, designers are being challenged to design OBCs that are not only highly efficient in operation but also small and lightweight. They must be able to cope with the rigours of the automotive environment (heat and vibration among others) as well as being able to be produced at a cost point that meets the aggressive demands of auto makers.

While passive components may be simple in nature, they have a pivotal role in helping designers meet these challenging objectives, and the market is developing rapidly to meet increasing demands in this space. The choice on offer is substantial, and choosing appropriately is key.

Below we’ve highlighted our leading suppliers of components for on-board charger applications.

If you require advice on selecting the right components for your design, our technical specialists are on hand to help.

 

Featured suppliers

Static HTML

EV charging solutions Static HTML_1

Automotive solution Ask An Expert Spotlight

Engineering Services

Ready to start the engine of your automotive design?

Our automotive specialists are on hand to provide technical and product support you need.

Grid Box Dark_2

Focus magazine

Automotive design: accelerating innovation

This edition of Focus magazine addresses these challenges from each perspective.

Automotive-City-Car-EN-Image

EBV Infineon CoolSiC GBD

Semiconductor solutions

Infineon CoolSiC™ MOSFETs and Diodes from EBV

Now is the time to discover the benefits of silicon carbide (SiC). Drive down system costs and improve reliability and performance with Infineon's CoolSiC™ solutions.

Grid Box Dark

Technology solutions

Passive components for SiC and GaN applications

Passive component manufacturers are responding to developments in SiC and GaN applications with product specifications to fully exploit these wide band-gap semiconductor innovations. Learn about these developments and view our product portfolio.

Grid Box Light_3-ET

Amphenol Communication Solution

Amphenol has developed a broad range of innovative connector solutions to support automotive designs, specialising in plating, signal integrity performance, and power management.

Grid Box Light

Murata-Logo-Automotive-campaign-EN-Image

Empowering innovative automotive systems with the latest passive, power and sensor solutions.

Grid Box Light_1

Yageo-Logo-Automotive-campaign-EN-Image

Increasing automotive system with the latest passive components solutions

Grid Box Light_3-XM

Bourns Logo

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products.

Grid Box Light_3-IF

TDK-Logo-Automotive-campaign-EN-Image

TDK automotive solutions include not only standard components, but also application-specific solutions, which are developed together with our customers.

Molex GBL

Integrating automotive systems with the latest connection systems, electronics and software solutions

Grid Box Light_3-VX

Panasonic Industry logo

Panasonic offers large eco-friendly, reliable, comfortable and safe range of automotive electronic components solutions.