Understanding Micro Switches And Hysteresis | Avnet Abacus

Understanding Micro Switches And Hysteresis | Avnet Abacus

Understanding micro switches and hysteresis

Giovanna Monari Photo

The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho


The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a household or business premises where you won’t find at least one, and probably many more.  They’re used in doors to sense an ‘open’ or ‘closed’ state, in vending machines to detect the dropping of coins, in printers and photocopiers, franking machines, and pressure switches for process applications.

Snap action micro switches, the most common type, often use an actuating lever to produce fast switching with very little physical pressure upon the actuator. With industrial versions capable of operating for 10 million cycles or more, and even low-cost consumer types capable of at least one million operations, they’re found in a huge range of applications, including in lamps, solenoids, motors, and flow and pressure switches. The actuator acts as a lever, with a small force applied to its free end being translated into a larger force as you move towards the pivot end, where it rests upon a plunger, or pin. Even when force is applied to the actuator very slowly, its amplifying effect means that the movement of the switch contacts is always very fast – a desirable characteristic in any switch.

This 4-minute video gives a clear, simple explanation of how micro switches are built and how they work.  

 

 

MicroSwitch

Cutaway showing the internal construction of a micro switch (Attribution: Benjamin D. Esham / Wikimedia Commons)

In operation, micro switches exhibit hysteresis. Wikipedia defines hysteresis as “the dependence of the output of a system not only on its current input, but also on its history of past inputs. The dependence arises because the history affects the value of an internal state.”

In micro switches, it’s easiest to think of it like this. When the actuator is depressed, there is a point at which the switch activates, connecting the Common contact to the normally open (NO) contact. As pressure on the actuator decreases, the point at which the switch reverts to its non-activated state, with the Common contact falling back onto the normally closed (NC) contact, is not the same as the activation point, it’s later. The distance between the actuating point and the release point is called differential movement, or hysteresis.

PressureSwitch

As pressure increases in the chamber the membrane deforms, bulging outwards to depress the lever on the micro switch (not to scale)

 

Actuators

Actuators come in a variety of forms, as shown on these Omron micro switches

 

 

 

 

 

 

 

 


In many instances this short time delay is a good thing. In fact, hysteresis is often deliberately introduced into electronic circuits to prevent  “chattering” of switches as they oscillate around a defined set point. However, in a few applications, excess hysteresis can be a disadvantage. This is particularly true for mechanical pressure and temperature switches, like the one shown here.

The temperature or pressure build-up is slow in most process applications. Hysteresis, sometimes called “differential movement”, means that the point at which the micro switch actuates as the pressure increases will be different from the point at which actuation is reversed under conditions of decreasing pressure. Hysteresis is a disadvantage here because it limits the resolution of the pressure switch. In other words, it limits the system’s ability to detect very small changes in pressure.  Some micro switches exhibit less hysteresis than others and the figure is not always shown in the data sheet so it may be worth asking if this aspect of performance is critical to your application. 

We stock a variety of these components from ALPS, C&K, Eledis, Omron & Panasonic. They come in a choice of styles with quick-connect, solder, or flying lead terminals and some versions are IP67 rated - sealed for use in harsh environments. Various actuators can be specified too – pin plungers, hinged levers, hinged roller levers, and simulated rollers levers are examples.

Applications advice from our technical specialists is always available, just click the Ask an Expert button to get in touch.

 

 

 

 

 

 

Want more like this? Sign up for our newsletters

About Author

Giovanna Monari Photo
Giovanna Monari

As a Senior Product Manager, Giovanna is responsible for marketing strategy and supplier management ...

Understanding Micro Switches And Hysteresis | Avnet Abacus

Engineering Services

Ask an expert

Have a question? Our regional technical specialists are on hand to help

Ask-an-Expert-EN-Image

Understanding Micro Switches And Hysteresis | Avnet Abacus

Related Articles

No related articles found

Understanding Micro Switches And Hysteresis | Avnet Abacus

Related Events

Related Designs Menu