Avnet Displays and SiS: delivering excellence together

Avnet Displays and SiS: delivering excellence together

Avnet Displays and SiS: delivering excellence together

Nishant Nishant
Silicon Integrated Systems wallpaper

As you might imagine, we are very particular when it comes to who we partner with. After all, we have an impeccable track record for giving our customers the very best displays. So, we’d like to introduce you to Silicon Integrated Systems (SiS), whose specialised firmware and hardware meets our every expectation – and yours.

The SiS 95xx series of Projected Capacitive (PCAP) touchscreen controller ICs, in particular, really stood out to our display engineers. Primarily for their reliability and functionality, but also for a set of features that are designed with industrial, commercial, and embedded touch applications in mind.

  • Dual Core IC with Integrated DSP for high-speed data processing and real-time performance
  • Works with 18V, minimising irradiated noise emissions, ensuring low interference
  • High-Speed Analog Data Acquisition for a superior signal-to-noise ratio (SNR) of 1 to 24
  • Real-Time Signal Analysis with FFT gives precise and reliable operation in any environment
  • Thick Surface Handling for touch functionality on surfaces of up to 10mm
  • Glove Recognition automatically detects, but also adjusts by usage
  • Water Compatibility functions flawlessly in multi-touch mode, even with water on the surface.

Contact us


Impressed? Us too. Especially when we looked at some of the standout features that SiS offer in the context of products and industries:

Home Automation

This is an area where stability and resilience really matter, so SiS developed a specialised firmware with GPIO functionality for just this purpose. For example, when a computer system becomes unresponsive, the solution lets users reset the board unit by simply touching a designated area of the touchscreen for a specified duration. This triggers the GPIO to activate a relay that resets the entire system, which we think you’ll agree is an easy, practical and effective safeguard to minimise downtime.

Agriculture and Automotive

In agricultural and automotive applications, there are rigorous standards around electromagnetic interference (EMI) and electromagnetic compatibility (EMC) and meeting them is crucial. The specialised firmware in SiS solutions is designed to minimise EMI, making our devices fully compliant with automotive-grade irradiation tests and EMC standards, including the demanding 150V/m test.

White Goods and Ticket Machines

Where easy maintenance is a must, air gap solutions are a dream. Unlike traditional laminated setups, the cover glass isn’t laminated on the projected capacitive (PCAP) touchscreen and it’s this ‘modular’ approach which allows customers to replace the cover glass themselves without requiring specialist tools or a cleanroom environment. This makes for a big reduction in downtime and maintenance costs.

Coffee Machines

These often operate where there is a lot of electrical interference, which can disrupt how they communicate using I2C or USB connections. Smart firmware from SiS can detect when communication freezes, automatically waking up I2C or USB buses, keeping everything running smoothly even in noisy environments. Because we all know that even an extra minute waiting for a coffee can feel like ten, right?

Medical and High-Frequency Devices

Dentist systems and high-frequency surgical devices are known to create extremely high levels of noise, which can cause the phenomenon of ‘phantom touches’. These compromise usability – which is the very last thing you want in critical medical scenarios. Thankfully, SiS solutions are engineered with these potential issues in mind and ensure accurate and reliable touch responses, even in high noise environments.

 

Working on a displays project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

About Author

Nishant Nishant
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Avnet Displays and SiS: delivering excellence together

Avnet Displays and SiS: delivering excellence together

Related Articles
DEEPX webinar image teaser shows DEEPX AI modules
Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem
By Michaël Uyttersprot   -   March 17, 2026
Learn how you can enable efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem.
Microsoft logo
SQL Server IoT 2025: Bringing AI and Enhanced Analytics to Edge Data
By Yann Stridde   -   February 5, 2026
Organisations are feeling increasing pressure to process information directly at the edge

Avnet Displays and SiS: delivering excellence together