Custom Meta Tags

Wireless Connectivity Hero Banner

Wireless & Connectivity

DECT (LC)

DECT

Nordic Semiconductor logo
Renesas logo

Digital Enhanced Cordless Telecommunications was introduced to the market in 1992.

It mainly uses the frequency bands 1880 to 1900 MHz, but due to extension of the ETSI also 2010-2025 MHz and 24-00 – 2480 MHz are specified.

Additionally, there are sub-sets specified such as DECT-ULE for ultra-low energy applications, DECT CAT-iq enhancing interoperability and IP-telephony with DECT.

Avnet Silica partners with market leader Renesas on DECT. For more details, please visit Renesas supplier page.

 

Products and features Chip Module Standard Cat-iq ULE URLLc NR+
Supplier
Nordic Semiconductor          
Renesas

Other technologies (GBL)

Other Wireless & Connectivity Technologies

WiFi (GBLS)

WiFi

Avnet Silica offers a full range of WiFi products, including chips, modules, and devices, as well as a full technology range from WiFi 4 to WiFi 6e. We also support routers and gateways.

SEE WIFI

GNSS (GBLS)

GNSS

Today GNSS technology is not only used for military and cars, but for many types of vehicle, in applications such as container tracking, animal and people tracking and logistics.

SEE GNSS

Antennas (GBLS)

ANTENNAS

Avnet Silica offers antennas from specialised suppliers, that focus solely on antenna design and production, such as Antenova and 2J Antenna, along with other suppliers that offer antennas as part of overall portfolio for wireless products, such as Quectel.

SEE ANTENNAS

Bluetooth (GBLS)

Bluetooth

Bluetooth is one of the most common wireless technologies in the market, propelled into the consumer world by the smartphone, as well as increased demand for fitness, health, and entertainment devices.

SEE BLUETOOTH

ISM (GBLS)

ISM 2.4GhZ and Sub-GHz

ISM radio bands are portions of the radio spectrum reserved internationally for industrial, scientific and medical (ISM) purposes. ISM Bands are license free and not available for Telecomm Applications, which are regulated.

SEE ISM 2.4GhZ and Sub-GHz

Router (GBLS)

ROUTER / GATEWAYS / MODEMS

Connecting short range wireless devices, or some wired devices to a wired or wireless infrastructure, requires bridging technologies, such as Modems, Gateways or Routers / Access Points.

SEE ROUTERS

Cellular (GBLS)

Cellular

Evolving from GSM to GPRS then to 3G (UMTS / WCDMA) we are now seeing global coverage with LTE / 4G, with next generation 5G leading the way in applications which require higher data transfer.

SEE CELLULAR

RFID (GBLS)

RFID / NFC

Radio Frequency Identification, is a technology that enables simple, secure and fast identification of things, persons and animals. It is mainly made for very short ranges, with one exception, the UHF based RFID called RAIN-RFID for mid range identification, used mainly in logistics.

SEE RFID / NFC

LPWAN (GBLS)

LPWAN

In Europe, major networks have announced their intention not to support 3G networks across Europe beyond 2020. We offer LPWAN technology from our market-leading suppliers, available in a range of modules.

SEE LPWAN

UWB (GBLS)

UWB / Ultrawide Band

Ultra-wideband is a radio technology that can use a very low energy level for short-range, high-bandwidth communications (approx. 500 MHz or 20% of the arithmetic center frequency) over a large portion of the radio spectrum. This co-existing with other radio standards is a major advantage.

SEE UWB / ULTRAWIDE BAND