Custom Meta Tags

Hero Banner

Wide Bandgap (SubNav)

Advantages of GaN Power Semiconductors (MT)

Advantages of GaN Power Semiconductors

Power electronics is a vitally important sector (LC)

Power electronics is a vitally important sector underpinning nearly all aspects of modern society.

PCB heating upGaN has superior thermal management properties compared to silicon

However, with ever-increasing demands for efficient, compact, and reliable systems, engineers must continually look to innovate and improve their designs.

Silicon has traditionally been the semiconductor material of choice and still commands a dominant share of the market. However, gallium nitride (GaN) is emerging as a strong contender for many applications, offering significant advantages over silicon. As a result, GaN is increasingly being chosen for a broad spectrum of power designs and is also making inroads into RF and optoelectronics.

The most common GaN device in power applications is the lateral high electron mobility transistor (HEMT), and in this article, we will look at some of the properties of GaN HEMTs, and the advantages compared to silicon MOSFETs.

Material properties of gallium nitride

GaN is a wide bandgap (WBG) material. This means that the gap between possible energy levels of its electrons is wider than it is in silicon: 3.4 eV for GaN, compared to just 1.1 eV in silicon.

To be able to conduct electricity, an electron in a semiconductor must cross the band gap to reach a higher energy state. The larger bandgap of GaN means that its devices have a higher breakdown voltage, as a greater electric field is needed to release electrons that can carry charge.

GaN's wide bandgap is not the only advantageous property it possesses. It also has greater electron mobility and a higher saturated electron drift velocity compared to silicon, which means that electrons can move more swiftly. This contributes to GaN's ability to operate at higher frequencies.

GaN semiconductors can be fabricated on various substrate materials, including silicon and silicon carbide (SiC). The choice of substrate can influence the GaN device's performance and introduces unique challenges during the manufacturing process.

Device-level properties of GaN semiconductors

Compared to silicon devices such as MOSFETs and IGBTs, the material properties of GaN devices give them an appealing mix of electrical properties.

GaN devices have a low drain-to-source on-state resistance (RDS(on)) compared to silicon, which reduces conduction losses and dissipated heat. GaN components also have no reverse recovery losses, and they have low gate charge compared to silicon, reducing losses and, hence, power consumption.

GaN's breakdown field strength is significantly higher than that of silicon — 3.3 MV/cm for GaN compared to 0.3 MV/cm for silicon. This provides GaN with an approximately ten-times advantage in handling higher voltages, allowing for the creation of significantly smaller devices for the same voltage handling.

Again, compared to silicon, the GaN alternatives offer shorter switch-off times and lower capacitance, both of which help to enable faster switching. GaN components also feature a low forward voltage drop and a robust intrinsic body diode.

Spot Power (GBL)

Technology

Power: designing solutions with power at the core

We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

Power - Power components lighting up on board

WBG (CO)

With the ongoing shift to renewable energy and the electrification of transport and industry, the demand for higher power and greater energy efficiency in electronics is increasing. Wide bandgap technologies including SiC and GaN bring many advantages.

WBG OVERVIEW

Board-level advantages of GaN power devices (LC)

Board-level advantages of GaN power devices

Due to the material- and device-level properties mentioned previously, GaN devices can operate at much higher switching frequencies than silicon. While specific switching speeds depend on the device design and application, GaN technology enables operation at frequencies significantly higher than traditional silicon devices, sometimes as high as 100 times faster, which minimises switching losses and can lead to improved performance in many applications.

Their ability to handle larger electric fields and higher breakdown voltage means that GaN-based devices can be made with a smaller footprint than silicon alternatives, with smaller and lighter components.

LOOKING FOR SUPPORT? CONTACT OUR POWER EXPERTS

System-level advantages of GaN semiconductors

Higher efficiency reduces energy consumption which, in turn, lowers both operational costs and the need for energy storage. This makes GaN particularly well suited to applications where power efficiency directly impacts system performance and therefore market value, such as consumer electronics, data centres, and electric vehicles (EVs).

A compact, high-power-density design is particularly valuable in space-constrained applications, including portable consumer devices, laptop and smartphone chargers, and automotive power electronics, where reducing size and weight is critical. The ability to integrate GaN into small-form-factor designs also enhances power adapters, fast-charging solutions, and point-of-load converters in computing and telecoms infrastructure.

While silicon or SiC may be better for high-power applications, emerging vertical GaN-on-GaN power devices offer higher breakdown voltages and current handling capabilities, extending GaN’s applicability to industrial power supplies and higher-voltage EV drivetrain components. The combination of high efficiency and fast switching speeds also makes GaN attractive for server power architectures and telecoms rectifiers, where reducing energy losses and thermal load improves overall system reliability, and reduces cooling requirements.

GaN’s ability to operate efficiently at elevated temperatures further enhances its suitability for automotive and industrial applications, where thermal constraints often dictate component selection and component cooling can be limited.

In RF and communication systems, GaN high-electron-mobility transistors (HEMTs) provide high linearity and low noise, making them ideal for 5G base stations, radar systems, and satellite communications. Their superior performance in high-frequency operation contributes to more efficient and compact RF power amplifiers, helping improve signal integrity and reducing power dissipation in high-frequency applications.

Additionally, the bidirectional capabilities of GaN HEMTs are valuable in circuit topologies that feature power flowing in both directions. Bidirectional functionality can offer advantages in some applications that use relays or solid-state switches.

Challenges in adoption of GaN technologies

While there is a lot of hype in the marketplace about GaN, it’s important to take a balanced approach to your design and consider the negatives as well.

GaN devices have historically been more expensive than silicon, but device vendors have steadily driven the price down. In some mid- to high-volume applications Avnet Silica can offer price parity with silicon. Furthermore, by using silicon substrates, GaN components can take advantage of the well-proven process steps used with silicon, and the cost advantages of economies of scale. Vendors have also taken steps to increase production volumes and to guarantee supply levels.

GaN is a more environmentally-friendly option than silicon, with the amount of energy required to make a GaN transistor around 10 or 20 times less than to make a silicon transistor1  — that’s before you even consider the significant energy savings (and hence carbon emission reductions) GaN delivers in its application due to its increased efficiency.

In terms of design, using GaN devices requires some re-thinking compared to existing silicon-based systems. Specifically, your system must be able to handle the higher switching frequencies of GaN — so you need to consider noise and EMC, as well as providing a suitable gate driver, and optimising the board layout to minimise parasitic inductances.

With GaN devices able to operate at higher temperatures than silicon, you also need to look at thermal management and cooling, and whether the high power density of GaN may cause issues with other components.

In practice, the choice of semiconductor material is often dictated by the voltage requirements of the application. While GaN has typically been used for systems up to approximately 650 V, advancements in the technology are anticipated to introduce higher voltage GaN semiconductors to the market, broadening potential uses. At present, for applications demanding voltages exceeding 1000 V, such as the traction inverters in EVs, silicon carbide (SiC) and silicon remain the more established solutions, though this may change as GaN technology progresses.

Making the right choice

For many power applications, GaN is already the obvious choice for design engineers, and it represents the future in many other uses — from consumer chargers and power banks, through automotive onboard chargers and DC/DC converters, and many more applications across telecoms, defense, industrial, and more.

For those considering GaN for their designs, Avnet Silica provides impartial expert guidance to ensure that the transition to GaN is as smooth as possible, helping to maximise the benefits of this advanced semiconductor technology.

References

1. https://www.powerelectronicsnews.com/selecting-gan-or-sic-devices-with-a-focus-on-reliability/

Working on a project (LC)

Working on a power project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

EMEA Power Experts (LC)

About Author

 

Author placeholder image
EMEA Power Experts

We use 'EMEA Power Experts' as a collective byline when our team of power experts and writers collaborate on content.

 

Follow us (GBL)

Like what you see?

Follow us on LinkedIn

Follow our dedicated power page on LinkedIn for the latest power updates and news from our team of power experts.

Modal

Contact us

Submit your inquiry via the form below.