The ability to validate electronic circuit function accurately and reliably before committing to real-world layouts and manufacture is immensely valuable to design engineers. Being able to see and remedy potential issues without physical design respins to prove fixes, saves development cost and can also significantly speed time-to-market for projects.
SPICE (Simulation Program with Integrated Circuit Emphasis) allows engineers to model complex circuits with various components, including resistors, capacitors, transistors, and integrated circuits, to predict circuit behaviour. SPICE software is open source in nature and as such, many IC manufacturers are happy to provide models that design engineers can download and plug into popular simulators like PSpice and LTSpice.
Piecewise Linear Electrical Circuit Simulation (PLECS) meanwhile, has been developed specifically to address the simulation and modelling needs of higher power circuits where thermal and losses modelling in addition to basic circuit performance is a requirement.
Wide Bandgap - a High Power Enabler
In higher power designs, the electronics sector is witnessing a transition from silicon to wide bandgap (WBG) semiconductors, such as silicon carbide (SiC) and gallium nitride (GaN). In these designs, conventional SPICE modelling techniques are barely used. The reason for this is that they can be computationally expensive and slow, and are unable to provide an accurate indication of losses and thermals (at device junction and system level) that are both more serious concerns in high-power circuits. Instead, Piecewise Linear Electrical Circuit Simulation (PLECS) is the simulator of choice due its ability to model these characteristics.
PLECS uses ideal switches and lookup tables for losses, balancing accuracy and simulation speed. However, because the losses and thermal models use typical datasheet values, it is important for some design margin to be factored in.
NEED SUPPORT? CONTACT OUR POWER EXPERTS
The Promise of Digital in Power Electronics
The integration of advanced simulation tools in power electronics design is not just enhancing current capabilities but is also paving the way for future innovations. Power electronic design is, per se, always interdisciplinary, because there are electronics, thermals, mechanics and control systems that play into one design.
With PLECS modelling, it is possible to have a suitable estimation of the losses of the parts that are used in the design. The data that is coming out of this simulation step can then be used to estimate thermal needs for the design. Various gas and liquid flow simulation tools can help to estimate how the heatsink needs to be formed and predict the needed gas or liquid flow to have the temperature in the right window over all the possible load cases of the electronics.
Once that is done, further mechanical studies can be completed with FEM, which is often necessary (especially in vehicle applications) because the case that holds the power electronics is also a stressed member of the frame, which brings even more difficulties.
With electronics, thermals and mechanics covered, one piece of the puzzle is left -- the control side of things. Here, digital technology helps in the form of hardware-in-the-loop test stations, which mimic the hardware for the control system of choice. This means that a control algorithm can be programmed in software on a µC or µP, and the test stand will then mimic the hardware that has been chosen.
This enables engineering teams to work in parallel instead of solving tasks one after another. With HIL test stations, a change of parts is just a parameter change for the test stand, and a prototype rebuild is needed.
A Better Future with Simulation and Digital Twin Technology
Between SPICE, PLECS, FEM and HIL technology, the resources that engineers have at their disposal to accurately model and predict how power circuits and systems will perform are varied and plentiful. Accelerating time-to-market and reducing the number of development stages and therefore cost, is highly desirable to innovators in a commercial environment. In addition, being able to achieve better levels of efficiency, reliability and to predict maintenance needs through the use of digital twins, presents long-term benefits beyond the design phase and into the operating life of power electronics.
Technology
Power: designing solutions with power at the core
We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

With the ongoing shift to renewable energy and the electrification of transport and industry, the demand for higher power and greater energy efficiency in electronics is increasing. Wide bandgap technologies including SiC and GaN bring many advantages.
WBG OVERVIEWWorking on a power project?
Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.
Like what you see?
Follow us on LinkedIn
Follow our dedicated power page on LinkedIn for the latest power updates and news from our team of power experts.