Custom Meta Tags

Hero Banner

Sub Navigation

Title and intro (LC)

Enhancing Experiences in Hospitality with Generative AI at the Edge

The hospitality industry has always been defined by its ability to create seamless, enjoyable experiences for guests. However, as expectations for convenience, efficiency, and personalisation continue to rise, traditional service models are being challenged. AI-powered chatbots have already begun to reshape customer interactions, assisting with check-ins, room service requests, and general inquiries. Yet, many of these solutions rely on cloud-based processing, which introduces latency, dependency on internet connectivity, and potential data security concerns.

Generative AI at the Edge is addressing these limitations by moving chatbot processing away from remote servers and onto local, embedded hardware. By enabling real-time, on-device AI interactions, Edge Gen AI chatbots ensure faster response times, uninterrupted service, and greater control over sensitive guest data. For hospitality businesses, the shift to edge computing represents a significant opportunity to enhance both customer experience and operational efficiency.

Intro cont (MM)

What are the Challenges of Traditional AI Chatbots?

Cloud-based AI chatbots have become increasingly common in hotels, offering automated support for common guest interactions. However, these solutions often struggle with real-world challenges that can negatively impact the guest experience.

One of the biggest issues is latency. When a chatbot relies on cloud servers to process speech, generate responses, and send them back to the user, delays can occur—especially during high-traffic periods or in locations with poor internet connectivity. These delays make interactions feel unnatural and frustrating, undermining the efficiency that chatbots are meant to provide.

Edge GenAI in hospitality

Addressing latency (LC)

Another concern is reliability. Many hotels operate in environments where internet access can be inconsistent, such as remote resorts or cruise ships. If a cloud-based chatbot loses connectivity while real-time data processing, it becomes unusable, leaving guests without the automated support they rely on. This dependency on cloud infrastructure creates a single point of failure, making the system vulnerable to outages.

Data privacy and security also pose significant challenges. When guest interactions are processed through external cloud servers, sensitive personal information may be stored or transmitted off-site. This raises concerns about compliance with regulations such as GDPR and can erode guest trust in AI-driven services.

Finally, there is the issue of cost and scalability. Cloud-based AI processing requires significant bandwidth and server resources, which can become expensive for hotels looking to deploy chatbot solutions across multiple properties. As AI adoption grows, the cost of maintaining cloud-based services at scale can become a financial burden.

Addressing Latency, Data Security, and Reliability with Edge AI

Edge AI chatbots offer a solution by bringing AI processing directly to the device, eliminating the need for constant cloud communication. This approach offers several key advantages that are particularly relevant to the hospitality industry.

  • One of the most important benefits is low latency. Since all AI computations occur locally, chatbot responses are generated in real time, providing a more natural and fluid interaction for guests. This is especially critical for high-touch hospitality services, where delays in communication can create frustration.
  • Another key advantage is operational resilience. Unlike cloud-reliant systems, Edge AI chatbots continue functioning even during network disruptions. This ensures that check-in kiosks, concierge assistants, and room service interfaces remain accessible to guests regardless of connectivity conditions.
  • Data privacy and security are also significantly improved. Because Edge AI chatbots process interactions locally, guest data never has to be sent to external servers, reducing exposure to potential security risks. This is particularly valuable for hotels handling sensitive payment information, passport details, or guest preferences.
  • Finally, Edge AI provides cost efficiency and scalability. By eliminating the need for constant data transmission to cloud servers, Edge AI reduces bandwidth requirements and operational costs. Hotels can deploy multiple chatbot instances across different locations without incurring additional cloud processing fees.

NEED AI SUPPORT? SPEAK TO OUR EXPERTS

Edge Gen AI (GBL)

Generative AI at the Edge

See advantages of Generative AI at the Edge, learn more about Edge Gen AI locations, see Gen AI at the Edge in Action Edge and access Gen AI resources such as articles and case studies.

An AI chip 'on the edge'

Main body and conclusion (LC)

How to Implement Edge AI Chatbots in Hospitality

The flexibility of Edge AI chatbots makes them valuable across a wide range of hospitality applications. One of the most common use cases is automated check-ins and check-outs. Instead of waiting in line at the front desk, guests can interact with a voice-based chatbot that verifies their reservation, provides room details, and issues a digital key—all in a matter of seconds.

In-room automation is another area where Edge AI chatbots are making an impact. Guests can adjust room settings, request housekeeping, or order room service simply by speaking to an embedded AI assistant. By integrating with smart hotel systems, chatbots can personalise guest experiences based on past preferences, making stays more comfortable and intuitive.

Hotels and resorts are also using Edge AI chatbots for concierge services. Whether providing local dining recommendations, booking excursions, or answering questions about hotel amenities, chatbots can deliver accurate and context-aware responses without human intervention. Because these AI assistants operate on local hardware, they remain responsive even in remote locations with unreliable internet access.

Another emerging application is multilingual guest support. Edge AI chatbots powered by local language models can communicate with international travelers in their native language, eliminating language barriers and enhancing customer satisfaction. Unlike cloud-based translation services, local AI models provide instant speech recognition and response generation without network delays.

How Avnet Silica is Delivering Edge AI Chatbot Solutions

As the need for reliable, high-performance Edge AI solutions grows, companies like Avnet Silica are providing the hardware and software infrastructure to support next-generation chatbot applications. Avnet Silica’s Edge GenAI chatbot runs locally on TRIA System on Modules (SOMs), offering a modular and flexible approach to AI deployment.

The TRIA SOM platform is designed for scalability, allowing hospitality businesses to customise chatbot capabilities based on their operational needs. By integrating advanced AI engines such as Whisper for speech-to-text transcription and Piper for natural-sounding text-to-speech output, Avnet Silica ensures that chatbots provide accurate and engaging voice interactions.

One of the key advantages of the TRIA SOM platform is its ability to process AI interactions locally, reducing reliance on cloud servers and ensuring uninterrupted operation. This not only improves response times but also enhances data security, making it easier for hotels to comply with privacy regulations. Additionally, Avnet Silica provides ongoing software support to help businesses integrate Edge AI chatbots seamlessly into their existing hospitality systems.

The Future of AI in Hospitality

The rise of Edge AI chatbots represents a fundamental shift in how hotels and resorts approach guest service automation. By moving AI processing on-device, these systems deliver faster, more reliable, and more secure interactions that enhance the overall guest experience. The ability to function without internet dependency ensures that AI-powered services remain available at all times, creating a consistent and scalable solution for hospitality businesses worldwide.

Looking ahead, Edge AI is expected to play an even greater role in personalised guest experiences, automated concierge services, and multilingual support. As technology advances, hotels will be able to further integrate AI-driven automation into smart room controls, loyalty programs, and predictive guest services.

For those interested in exploring the broader implications of Edge AI chatbots across industries, the comprehensive article, Revolutionising AI Chatbots, provides deeper insights into how localised AI solutions are transforming customer interactions.

As the hospitality industry embraces the next generation of AI-driven automation, Edge AI chatbots stand out as a game-changing technology that enhances efficiency, improves guest satisfaction, and future-proofs hotel operations. Now is the time for hospitality leaders to explore how Edge AI can redefine their approach to customer service.

Working on a project (LC)

Working on an Artificial Intelligence project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

Michael Uyttersprot Author (LC)

About Author

 

Michael Uyttersprot
Michaël Uyttersprot

Michaël Uyttersprot is Avnet Silica's Market Segment Manager for Artificial Intelligence, Machine Learning and Vision. He has 20 years of experience in the industry, starting his career as an engineer in robotics. His current focus is on supporting the development and promotion of embedded vision and deep learning solutions to customers for projects involving AI and machine learning. Michael is seen as a thought leader in the field of AI and ML and has presented his work and thoughts to large audiences at industry events such as Hardware Pioneers Max.

Generative AI (GBL)

Overview

Generative AI Overview

Head over to our Generative AI overview page for more Generative AI articles, applications and resources.

Generative AI - chip brain and code

Modal

Contact us

Submit your inquiry via the form below.