Custom Meta Tags

Hero Banner

Sub Navigation

Generative AI title (LC)

Generative AI - From Imagination to Reality

Intro and MU video (MM)

Generative AIs are artificial intelligences that are designed to analyze text, images, video and other content formatted for human consumption, and use this data to create additional content that people can read, view, or listen to. ChatGPT from OpenAI is among the most famous examples of a generative AI – the G in GPT stands for “generative.” Generative AIs can accept a wide variety of natural language inputs (text, speech, even gesture), process those requests, and provide a response in the appropriate format, which could be text, video, or audio. That can include intermodal interactions, turning text to speech, for example. People will increasingly rely on generative AIs to provide information and support.

Generative AIs are typically deep-learning models. Deep learning is a specific type of neural network; neural networks are a specific type of machine learning (ML) that are set up to process information in a manner designed to mimic the way brains function. Generative AIs are almost always trained extensively on existing data (research papers, image libraries, music catalogs, fiction, etc.). Generative AIs can also be instructed to generate new content that previously did not exist – a novel, a movie script, an image, even video.

How to enhance embedded systems with Generative Al and Local LLMs | Michael Uyttersprot at HWPMAX25

Intro cont (LC)

Some of the most common use cases for generative AIs are:

  • Personal Assistants
  • Voice Assistants – (Alexa enhancements for smart homes)
  • Changing appearance on screens (vision related)

CONTACT OUR AI EXPERTS

Generative AI at the Edge

Generative AI at the Edge (MM)

Generative AI at the Edge - transforming industries

Generative AI at the edge is transforming the world around us by enabling low-latency, more secure and real-time AI on devices. Having AI 'on the edge' means personalised applications can run more efficiently without reliance on data centres. Learn more about Generative AI on the Edge, how it's revolutionising industries and its key applications with our dedicated Generative AI on the Edge microsite. 

Learn More

Running LLMs Locally (MM)

Running LLMs Locally

The large language model (LLM) is the foundation for the revolution in generative artificial intelligence (AI) that delivers natural interaction and even reasoning capability. The LLM also forms the basis for a new generation of agentic AI systems that can organise and perform complex tasks autonomously, adapting and responding to changing conditions. But why would one choose to run an LLM locally? We explore the fundamentals of LLMs, system requirements, implementation and overall benefits of running LLMs locally.

Learn More

GenAI applications (LC)

Key Generative AI applications

Edge Gen AI Chatbot (MM)

Generative AI at the Edge Chatbot

The Edge Gen AI Chatbot (demonstrated at Electronica 2024 and embedded world 2025) is a locally operated chatbot that runs directly on embedded devices, delivering fast, low-latency responses while ensuring enhanced privacy. Its modular software design allows flexibility across diverse hardware configurations, making it adaptable to specific application requirements. Additionally, it is compatible with a broad selection of TRIA System-on-Modules (SOMs) to optimise performance. Comprehensive software support is provided, offering robust resources and tools for seamless integration and customisation.

Learn More

Personal Assistants (MM)

Personal Assistants

Personal assistants are designed to respond to queries. Queries can be fairly simple requests to provide a single data point (“where is the nearest gas station?”), but they can also require research on complex subjects, with the requested result to be a report complete with high-level analysis (“provide a synopsis of ‘Gravity’s Rainbow’ and explain the major themes of the book”). Personal assistants of this nature can be installed on potentially any computer-based system; chat assistants (e.g. ChatGPT) and similar are now widely accessible through computers, laptops, and smartphones.

AI Personal Assistant - robotic cleaner

Voice Assistants (MM)

Voice Assistants

Voice assistants are a specific type of personal assistant in that the input is always spoken language. There are any number of well-known examples, among them Alexa (Amazon) and Siri (Apple). The first voice assistants were based on less sophisticated AIs and were capable of responding only to simpler requests (“play ‘Hotel California’ on Spotify”), but they are obvious candidates for generative AI. Voice assistants tend to be bundled into systems where hands-free operation is likely to be preferred. Originally voice assistants were built into smart speakers, but voice assistants are appropriate in other environments, including passenger vehicles, for example.

AI Voice Assistant

Changing appearances (MM)

Modifying Appearance on Screens

AI revolutionizes the way appearances are altered on screens through advanced algorithms that analyze, interpret, and manipulate visual data in real-time. From enhancing facial features to applying virtual makeup or altering backgrounds seamlessly, AI-powered software utilizes deep learning techniques to understand and modify digital content with unprecedented precision. By harnessing machine learning models trained on vast datasets, these technologies can intelligently adapt to diverse scenarios, ensuring natural-looking transformations and immersive experiences for users across various applications, including video conferencing, gaming, and virtual reality. A prime example of this is the Kontron x86 AMD Industrial Platform that was demonstrated on Avnet Silica's booth at Embedded World 2024 and electronica 2024. 

WATCH THE INTERVIEW WITH ELECTROPAGES AT EMBEDDED WORLD

Martin Grossen demonstrates the Kontron x86 AMD Industrial Platform at electronica 2024

Solutions (LC)

Featured Generative AI solutions

onsemi Image Sensors (MM)

onsemi Image Sensing Technologies

As a leader of intelligent sensing technology, onsemi develops innovative solutions with customers and specific applications in mind. Leveraging its deep technical expertise, onsemi's sensing products are designed to solve application-focused challenges, delivering efficient and optimized performance. onsemi offers a diverse portfolio of products serving a range of markets, including automotive, industrial, and commercial. Learn more about the: 

  • AR0820AT
  • AR0822
  • AR0823AT
Learn More

Featured article (MM)

Featured articles and podcasts

Evolution of Generative AI (MM)

The Evolution of Generative AI

Generative AI is not new. It has, however, recently taken an enormous leap in what it can do, inspiring no little amazement, as well as a bit of alarm.

A popular candidate as the first generative AI is the first chatbot, ELIZA, introduced in the 1960s, which was trained to respond like a psychologist. The subsequent history of AI research was marked by AI “winters” alternating with periods of resurgence typically coincident with some applicable technological advance, such as the introduction of microprocessors or the formulation of AI techniques such as back-propagation.

Learn More

Related articles (LC)

Who is Avnet Silica's AI expert, Michaël Uyttersprot?

Michaël Uyttersprot is Avnet Silica's Market Segment Manager for Artificial Intelligence, Machine Learning and Vision. He has 20 years of experience in the industry, starting his career as an engineer in robotics. His current focus is on supporting the development and promotion of embedded vision and deep learning solutions to customers for projects involving AI and machine learning. Michael is seen as a thought leader in the field of AI and ML and has presented his work and thoughts to large audiences at industry events such as Hardware Pioneers Max. He also regularly joins webinars in partnership with major AI players in the semiconductor space, including NXP, STMicroelectronics and AMD. 

Articles by Michael

 Podcasts featuring Michael

Episode 75: Billion-parameter brains in pocket-sized chips: The local AI revolution


Episode 59: Exploring Future Technology Trends - A Look Ahead with Avnet Silica


Episode 44: Seeing Beyond the Surface: AI in Defect Visual Inspection

 

Michael Uyttersprot

 

Related articles

AI Articles Teaser

DEEPX webinar image teaser shows DEEPX AI modules
Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem
By Michaël Uyttersprot   -   March 17, 2026
Technical article
Learn how you can enable efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem.
Read More
Trendliner cover - Q3 2025
Semiconductor market pulse: Six insights for Q1 2026
By Thomas Foj   -   February 12, 2026
Trend report
The latest on market trends, technology advances, and supply chain shifts shaping Q1 2026.
Read More
Microsoft logo
SQL Server IoT 2025: Bringing AI and Enhanced Analytics to Edge Data
By Yann Stridde   -   February 5, 2026
Technical article
Organisations are feeling increasing pressure to process information directly at the edge
Read More
Smart Agriculture Solutions webinar spotlight
Smart Agriculture Solutions
By Harvey Wilson   -   January 23, 2026
Technical article
Practical Innovations in Connectivity, Positioning and Edge Intelligence
Read More
'AI' illuminated on a AI semiconductor chip
FPGA vs GPU vs CPU vs MCU – hardware options for AI applications
By Michaël Uyttersprot   -   January 6, 2026
Technical article
Field programmable gate arrays (FPGAs) deliver many advantages to artificial intelligence (AI) applications. How do graphics processing units (GPUs) and traditional central processing units (CPUs) compare?
Read More
Smart building webinar
Integrating AI in Smart Buildings
By Harvey Wilson   -   September 8, 2025
Technical article
The way we design, operate, and interact with buildings is evolving rapidly. With the rise of AI, IoT, and advanced analytics, buildings are transforming into intelligent, energy-efficient structures that can adapt in real time to occupant needs.
Read More
Servers and windmills
Shaping the future of Healthcare - Avnet Silica's latest webinar series
By Harvey Wilson   -   January 20, 2025
Technical article
With the growing demand for personalised healthcare, remote monitoring, and advanced diagnostic tools, innovative electronics are paving the way for safer, smarter, and more efficient medical devices.
Read More
AI Vision - Human eye with graphics and code being analysed
Kits not bits - fast tracking edge AI development with ease and no risk
By Harvey Wilson   -   September 16, 2024
Technical article
This article looks at how these modules have evolved from development tools, for teaching and prototyping, to enterprise-quality components that can simplify your product development while meeting industrial standards.
Read More

Modal

Contact us

Submit your inquiry via the form below.

 
 

Spot Design Hub Project (GBD)

Tools

Design Hub

Browse and review over a thousand proven reference designs to accelerate your design process. Try our design tool and then export it to your CAD tool of choice.

Spot Training Events (GBD)

Training & Events

Learning for better, faster projects builds

Connect with the Avnet Silica experts who will guide you to reach further with your projects with on-going seminars, workshops, trade shows and online training.

Customer asking question at seminar.

Smart Cities (GBD)

Market

Smart City

Smart City is an opportunity to reimagine our cities with the goal to change our quality of life and to supply clean water and sufficient energy for all citizens in an environmentally sustainable and equitable way. Let's make our cities smart.

Smart City - Connected City

Contact Us (GBD)

Contact us

Have a question?

Int. Freecall - 00800 412 412 11 | Product or shop-related inquiries: OnlineSupportEU@avnet.com | For anything else, head over to our contact form.