Precise positioning as a foundation for smart agriculture
Smart agriculture is transforming how farms manage productivity, resources, and operational efficiency. As agricultural machinery becomes increasingly automated and connected, precise positioning is becoming a critical enabling technology.
Applications such as precision planting, automated spraying, drone-based crop monitoring, and autonomous vehicle guidance depend on machines understanding their position and movement with extremely high accuracy. Delivering this level of performance requires positioning technologies capable of moving beyond traditional meter-level GNSS accuracy.
u-blox addresses these requirements with a portfolio of high-precision GNSS technologies designed to support next-generation agricultural systems. By combining advanced receivers, correction services, and supporting hardware such as high-performance antennas, u-blox enables OEMs and system developers to implement reliable positioning solutions capable of delivering centimetre-level accuracy in demanding agricultural environments.
Precision agriculture applications
Modern agricultural systems rely on positioning data to guide a wide range of automated and semi-automated operations. These include yield mapping, variable-rate application of inputs, drone-based crop monitoring, precision planting, and autonomous vehicle guidance.
Each of these applications requires different levels of positioning accuracy. Yield monitoring and field mapping can typically operate with metre-level positioning, while applications such as variable-rate fertilizer or seed application require decimetre-level precision.
More advanced functions such as precision planting and autonomous tractor guidance demand centimetre-level accuracy and highly reliable positioning data. In these systems, machinery must be able to return to exactly the same field lines and maintain consistent alignment between multiple machines operating in the same environment.
Delivering these capabilities requires positioning systems that can provide both high absolute accuracy and repeatable positioning across large agricultural environments.
From meter-level GNSS to centimetre-level positioning
Standalone GNSS positioning typically delivers horizontal accuracy of one to two metres under ideal conditions. While this is suitable for asset tracking or telematics applications, it is insufficient for precision agriculture systems.
u-blox Webinar
Precise Positioning as a Key Enabler for Smart Agriculture
This session examines how precise GNSS positioning accelerates the adoption of smart agriculture and transforms resource management, crop production and machine operation.

Positioning errors arise from atmospheric effects, satellite orbit and clock inaccuracies, multipath reflections, and receiver noise. Without correction data, these factors limit the accuracy achievable with standalone GNSS receivers.
To overcome these limitations, high-precision positioning systems combine GNSS measurements with correction technologies such as Real-Time Kinematic (RTK) positioning and Precise Point Positioning (PPP). These approaches compensate for signal errors and allow positioning systems to deliver centimetre-level accuracy and high repeatability.
In agricultural environments, this accuracy is essential for enabling automated machine control, coordinated operations between multiple machines, and reliable sensor fusion with cameras, radar, and inertial measurement systems.
The u-blox high-precision positioning platform
u-blox supports precision agriculture through its u-blox locate platform, which integrates high-precision GNSS hardware with positioning services and development support.
This platform approach brings together several key elements required to deploy reliable positioning systems:
- High-performance multi-band GNSS receivers
- High-precision antennas optimized for multi-frequency signals
- Scalable correction services delivering centimetre-level accuracy
- Development tools and technical support to accelerate system integration
By combining these elements into a unified ecosystem, u-blox helps equipment manufacturers accelerate development while ensuring reliable positioning performance across a wide range of agricultural applications.
High-precision GNSS receivers
A key component of the u-blox portfolio is the ZED-X20P high-precision GNSS module, designed for demanding industrial and autonomous applications. The device supports multi-band GNSS operation across L1, L2, L5, and L6 frequencies as well as L-band correction signals, enabling access to multiple satellite constellations and correction services.
This architecture enables the module to support several positioning technologies including RTK, PPP-RTK, and PPP. The combination of multi-band reception and advanced correction algorithms enables centimetre-level accuracy while maintaining reliable positioning performance even in challenging environments.
The module also incorporates security features designed to protect positioning data and system integrity, supporting the development of reliable autonomous platforms.
Antennas and system integration
GNSS signals are extremely weak when they reach the receiver, making antenna quality and placement critical for achieving reliable positioning performance. To address this requirement, u-blox offers the ANN-MB2 all-band GNSS antenna. Developed for high-precision applications, it supports multiple GNSS frequency bands and is optimized for use with the u-blox X20 platform. The antenna enables robust reception from multiple satellite constellations and correction services while simplifying system integration for equipment developers.
Correction services with PointPerfect
To deliver centimetre-level positioning performance, u-blox provides correction services through its PointPerfect platform. These services deliver correction data via satellite and IP networks, allowing devices to compensate for GNSS signal errors and significantly improve positioning accuracy. Different service tiers support a variety of application requirements. High-performance RTK-based services can achieve positioning accuracy of one to two centimetres with convergence times of less than ten seconds, while more scalable PPP-based services provide global coverage with slightly longer convergence times. These services allow developers to deploy precision positioning systems in a wide range of agricultural scenarios, including autonomous vehicles, drones, and robotic equipment.
Example application: UAV precision positioning
The combination of high-precision receivers, optimized antennas, and correction services enables advanced applications such as drone-based crop monitoring and mapping.
In one example demonstration, u-blox technologies were used in a UAV platform operating in Finland. The system combined the ZED-X20P high-precision GNSS module with the ANN-MB2 antenna and PointPerfect correction services to deliver highly accurate positioning during flight operations.
This architecture enables UAVs to perform high-precision mapping, crop monitoring, and field analysis while maintaining reliable positioning performance.
Frequently questions
| Questions | Answers |
|---|---|
| Why is meter-level GNSS no longer sufficient for smart agriculture? |
As agricultural machinery becomes more automated, machines must understand their position and movement relative to other equipment with high precision. Meter-level positioning does not provide the repeatability required for tasks such as precision planting or automated spraying, where machines must operate along the same field lines across multiple passes. |
| Which agricultural applications require centimetre-level accuracy? |
Applications such as precision planting, row-based crop management, automated spraying, and coordinated harvesting depend on centimetre-level positioning. These tasks require machines to maintain precise alignment and repeatedly follow the same tracks in order to maximise productivity and minimise input waste. |
|
How should engineers choose between RTK, PPP, and PPP-RTK? |
Each positioning approach involves different trade-offs. RTK delivers the highest accuracy and fastest convergence but requires access to local base-station infrastructure. PPP and PPP-RTK offer broader geographic coverage and easier scalability, although convergence times may be longer depending on the service used. |
| Why is GNSS considered the reference for autonomous agricultural systems? |
GNSS provides the global reference frame used by other sensors within autonomous machines, including inertial measurement units, cameras, and radar. Reliable GNSS positioning allows these sensors to work together effectively within a sensor-fusion system that supports accurate vehicle guidance and control. |
| Why are multi-band GNSS systems combined with correction services? |
Even multi-band GNSS systems are affected by atmospheric and satellite-related errors that limit standalone accuracy. Correction services provide additional data that compensates for these errors, allowing positioning systems to achieve centimetre-level positioning accuracy. |
Article
Designing Smart Agriculture Systems: 5 Key Questions for Engineers
Smart agriculture is among the fastest-growing application areas for connected technologies, but what technologies are behind the transformation, and what do engineers need to consider?