Tria Smart Agriculture Solutions
As agricultural machinery becomes increasingly automated and connected, the way operators interact with machines is also evolving. Traditional control panels are gradually giving way to more advanced human–machine interfaces capable of analysing machine behaviour and responding to operator commands in real time.
Tria supports this transformation by developing embedded platforms that integrate artificial intelligence directly into edge systems. By combining embedded computing hardware, optimised software pipelines, and AI acceleration technologies, Tria enables developers to implement intelligent agricultural systems capable of perception, reasoning, and natural interaction.
These technologies allow agricultural machines to move beyond conventional interfaces toward systems that can communicate more intuitively with operators while supporting increasingly complex levels of automation.
Speech-to-speech interaction at the edge
A central focus of Tria’s smart agriculture demonstration is the implementation of a speech-to-speech AI pipeline designed to enable natural interaction between operators and machines.
In this architecture, speech input from the user is processed by a speech-to-text engine. The resulting text is analysed by a large language model (LLM), which generates a contextual response. This response is then converted back into audio using a text-to-speech system, allowing the machine to communicate directly with the operator.
This conversational interface opens new possibilities for human-machine interaction in agricultural environments. Operators can request machine status information, ask for operational guidance, or issue commands using natural speech rather than navigating complex control menus.
Why local AI processing matters
Running this type of AI pipeline locally offers several important advantages. Agricultural machines often operate in remote environments where reliable connectivity cannot be guaranteed, making cloud-based AI services impractical.
Local AI processing reduces latency, protects operational data, and enables machines to function without continuous internet access. For industrial and agricultural equipment, this combination of reliability, privacy, and responsiveness makes edge-based AI processing an attractive alternative to cloud-dependent architectures.
Optimising AI for embedded systems
Deploying advanced AI workloads on embedded systems requires careful optimisation. Developers must balance compute performance, memory usage, and power consumption while reducing model size and inference complexity.
Techniques such as model quantisation, parameter reduction, and optimised inference frameworks allow conversational AI pipelines to run efficiently on embedded hardware. Through these approaches, speech-to-speech systems can achieve practical response times, typically within two to six seconds for conversational interactions.
Demonstrating conversational AI on a smart tractor platform
To demonstrate the feasibility of this architecture, Tria implemented a proof-of-concept conversational interface for an intelligent tractor system.
Tria Webinar
Enabling Natural Language Control for Agricultural Machines
This session introduces how generative AI is transforming edge computing through a practical agricultural use case.

The demonstration integrates speech recognition, a locally running language model, and speech synthesis to enable direct interaction between the operator and the machine. The system also integrates sensor inputs and control interfaces that allow the AI system to interact with the tractor’s operational environment.
This proof-of-concept demonstrates that conversational AI can run effectively on embedded hardware when models and software pipelines are properly optimised.
AI-enabled human–machine interfaces
In addition to conversational interaction, Tria supports the development of advanced visual HMIs designed for modern agricultural equipment.
These interfaces integrate camera inputs, digital visualisation, and AI inference to provide operators with real-time insights into machine activity and environmental conditions. By combining video processing, AI analytics, and graphical dashboards, these systems provide a richer and more intuitive interface than traditional control panels.
Tria’s embedded platforms enable developers to integrate these capabilities into agricultural machines while maintaining the reliability and performance required for industrial environments.
AI acceleration through the DEEPX collaboration
To further enhance the capabilities of edge-AI systems, Tria is collaborating with DEEPX to integrate dedicated neural-network accelerators into its embedded platforms.
DEEPX processors such as the DX-M1 deliver high-performance AI inference while maintaining very low power consumption. These accelerators enable demanding workloads such as computer-vision analysis and AI inference to run efficiently on embedded systems.
Next-generation devices such as the DX-M2 are designed to support generative-AI workloads directly at the edge, delivering performance in the range of 25–30 tokens per second for large-language-model inference.
By combining embedded computing platforms with dedicated AI acceleration technologies, Tria enables developers to implement increasingly sophisticated AI capabilities directly within agricultural machinery.
Enabling the next generation of agricultural machines
Together with complementary technologies such as connectivity, sensing, compute platforms, and precision positioning, edge AI plays an increasingly important role in the smart agriculture ecosystem.
Working with Avnet Silica, developers can access Tria’s embedded platforms, AI frameworks, and partner ecosystem to accelerate the development of intelligent agricultural equipment.
Frequently questions
| Questions | Answers |
|---|---|
| Can the system support multiple languages in real time? |
Yes. Speech-to-speech AI pipelines can support multiple languages depending on the speech-recognition and language models used. Selecting appropriate models allows systems to recognise and generate responses in multiple languages. |
| Can speech processing operate entirely offline? |
Yes. Running AI workloads locally allows speech recognition, language processing, and speech synthesis to operate without cloud connectivity. This enables reliable operation in remote agricultural environments. |
|
What challenges arise when combining vision and transformer models on embedded systems? |
Both workloads require significant compute and memory resources. Developers must carefully balance system resources and optimise models to ensure efficient operation on embedded platforms. |
| What optimization techniques help overcome embedded-system constraints? |
Techniques such as model quantisation, reducing parameter sizes, and using optimised inference frameworks allow complex AI pipelines to run efficiently within the resource limits of embedded systems. |
| What advantages do dedicated AI accelerators provide? |
Dedicated neural-processing units significantly improve AI performance while maintaining low power consumption, allowing demanding workloads such as computer vision and generative-AI inference to run efficiently on edge platforms. |
To explore Tria solutions for intelligent Smart Agriculture platforms, contact Avnet Silica to discuss your project requirements.
Article
Designing Smart Agriculture Systems: 5 Key Questions for Engineers
Smart agriculture is among the fastest-growing application areas for connected technologies, but what technologies are behind the transformation, and what do engineers need to consider?