Custom Meta Tags

Hero Banner

Sub Navigation

Title and intro (LC)

Automotive Memory & Storage

Powering the Digital Vehicle: Understanding the Rising Importance of Automotive Memory and Storage

The automotive industry is entering a new era defined by electrification, autonomy, and connectivity. Electric vehicles (EV) are evolving into sophisticated computing platforms that generate, process, and store immense volumes of data. Memory and storage technologies are now central to this transformation, underpinning safety-critical control systems, infotainment and facilitating over-the-air (OTA) updates.

Intro cont (MM)

For automotive OEMs and Tier 1 suppliers, designing data-driven systems across diverse and demanding automotive environments is an inherently complex task. How then, can designers ensure the right balance between performance, reliability, and availability when every subsystem, from ADAS to battery management, has unique memory needs?

The answer lies in how the industry approaches the design, sourcing, and long-term support of memory and storage solutions. As vehicles become increasingly defined by software and data, memory is not just a supporting component – it’s fast becoming one of the defining factors shaping next-generation mobility.

CONTACT US

Computer memory RAM on circuit motherboard background. Close up. system, main memory, random access memory, onboard, computer detail.

Main body (LC)

Understanding the Unique Demands of Automotive Memory and Storage

Automotive systems operate in some of the harshest electronic environments – significant temperature variations, continuous vibration, and exposure to electromagnetic interference (EMI), all within compact, highly integrated systems. Non-volatile and volatile memory alike must perform reliably under these stresses for the duration of a vehicle’s service life. Furthermore, with vehicle models remaining in production for many years, sometimes with mid-cycle facelifts further increasing lifespans, manufacturers require stable access to identical components for prolonged periods.

The inherent longevity of automotive platforms fundamentally shapes the design approach. In consumer electronics, products such as mobile phones evolve rapidly, and component end-of-life transitions carry minimal impact. In contrast, a single change to a memory device within an automotive platform can trigger extensive requalification and validation across multiple electronic control units (ECUs), which may be deployed across countless models, leading to significant redesign costs.

For OEMs and Tier 1 suppliers, securing long-term availability, transparent change management, and dependable lifecycle support is therefore as strategic as the initial technology selection itself.

Stringent certification requirements, such as AEC-Q100 and ISO 26262 for functional safety, raise the bar further. Automotive-grade memory must undergo exhaustive validation, reliability screening, and traceability testing to ensure stable performance across millions of operating hours – particularly in safety-critical applications where data integrity cannot be compromised.

Even though these essential expectations are still difficult, emerging trends in vehicle design are making the situation more difficult.

Diagram of Closed vs Open Memory Architectures - NXP

An NXP diagram shows how an open architecture uses external memory such as NOR Flash. (Source: NXP)

Keeping Up with Expanding Data Footprints

Against this backdrop of longevity and reliability, data demands are accelerating. Modern vehicles now operate as distributed computing networks – processing and storing sensor, control, and infotainment data at the edge.

In advanced driver-assistance systems (ADAS) such as automatic emergency braking (AEB), multiple camera, radar, and LiDAR sensors generate continuous high-bandwidth data streams. These require high-speed DRAM to buffer and process frames in real time, while NOR flash provides secure, instant-access storage for boot code and calibration data. Non-volatile storage is also increasingly essential for data logging, OTA updates, and AI model retention – enabling vehicles to learn, adapt, and maintain functionality throughout their lifespan.

Infotainment and digital cockpit domains place different demands. Rich graphics, real-time navigation, and connected applications depend more heavily on high-capacity NAND-based storage such as eMMC or UFS to host operating systems, user data, and media files. This must also be supported by low-power dynamic memory, like LPDDR4, to ensure smooth rendering, low-latency interaction, and rapid response to user inputs.

Moreover, critical vehicle systems such as EV battery management systems (BMS) depend on small, fast SRAM arrays for real-time monitoring, cell balancing, and diagnostics, where deterministic latency and reliability take precedence over density.

In each subsystem, the memory must exactly match both the data behaviour and the environment it serves.

The Shift to Centralised Compute

The increased digitisation of vehicles is also driving a shift in architecture. Instead of numerous standalone ECUs, new zonal designs group electronic functions into a handful of high-performance compute zones that coordinate multiple domains, from safety to infotainment, through a central backbone. This consolidation reduces wiring complexity, improves power efficiency, and allows for faster data exchange between systems, enabling greater vehicle intelligence and functionality.

For memory, however, it raises the stakes – each zone now handles multiple real-time workloads, demanding high-bandwidth DRAM for active data processing, low-latency SRAM for control tasks, and increased NAND flash density to maintain reliability and performance under heavier data loads.

The Rise of Software-Defined Vehicles (SDVs)

At the same time, the rise of SDVs is reshaping how the industry approaches long-term design and value creation. By allowing functionality to be defined, updated, or activated through software, SDVs enable manufacturers to simplify production, reduce hardware variants, and deploy shared electronic platforms across multiple models.

For customers, they also offer a more dynamic ownership experience – one where capability evolves over time. OTA updates can unlock dormant hardware such as advanced driver-assistance features, activate comfort functions like heated seats, or introduce entirely new software-driven services. This transforms vehicles from fixed, hardware-bound products into continuously evolving digital systems. However, to support this adaptability, memory and storage must not only meet current technical requirements but also include the overhead necessary to accommodate years of software evolution and data growth.

Examples of these shifts are now evident with BMW’s iX3, unveiled at IAA 2025 – the company’s first fully software-defined production vehicle. Its deployment of “four superbrain” processing units highlight how modern automotive design is pivoting towards centralised processing where data is fundamental to how the vehicle operates and evolves through software.

Meeting the Next-Generation of Automotive Memory Requirements

Memory and storage sourcing in automotive design is inherently complicated, and mistakes in product selection can be incredibly costly. Navigating the complex myriad of technical, regulatory, and logistical challenges requires both deep expertise and reliable partners for today and tomorrow. Avnet Silica serves as that partner, combining a broad line card with supply chain assurance and in-house application expertise, allowing engineers to select the right combination of non-volatile and volatile memory for any vehicle subsystem – from ADAS to digital cockpit.

Micron

Micron directly addresses one of the biggest challenges in automotive design: long-term availability, giving engineers the assurance that DRAM, LPDDR, NOR, NAND, eMMC, and UFS solutions used early in development will remain available throughout multi-year vehicle platform programs.

Micron offers standardised lifecycle support for typical automotive programs, while an extended product longevity option ensures stability and continuity for mission-critical applications with 7–10+ year lifecycles and beyond. This helps to ensure replacements, requalification, and redesigns are minimised, maintaining schedule and cost control.

Devices such as the MT53E1G32D2FW-046 32 Gbit LPDDR4 SDRAM offer bandwidths of 4266 MT/s in a 200-ball TFBGA package with a wide temperature tolerance. It is suited for the latest infotainment and digital cluster deployments, where it can provide high-speed data buffering and real-time access for system-on-chip (SoC) processing.

Serial NOR flash solutions, such as the 1 Gbit MT25QL01GBBB8E12, deliver reliable, execute-in-place (XIP) enabled storage for automotive environments. The Quad-SPI interface ensures high-speed data transfer of up to 133 MHz, supporting applications such as infotainment OS storage, digital cluster boot code, or safety calibration tables.

Memory and Storage Overview (GBL)

Memory and Storage Overview

Our team is dedicated to helping you find the right parts for data storage in electronic systems. Memory products include a variety of both volatile and non-volatile devices, covering new and mature technologies.

Memory and storage

EV Charging (GBL)

EV Charging

Whether you’re manufacturing wall-boxes, or you need high power fast charging options with communications and security built-in, Avnet Silica has the experience and capabilities to deliver charging technology solutions at any scale.

An EV charger plugged in with the sun shining above

ADAS (GBL)

ADAS/Autonomous Driving

Advanced Driver Assistance Systems (ADAS) and autonomous driving technology are revolutionising the way we think about cars and transportation. ADAS includes a range of features designed to improve driver safety and convenience.

Aerial shot of cars with ADAS system graphics

MT53E1G32D2FW-046 (GBL)

Featured product

Micron MT53E1G32D2FW-046

The MT53E1G32D2FW-046 32 Gbit LPDDR4 SDRAM offer bandwidths of 4266 MT/s in a 200-ball TFBGA package with a wide temperature tolerance. It is suited for the latest infotainment and digital cluster deployments.

Micron MT53E1G32D2FW-046

MT25QL01GBBB8E12 (GBL)

Featured product

Micron MT25QL01GBBB8E12

The 1 Gbit MT25QL01GBBB8E12 delivers reliable, execute-in-place (XIP) enabled storage for automotive environments. The Quad-SPI interface ensures high-speed data transfer of up to 133 MHz, supporting applications such as infotainment.

Micron MT25QL01GBBB8E12

Conclusion and Webinar (LC)

Integrated Silicon Solution Inc. (ISSI)

ISSI maintains long-term production for lower-density and specialised products often excluded by other manufacturers, ensuring engineers can source components continuously without triggering costly redesigns.

Components such as the IS25LP040E-JYLA3-TR serial flash memory are AEC-Q100 automotive qualified, featuring a 104 MHz clock speed and fast QPI interface. Its functionality is ideal for small, safety-critical storage tasks such as storing boot code, calibration data, or firmware in ECUs, instrument clusters, and other control modules, where deterministic performance and reliability are essential.

SanDisk

Engineers face the challenge of managing larger volumes of sensor, infotainment, and AI data while maintaining reliability over long vehicle lifecycles. SanDisk provides high-performance, automotive-grade embedded flash drives, including eMMC and UFS solutions, tailored for the growing demands of connected and autonomous vehicles.

Within its portfolio, the iNAND® range of embedded flash drives includes both UFS and eMMC variants, offered in a wide range of capacities and featuring 3D NAND technology for higher density, improved endurance, and reduced cell-to-cell interference. Automotive-grade variants are AEC-Q100 qualified and engineered to support e-cockpits, infotainment, ADAS sensor fusion, and AI-driven workloads.

Features such as high read/write speeds, strong error correction, extended data retention, and thermal and power management optimised for automotive temperature ranges ensure reliable, long-term operation for next-generation vehicles requiring higher-density storage solutions.

Future-Proofing Automotive Memory: Navigating Innovation and Longevity

Looking ahead, automotive memory and storage will continue to evolve under competing pressures. The push toward centralised compute architectures, increasingly software-defined vehicles, and expanding data footprints drives innovation, while long vehicle lifecycles demand stability and predictable availability.

Future designs may further consolidate memory, favouring higher-density, high-bandwidth solutions. Yet for today’s engineers, one thing remains clear: a diverse portfolio of memory technologies is essential to meet the subsystem-specific demands of both current and next-generation vehicle architectures.

Webinar: Reimagining Automotive Design - Memory, Connectivity, and Intelligence Combined

As vehicles evolve into intelligent, connected, and software-defined systems, the demand for reliable memory, advanced connectivity, and long-term component stability has never been greater.

Join Avnet Silica and our key technology partners - ISSI, Macronix, Micron, and TE Connectivity - for an exclusive webinar dedicated to exploring how the latest innovations in memory and interconnect technologies are powering the transformation of the automotive industry.

From next-generation ADAS and autonomous driving to electrification and zonal architectures, our experts will uncover how cutting-edge solutions are enabling safer, smarter, and more sustainable vehicles.

Whether you are an engineer, designer, or decision-maker, this session will provide valuable insights into the technologies shaping tomorrow’s automotive systems - and how Avnet Silica and its partners can help you turn these innovations into reality.

REGISTER TODAY

ISSI logo
Macronix logo
Micron logo
TE Connectivity logo

Spot Automotive (GbD)

Markets

Automotive and Transportation

The automotive landscape is experiencing innovation like never before. Avnet Silica puts you in the driver’s seat by providing technical assistance every step of the way.

Modal

Contact us

Submit your inquiry via the form below.

 
 

Spot AI ML (GBD)

Technologies

Artificial Intelligence & Machine Learning

Avnet Silica’s focus is on machine learning on the edge, in the cloud, and on-premises. Avnet Silica provides state-of-the-art machine learning products and AI solutions close to end applications.

Spot Power (GBD)

Technologies

Power

Our EMEA power FAEs are helping hundreds of businesses across EMEA shift to more efficient, smarter and cleaner power technologies. Explore our power capabilities and browse resources on wide bandgap technology, thermal management and more.

Powering the Shift icon with text overlay

Contact Us (GBD)

Contact us

Have a question?

Int. Freecall - 00800 412 412 11 | Product or shop-related inquiries: OnlineSupportEU@avnet.com | For anything else, head over to our contact form.