Custom Meta Tags

Hero Banner

Title and Intro (LC)

In-Vehicle Networking

In-vehicle networking refers to the intricate system of interconnected electronic components within automobiles, facilitating communication and data exchange between various onboard systems. As automotive technology continues to advance rapidly, in-vehicle networking plays a pivotal role in enhancing vehicle functionality, safety, and efficiency. From managing engine performance to enabling advanced driver assistance systems (ADAS) and infotainment features, these networks integrate sensors, controllers, and actuators to create a seamless driving experience. With the emergence of autonomous vehicles and the integration of internet connectivity, in-vehicle networking stands at the forefront of innovation, reshaping the landscape of transportation and redefining the relationship between vehicles and their occupants.

The building blocks of In-Vehicle-Networking

Building blocks (Tabs)

CAN (Controller Area Network) transceivers play a crucial role in in-vehicle networking due to their ability to facilitate robust and reliable communication between electronic components within an automobile. These transceivers serve as the interface between the CAN protocol and the physical transmission medium, typically twisted-pair wiring. One of the primary reasons for their importance is their capability to withstand the harsh electromagnetic environment prevalent in vehicles, characterized by high levels of electrical noise and interference. CAN transceivers utilize differential signalling, which enhances noise immunity, ensuring accurate data transmission even in challenging conditions. Additionally, they enable efficient communication across multiple nodes within the vehicle, supporting real-time exchange of critical information between systems such as engine control units, anti-lock braking systems, airbag modules, and more. Overall, CAN transceivers are indispensable components in in-vehicle networking architectures, facilitating the seamless operation of automotive systems while prioritising reliability, efficiency, and safety.

Ethernet is increasingly crucial for in-vehicle networking as it accommodates higher data rates and advanced functionalities vital for modern automotive systems. With vehicles becoming more connected and automated, Ethernet's bandwidth is indispensable for transmitting large data volumes efficiently, supporting applications such as high-definition video streaming, advanced driver assistance systems (ADAS), and in-vehicle infotainment. Its scalability and flexibility enable the integration of diverse electronic components, while its interoperability benefits from a mature ecosystem derived from other industries, simplifying development and reducing costs for automotive manufacturers. Ethernet's ability to handle complex network architectures and deliver real-time information makes it essential for meeting the evolving demands of automotive technology, ensuring safer, more connected, and immersive driving experiences.

LIN (Local Interconnect Network) holds significance in in-vehicle networking primarily for its role in connecting and coordinating non-critical, peripheral electronic components within automobiles. Unlike more robust protocols like CAN (Controller Area Network) or Ethernet, LIN is designed for low-speed communication and is well-suited for applications such as controlling interior lighting, window motors, and climate control systems. Its importance lies in its cost-effectiveness and simplicity, offering a lightweight solution for integrating less critical systems, thereby reducing overall system complexity and cost. LIN enables efficient communication between various electronic control units (ECUs) while consuming minimal power, making it ideal for applications where real-time response is not critical. Moreover, LIN's deterministic behaviour ensures reliable operation, enhancing the overall efficiency and performance of in-vehicle networks.

Featured IVN products (LC)

Featured IVN products

TJA146x (GBL)

CAN

NXP TJA146x CAN Signal Improvement Capability

The TJA146x series actively improve CAN signals to ensure robust communication in large networks and at faster bit rates.

NXP TJA1462

NXP SJA1105EL (GBL)

CAN

NXP SJA1105EL

The SJA1105EL Ethernet switch offers a flexible solution for implementing modular and cost-optimized ECUs capable of supporting any in-vehicle connectivity requirement.

NXP SJA1105EL

UJA1023T (GBL)

LIN

NXP UJA1023T

The UJA1023 is a stand-alone Local Interconnect Network (LIN) I/O follower that replaces basic components commonly used in electronic control units for input and output handling.

NXP sot109

All NXP FSP (GBL)

All

See all NXP Products

See all NXP products via the Avnet Silica Full Service Portal.

NXP Logo

Featured resources (LC)

Featured Resources

IVN Article (GBL)

Article

The Transformative Journey of In-Vehicle Networks

As vehicle designs have evolved to include infotainment systems, vehicle-to-everything communication (V2X), and advanced driver assistance systems (ADAS), the volume of data that flows within the IVN has increased dramatically.

In Vehicle Networking

Ethernet Evolution (GBL)

Article

Ethernet evolution: The rise of SPE & TSN in automotive and industrial

The ability to deliver a deterministic, time - synchronised network link using lightweight, flexible, single-pair Ethernet cables offers significant benefits to industrial and automotive networking.

Single Pair Ethernet

ADAS (GBL)

Automotive

ADAS, autonomous driving, and sensors: smart linking

Learn more about regulations surrounding Advanced Driver Assistance Systems, see featured ADAS and sensor products, and read more in our technical articles.

ADAS Arial Shot