RF and Connectivity Banner (HB)

Display portlet menu

RF & Connectivity

RF and Connectivity Sub Navigation

Display portlet menu

EBV - RF and Connectivity - trends (LC)

Display portlet menu

Trends: Basestation

Wireless communication is an important part of everyday life in the broad field of consumer electronics where Bluetooth, BLE, WLAN and other RF technologies already play a significant role. EBV Elektronik identified the most exciting trends in the sectors of:

GSM/UMTS/LTE

A wireless base station provides a secure connection between multiple host devices

After the data processing on the transmitter side of mobile communications base stations for GSM, UMTS, LTE, etc., the digital audio stream next reaches a very fast D/A converter (DAC) and is then sent as an analog signal by cable to the remote radio head or to tower mounted amplifiers where special LDMOS transistors, which are particularly suitable for RF, amplify the signals, in order to forward them to the antenna. On the receiver side of the base stations an LNA initially amplifies the RF signal before it is then transferred via PLLs and particularly fast A/D converters (ADC) from the analog RF domain to the digital domain.

Tetra and Digital Radio Services (MM)

Display portlet menu

Tetra and digital radio services

From RF side, tetra-and trunked radio networks operate in the same way as the publically accessible mobile communications networks

Although tetra-and trunked radio systems employ major functional elements, which are also used in public mobile communications applications such as GSM, UMTS or LTE, they also offer additional functionality such as point-to-multipoint connections and additionally work in other frequency ranges. In addition, the numbers of the terminals are several orders of magnitude lower than for public mobile communications, because only relatively small teams of railway-, police-, fire-service- and emergency-service workers, etc., operate in tetra- and trunked-radio systems. On the RF side, tetra-and trunked radio networks operate in the same way as the publically accessible mobile communications networks: after the data processing on the transmitter side of mobile communications base stations for GSM, UMTS, LTE, etc., the digital data stream next reaches a very fast DAC and is then sent as an analog signal by cable to the remote radio head or to tower-mounted amplifiers, where special LDMOS transistors, which are particularly suitable for RF, amplify the signals, in order to forward them to the antenna. On the receiver side of the base stations an LNA initially amplifies the RF signal before it is then transferred via PLLs and particularly fast ADCs from the analog RF domain to the digital domain.