Custom Meta Tags

Manufacturer Hero Banner

Franchised Partner

Xilinx Main Title

AMD

Xilinx Mixed Media

AMD develops highly flexible and adaptive processing platforms that enable rapid innovation across a variety of technologies – from the endpoint to the edge to the cloud. AMD is the inventor of the FPGA, hardware programmable SoCs and the ACAP, designed to deliver the most dynamic processor technology in the industry and enable the adaptable, intelligent and connected world of the future. For more information, visit www.amd.com.

Manufacturers Categories Static HTML

Xilinx Featured product highlights (LC)

Featured product highlights

EBV - Product Highlights - AMD Cost-Optimized Products (GBL)

AMD Cost-Optimized Products

Learn how the broad portfolio of AMD FPGAs and SoCs are ideal for many applications, regardless of if you're looking for performance, power, or physical size, while maintaining cost optimization.

EBV - Product Highlights - AMD Xilinx Industrial Robotics (GBL)

AMD Industrial Robotics

Discover how the AMD Kria™ robotics starter kit, along with the Kria™ robotics stack, enables rapid development for robotics, machine vision, and industrial communication and control, through adaptive computing.

EBV - Product Highlights - AMD Smart Door Lock (GBL)

AMD Smart Door Lock

Step into the future of home security with smart door locks, where cutting-edge technology meets convenience. One standout innovation in door locks is the integration of camera-based AI systems for face-recognition.

EBV - Motor Control - Product Highlights (GBL)

Motor Control Solutions

Digital motor control can be defined as a drive system that combines an electric motor with power electronics for its energy delivery and processor units for motion control, as well as sensor and communication interfaces.

EBV - Product Highlights - AMD KRIA Adaptive MC SOMs (GBL)

AMD Kria™ Adaptive Motor Control SOMs

AMD is focused on developing power-efficient and highly deterministic industrial solutions suitable for large-scale deployments. The AMD Kria™ starter kit offer a latency advantage when compared to competitive products.

EBV - AMD-Xilinx - Kria SOM Family Highlights (GBL)

AMD Kria™ SOM Family

AMD Kria™ SOM Family is ideal for Edge and Vision Application Development and features a custom custom-built Zynq™ UltraScale+™ MPSoC device in a small form factor card.

EBV - Product Hightlights - AMD Healthcare (GBL)

Adaptive & Intelligent Healthcare Solutions from AMD

Technological advancements that are creating solutions for earlier detection, better imaging, and virtual and robotic-assisted care have the ability to help healthcare providers increase patient outcomes and provide more effective personalized care.

EBV - AMD - ZUBoard 1CG Highlights (GBL)

AMD ZUBoard 1CG

The ZUBoard 1CG provides the flexibility and versatility for engineers to experiment with and learn the AMD Zynq™ UltraScale+™ architecture.

EBV - AMD robotics starter kit (GBL)

AMD Kria™ KR260 Robotics Starter Kit

The AMD Kria™ KR260 Robotics Starter Kit integrates high-performance industrial interfaces and features native ROS 2 support. It enables roboticists and industrial developers without FPGA expertise to develop hardware accelerated applications.

EBV - MiniZed Dev Board Grid Box Light (GBL)

AMD MiniZed Development Board

Featuring a AMD Zynq™ Z7007S, which integrates an Arm Cortex-A9 processor with AMD Artix™ 7 programmable logic, the MiniZed is a low-cost yet versatile development board targeted for entry-level Zynq designs.

EBV - AMD - Hackster Grid Box Light (GBL)

Hackster.io AMD Projects

Everything you need to get going fast!

EBV Xilinx NPI teaser (NPI-table)

Image Product Description Link New

EBV - AMD - Related events Static HTML

 

Related events

AMD: Cost-Optimized Portfolio for Industrial Cameras | EBV Elektronik

AMD: Cost-Optimized Portfolio for Industrial Cameras

Online, On Demand

This presentation explores some of the trends driving new processor requirements in industrial cameras and provides examples of Xilinx's recent solutions that offer increased performance per watt and unlock intelligence, resolution, and speed for compact form factor cameras

EBV Xilinx NPI headline (html)