Broadcom Slew Rate Control Gate Driver | EBV Elektronik

Display portlet menu

Broadcom Slew Rate Control Gate Driver | EBV Elektronik

Display portlet menu

Broadcom | Reduce Motor EMI and Insulation Voltage Stress with Slew Rate Control Gate Driver

Online, On Demand


Live presentation date: October 5, 2022 

Overview

The pulse-width modulation (PWM) technique is widely used in insulated-gate bipolar transistor (IGBT) inverters. The high switching speed of theIGBT leads to high dv/dt in the inverter and results in a lot of negative side effects to the motor drive. These side effects degrade and reduce the lifetime of the motor. Broadcom's new slew rate control smart gate driver provides a simple and cost-effective way to reduce the high dv/dt, improve the lifetime and performance of the motor.

In motor drives, easy control and high efficiency are some of the many benefits of variable speed or frequency drives (VSD/VFD). However, the operation of these pulse-width modulation (PWM) driven motors causes a number of negative effects in the equipment, such as. damage to the motor’s insulation and bearings due to the excessive dv/dt voltage. Signal errors in equipment can arise due to strong EMI generated by PWM driven motors. These negative effects degrade the lifetime and performance of the motor.

Existing solutions use expensive and bulky dv/dt filters which lead to efficiency losses. In this webinar, we will introduce the new slew rate control smart gate drive, ACFJ-3405, to control the dv/dt of the IGBT dynamically. ACFJ-3405 has 2 levels of slew rate control which change the strength of its output current, driving the gate of the IGBT. Depending on the motor current loading condition, the dv/dt and switching loss will be optimized by ACFJ-3405, as it controls its output driving strength dynamically. This simple and cost-effective method of controlling the IGBT slew rate will help to improve the lifetime and performance of the motor.

Key Takeaways

  • ​Understand how the PWM technique and the long cable between drive and motor cause excessive dv/dt voltage
  • Recognize the many negative effects to the motor due to the high dv/dt
  • Discover how the new slew rate control smart gate drive solves dv/dt issues
  • Learn about other smart gate drive features that can protect the IGBT and improve the lifetime of the inverter

Speaker 


Arndt Schwaiger, Field Applications Engineer, Industrial Products, Broadcom Inc.

 

Register Now

Broadcom Slew Rate Control Gate Driver | EBV Elektronik

Display portlet menu

RELATED EVENTS

NXP | Secure your next wireless system with NXP latest wireless connectivity & hardware security solutions

Online, On Demand

Join our 1.5-hour webinar to explore NXP's wireless connectivity solutions, upcoming products, and secure communications aligned with the Cybersecurity Resilience Act.

Witekio | Navigating the EU Cyber Resilience Act: Avoid Penalties and Enhance Security

Online, On Demand

Join Witekio and EBV Elektronik's webinar to master the EU Cyber Resilience Act. Gain crucial insights for OEMs, engineers, and product managers to navigate cybersecurity compliance.

NXP | Live Lab: Designing Motor Control Applications with New MCX

Online, On Demand

Discover the groundbreaking NXP MCX MCU series for motor control! Join EBV's Canberk Sezer in this webinar to explore advanced features, performance, and applications.