Training & Events
Renesas and Witekio: Embedded Artificial Intelligence / Machine Learning
Date: 16 juin 2020
Location: Online, On Demand
Artificial Intelligence   Filter By   Artificial Intelligence RSS FEED
AI is changing the game. Whether you're working on systems that act intelligently in a specific domain (narrow AI), or in general (strong AI). Designing those systems is no easy task. Explore our resources to stay up to date in the world of AI trends, technology, and technical expertise.
Smart cameras and image processing combined
Lernende Roboter Passen Sich An Ihre Aufgaben Und Umgebung An
2 août 2022
Zukünftig können die mechanischen helfer ohne programmierung unterschiedliche objekte greifen und sich in komplexen umgebungen unabhängig bewegen.
Smart cameras and image processing combined
How Learning Robots are Adapting to Their Tasks and Environment
2 août 2022
While robots required complicated programming by experts in the past, the systems will be able to teach themselves how to carry out their tasks in the future. This will allow robots to adapt autonomously to changing surrounding circumstances
Smart cameras and image processing combined
Von Der Vorausschauenden Wartung Bis Zum Kollaborativen Roboter
1 août 2022
Die KI kann zum Wachstumsmotor für die Industrie werden: Alleine in Deutschland könnte bis 2030 das Bruttoinlandsprodukt durch den frühen und konsequenten um bis zu vier Prozent höher liegen als ohne den Einsatz von KI
Smart cameras and image processing combined
From Predictive Maintenance to Collaborative Robots
1 août 2022
AI and machine learning are exploiting opportunities in connection with Industry 4.0 in particular because enabling a production operation to organize itself autonomously and respond flexibly takes huge volumes of data.
view from autonomous vehicle as it interprets street signs
FPGA vs. GPU vs. CPU – hardware options for AI applications
7 avril 2021
Field programmable gate arrays (FPGAs) deliver many advantages to artificial intelligence (AI) applications. How do graphics processing units (GPUs) and traditional central processing units (CPUs) compare?
view from autonomous vehicle as it interprets street signs
Top 10 pitfalls in developing machine vision systems with artificial intelligence
7 avril 2021
Machine vision (MV) and artificial intelligence (AI) provide valuable inspection and analysis capabilities to a wide range of leading-edge applications. As with all advanced technologies, there are pitfalls to avoid.
interior of autonomous car
The State of Automotive Only Starts with Autonomous Driving
6 mars 2020
Learn how the state of automotive spans a variety of applications, from electrication to in-cabin AI.
The brain functions like a machine, or so according to the theory of Marvin Minsky, one of the most important pioneers of artificial intelligence.
KI-Pionier Minsky: Vorläufig tot?
4 mars 2019
Das Gehirn funktioniert wie eine Maschine, so die ­These von einem der wichtigsten Pioniere der ­Künstlichen Intelligenz. Also kann man es nach­bauen – und sich durch ein Back-up des Bewusstseins auf einem Rechner unsterblich machen.
Could our entire life simply be a computer simulation
AI-pioneer Minsky: Temporarily dead?
4 mars 2019
The brain functions like a machine, or so according to the theory of Marvin Minsky, one of the most important pioneers of artificial intelligence. In other words, it can be recreated – made immortal by backing up its consciousness onto a computer.
Mit verschiedenen Ansätzen der Datenauswertung sollen Maschinen intelligent werden.
Neuronale netze simulieren das gehirn
27 février 2019
Mit verschiedenen Ansätzen der Datenauswertung sollen Maschinen intelligent werden. Im ­Fokus steht dabei nicht nur die Leistungsfähigkeit, ­sondern immer mehr auch eine Flexibilität, wie sie das menschliche Gehirn bietet.
Kognitive Computerassistenten helfen Medizinern bei Diagnose- und Therapieentscheidungen.
Ist KI besser als der arzt?
27 février 2019
Kognitive Computerassistenten helfen Medizinern bei Diagnose- und Therapieentscheidungen. ­Sie sind deutlich schneller bei der Auswertung von medizinischen Informationen und erreichen ­mindestens die gleiche Präzision.
Cognitive computer assistants are helping clinicians to make diagnostic and therapeutic ­decisions
AI better than the doctor?
27 février 2019
Cognitive computer assistants are helping clinicians to make diagnostic and therapeutic ­decisions. They evaluate medical­ data much faster, while ­delivering at least the same level of precision.
Artificial neuronal networks are playing a big role
Neuronal networks simulating the brain
27 février 2019
Machines are being made more intelligent based on a variety of data analysis methods. The focus of these efforts is shifting increasingly from mere performance capability towards creating the kind of flexibility that the human brain achieves.
Artificial Intelligence has enormous potential for improving our lives
AI Smarter than humans?
25 février 2019
What began in the 1950s with a conference has grown into a ­key technology. It is already influencing our lives today, and as the intelligence of machines increases in the future that influence is bound to spread much more.
KI ist eine Schlüsseltechnologie, die sich in den kommenden Jahren nicht nur maßgeblich auf unser tägliches Leben, sondern auch auf die Wettbewerbsfähigkeit der gesamten Wirtschaft auswirkt.
Ist KI schlauer als der Mensch?
27 février 2017
Was in den 1950ern mit einer Konferenz der KI-Pioniere John McCarthy und Marvin Minsky begann, ist zu einer Schlüsseltechnologie ­geworden.­ Sie beeinflusst schon heute­ ­unser Leben – und wird es mit steigender Intelligenz der Maschinen in Zu
First        1        Last          Results Per Page: 30  60  90  All