Analog and power management considerations | EBV Elektronik

Analog and power management considerations | EBV Elektronik

Analog and power management considerations for low power asset tracker design

Milan Ivkovic Photo
ST Analog Asset Tracking

With the advent of the industrial internet of things (IIoT) and a continued move towards shorter supply chains, tracking deliveries and consignments is increasingly necessary. Compact, robust, battery-powered wireless asset trackers are regularly attached to shipping containers and pallets to keep customers and suppliers informed of delivery progress and how well the goods have been treated during transportation.

This article will investigate engineers' technical challenges when designing wireless asset trackers. Emphasis is placed on the selection of analog components and the constraints imposed by battery operation.

 

Why are connected asset trackers essential for supply chains?

Whether retail or manufacturing, many businesses constantly strive to minimise the amount of inventory they hold. Holding stock adds considerable costs to an operation already operating on tight margins. Warehouses and staffing them is an expensive business, which is why a just-in-time philosophy has become so popular for supply chains and logistics operations. However, this requires a constant stream of inbound shipments to fulfil customer orders and knowing their location has become crucial.

The internet of things has already transformed many business operations and consumer services, and the development of battery-powered wireless connected asset trackers continues the adoption of IoT technologies.

 

Asset tracker architecture

Essentially, an asset tracker contains circuit functions to determine its position and communicate the location data with a unique identifier to a central tracking control system. Depending on the type of consignment they are tracking, a tracker may be placed outside a shipping container with materials on a pallet or on the vehicle making the delivery. Asset trackers are usually entirely self-contained and operate from a battery source to provide maximum flexibility. Consequently, understanding the power consumption profile of the asset tracker is extremely important.

 

Another aspect of an asset tracker is that, since it can send location data, typically over a cellular wireless link, it could also send a small amount of additional information that might be useful. Some goods, for example, an urgent pharmaceutical delivery, may stipulate strict temperature-controlled conditions, so sending the consignment's temperature provides an audit of the environmental conditions during its journey. A shipment prone to damage from mechanical shock would benefit from constantly monitoring acceleration forces and shocks. Different analogue and digital sensors can provide information on various environmental, mechanical, and positional parameters. Figure 1 illustrates the major functional blocks of a wireless asset tracker.

Asset Tracking


Figure 1 - The major functional blocks of a battery-powered wireless connected asset tracker – key analog functions are highlighted in the shaded areas (source ST)


Asset tracker design challenges

Reliability is a crucial design requirement for a self-contained asset tracker. Maintaining operation over weeks and months from a battery emphasises ultra-low power design. It is a delicate balancing act between minimising power consumption and higher power demands when sending regular tracking updates. Three design considerations stand out as requiring an in-depth review.

 

Efficient DC-DC conversion and regulation

Factors influencing the choice of battery include its capacity, the physical shape and dimensions, and the output voltage. It may be that the battery voltage does not cater to all required circuit voltages, so DC-DC conversion will be necessary to a step up or step down a supply rail. Also, the battery voltage will typically reduce slightly as its charge reduces, so tight voltage regulation should be employed to prevent erratic tracker behaviour.

 

Battery current and voltage monitoring

The battery's discharge state is an essential indicator of the tracker's operational status. Monitoring the terminal voltage and load current allows it to be sent together with location data and other vital sensor data to the host monitoring application. Since the monitoring circuits also depend on the battery for its supply, it is imperative that these functions also have low power consumption characteristics.

 

Fast and precision analog sensor design and signal processing

Discrete analog sensor circuits and digital sensor ICs should also have low power credentials. Operational amplifiers (op-amps) are a popular method of architecting low power sensor elements and signal conditioning circuitry. Examples include the battery current and voltage measurement functions in addition to temperature, humidity, pressure, and strain parameters. Op-amps used in these circuits should also offer a quick and fast measurement capability. During active operation, the power consumption will increase, and the time duration for a sensor to register a precise value is key.

 

Selecting analog and power management components for a low power wireless tracker

Let's investigate some analog and power management components suitable for use in low power asset trackers, starting with power conversion and regulation.

The ST1PS02 series is an example of a nano-amp quiescent step-down DC-DC converter from STMicroelectronics. This converter offers a no-load current consumption of just 500 nA, is 92 % efficient when supplying a 10 mA load, and can deliver up to 400 mA at full load. Designed specifically for compact wearable consumer electronics and portable industrial sensors, the ST1PS02 is constructed in a miniature TQFN12 plastic package measuring 2 mm x 1.7 mm x 0.55 mm. Figure 2 showcases the device used in an example use case. Only an inductor, some small decoupling capacitors and two resistors are necessary to enable all features of the DC-DC converter circuit.

 

ST1PS02 Diagram


Figure 2 - An example application using the high efficiency ST1PS02 400 mA nano-quiescent synchronous step-down DC-DC converter with digitally selectable output voltage (source ST)

 

The ST1PS02 series has an input voltage range of 1.8 V to 5.5 V and can deliver a single selectable output voltage (device dependent) between 1.0 V to 3.3 V. The logic inputs D0, D1, D2 determine the precise output voltage setting which can be hardwired on the PCB. Alternatively, the output level can be controlled from the MCU to optimise the voltage level according to application requirements. An under-voltage lockout feature disables the output, should the input fall below 1.57 V. Output voltage regulation is maintained within +/- 1.5 % of nominal output.

Another low power management IC suitable for asset tracker applications is the STLQ020 series. This 200 mA low-dropout voltage regulator can accommodate an input voltage between 2 V to 5.5 V and has a no-load consumption of 300 nA. The series is available with either a fixed output voltage, in the range of 0.8 V to 4.5 V, or with an adjustable output voltage. Figure 3 shows the internal architecture of the fixed output voltage variant of the STLQ020 series.

 

LDO Diagram


Figure 3 - The internal architecture of the low power 200 mA ultra-low quiescent current LDO (source ST)

 

The STLQ020 is available in a choice of three package formats, the smallest of which measures 0.773 mm x 0.773 mm x 0.36 mm - Flip-Chip 4

As previously mentioned, measuring the battery's voltage and the load current provides a reliable indication of the asset tracker's health status. Ultra-low-power op-amps offer a viable method of measuring low currents. Suitable devices include the TSU101 and the TSU111 from ST. The TSU101, for example, is a 580 nA per channel op-amp capable of rail-to-rail operation with a low supply voltage range from 1.5 V to 5.5 V. The gain-bandwidth product of 8 kHz makes them suitable for a range of battery-powered, portable sensor and signal conditioning applications.

Figure 4 shows an example current sensing application using a shunt resistor to measure the current. The input voltage offset through the divider requires a low bias current op-amp to prevent influencing the current measurement. The ST TSU111 op-amp, highlighted in Figure 4, offers high accuracy, typically 150 mV, 11.5 kHz gain-bandwidth, and a ten pA input bias current, and zero-drift technology providing temperature stability as well as high precision.

 

TSU111 Diagram


Figure 4 - A current measurement reference circuit using a TSU111 nano power high accuracy op-amp (source ST)

 

We can measure different input current ranges by tuning the resistances (Rsense = 100 mOhm) and Vref. The critical factor is the absolute minimum current capable of measurement. In the circuit, the impedance seen from the Rsense towards the op-amp is high, so the current drawn is negligible.

What is critical is the bias current from the op-amp, which flows through the 100 Ohm resistors. Even one mV over sense resistor, as illustrated in Figure 4, will generate an error and order of magnitude higher than the 150 mV offset voltage of the selected op amp.

Another sensing example is for the asset tracker to measure the ambient temperature. Figure 5 highlights a simple sensor example using an ST STLM20 precision analog ultra-low current temperature sensor with a ST TS883 rail-to-rail nanopower dual comparator.  

 

TS883 Diagram


Figure 5 - An example analog temperature sensor circuit incorporating the ST TS883 nanopower comparator (source ST)

 

The two comparators of the TS883 are configured to monitor the ambient temperature within ±10 °C of a +25 °C centre temperature. Resistors R1, R2, R3 create a voltage divider to set the two comparator reference voltages. At 25 °C, the output voltage is 1.574 V, and the highest temperature limit of 35 °C, the output is 1.457 V, and at the lower threshold 15 °C, the output is 1.691 V. Further details on how to create a similar design and how the resistor values are calculated can be found in ST Application Note AN4071.

The TS883 is a rail-to-rail 0.9 V open drain dual comparator. Current consumption is typically 250 nA per comparator.

 

Analog design; the vital ingredient for low power asset trackers

By incorporating low power analog sensing and power management components in an asset tracker, battery life is prolonged, helping logistics and supply chain professionals to stay informed on the location of their consignments.

 

Discover ST’s analog portfolio and find more application examples

ST Analog is colourful

 

  About Author

Portrait photo of Karl Lehnhoff

Karl Lehnhoff joined EBV Elektronik in 2008 as a regional application manager. From 2011 till 2019 he headed the renewable energies segment, today called city and infrastructure, as a director. He has served in his current role since March 2019. Previously he held multiple different roles in R&D, field application engineering and field sales. He has a degree as Dipl.-Ing. (FH) in electronics from University of Applied Sciences in Dortmund.

About Author

Milan Ivkovic Photo
Milan Ivkovic

Milan Ivkovic received his Dipl-ing. diploma in 2000 and MSc diploma in 2007 at the University of Be...

Analog and power management considerations | EBV Elektronik

Analog and power management considerations | EBV Elektronik

Related Articles
How Chip-on-Board Technology is Driving a New Era of Embedded Intelligence
How Chip-on-Board Technology is Driving a New Era of Embedded Intelligence
March 17, 2026
Chip-on-Board (CoB) technology integrates dual-band Wi-Fi SoCs directly onto PCBs, enabling compact, efficient, and secure devices. This approach helps engineers build smarter, scalable products across life sciences, smart homes, and beyond.
Image of How STMicroelectronics Helps Pozyx Power Industrial RTLS
How EBV Elektronik and STMicroelectronics Helps Pozyx Power Industrial RTLS
November 17, 2025
The article explores how Pozyx leverages STMicroelectronics components to create a precise and robust location tracking system, highlighting the specific requirements for tags and anchors.

Analog and power management considerations | EBV Elektronik

Related Events
ebv25116-EBV-onsemi-Imaging-Solutions-for-Drones-768x432
onsemi I Imaging Solutions for Drones and Autonomous Mobile Robots
Date: October 28, 2025
Location: Online, On Demand

Related Designs Menu

Related Designs Menu